<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Soldering Curve for P1020 in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Soldering-Curve-for-P1020/m-p/401289#M2233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please, refer to these documents:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/package_info/PBGAPRES.pdf" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/package_info/PBGAPRES.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3300.pdf" target="_blank"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3300.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/files/product/doc/ENV_PBFREEOV2.pdf" target="_blank"&gt;http://www.freescale.com/files/product/doc/ENV_PBFREEOV2.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note. Package Peak Temperature (PPT) profile is for determination of components Moisture Sensitivity Level (MSL) and the parts’ processability per J-STD-020. PPT is the minimum temperature used for MSL qualification. Actual reflow temperature should not exceed this value. Optimal temperature profile depends on the solder paste and flux used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The actual reflow profile to be used for any PCB should be available from the paste supplier as a recommended profile. Use care when looking at the paste reflow profiles supplied by paste vendors. Adjustments will have to be made when using a paste-flux for a set of conditions it is not primarily targeted for.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 May 2015 05:36:26 GMT</pubDate>
    <dc:creator>LPP</dc:creator>
    <dc:date>2015-05-06T05:36:26Z</dc:date>
    <item>
      <title>Soldering Curve for P1020</title>
      <link>https://community.nxp.com/t5/P-Series/Soldering-Curve-for-P1020/m-p/401288#M2232</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do we have soldering recommendation documents for P1020 QorIQ device?&lt;/P&gt;&lt;P&gt;The package is &lt;SPAN class="ng-scope"&gt;&lt;A href="https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=P1020&amp;amp;cof=0&amp;amp;am=0&amp;amp;tab=Buy_Parametric_Tab&amp;amp;fromSearch=false"&gt;TEPBGA 689&lt;/A&gt;&lt;/SPAN&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A customer had issues on the device soldering on their first prototypes (proven by X-Ray).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 May 2015 12:35:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Soldering-Curve-for-P1020/m-p/401288#M2232</guid>
      <dc:creator>bfac</dc:creator>
      <dc:date>2015-05-05T12:35:54Z</dc:date>
    </item>
    <item>
      <title>Re: Soldering Curve for P1020</title>
      <link>https://community.nxp.com/t5/P-Series/Soldering-Curve-for-P1020/m-p/401289#M2233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please, refer to these documents:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/package_info/PBGAPRES.pdf" target="_blank"&gt;http://cache.freescale.com/files/32bit/doc/package_info/PBGAPRES.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3300.pdf" target="_blank"&gt;http://cache.freescale.com/files/microcontrollers/doc/app_note/AN3300.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://www.freescale.com/files/product/doc/ENV_PBFREEOV2.pdf" target="_blank"&gt;http://www.freescale.com/files/product/doc/ENV_PBFREEOV2.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note. Package Peak Temperature (PPT) profile is for determination of components Moisture Sensitivity Level (MSL) and the parts’ processability per J-STD-020. PPT is the minimum temperature used for MSL qualification. Actual reflow temperature should not exceed this value. Optimal temperature profile depends on the solder paste and flux used. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The actual reflow profile to be used for any PCB should be available from the paste supplier as a recommended profile. Use care when looking at the paste reflow profiles supplied by paste vendors. Adjustments will have to be made when using a paste-flux for a set of conditions it is not primarily targeted for.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 May 2015 05:36:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Soldering-Curve-for-P1020/m-p/401289#M2233</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2015-05-06T05:36:26Z</dc:date>
    </item>
  </channel>
</rss>