<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Get header files into sysroot in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Get-header-files-into-sysroot/m-p/400172#M2220</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need xmlreader.h from libxml2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can build it and I get an xmlreader.h but it does not appear in the installed sysroot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do:&lt;/P&gt;&lt;P&gt;bitbake libxml2&lt;/P&gt;&lt;P&gt;bitbake fsl-toolchain&lt;/P&gt;&lt;P&gt;bitbake fsl-image-core&amp;nbsp; # it says nothing needed to be done&lt;/P&gt;&lt;P&gt;cd tmp/deploy/sdk ; ./fsl-networking-eglibc-x86_64-ppce500v2-toolchain-QorIQ-SDK-V1.7.sh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After doing that the file xmlreader.h is no where to be found in the installed directories, it is however, under ./work in a number of places and at &lt;/P&gt;&lt;P&gt;./sysroots/x86_64-linux/usr/include/libxml2/libxml/xmlreader.h&lt;/P&gt;&lt;P&gt;./sysroots/p2020rdb/usr/include/libxml2/libxml/xmlreader.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I get it installed into my sysroot when I run &lt;SPAN style="font-size: 13.3333330154419px;"&gt;./fsl-networking-eglibc-x86_64-ppce500v2-toolchain-QorIQ-SDK-V1.7.sh&amp;nbsp; ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, while I am at it, I haven't found anywhere in the Freescale documentation where it explains these kinds of sequences of steps to add new libraries, header files, etc. Any pointers to the place in the documentation should prevent some future questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 04 May 2015 20:42:09 GMT</pubDate>
    <dc:creator>kevindankwardt</dc:creator>
    <dc:date>2015-05-04T20:42:09Z</dc:date>
    <item>
      <title>Get header files into sysroot</title>
      <link>https://community.nxp.com/t5/P-Series/Get-header-files-into-sysroot/m-p/400172#M2220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I need xmlreader.h from libxml2.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can build it and I get an xmlreader.h but it does not appear in the installed sysroot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I do:&lt;/P&gt;&lt;P&gt;bitbake libxml2&lt;/P&gt;&lt;P&gt;bitbake fsl-toolchain&lt;/P&gt;&lt;P&gt;bitbake fsl-image-core&amp;nbsp; # it says nothing needed to be done&lt;/P&gt;&lt;P&gt;cd tmp/deploy/sdk ; ./fsl-networking-eglibc-x86_64-ppce500v2-toolchain-QorIQ-SDK-V1.7.sh&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After doing that the file xmlreader.h is no where to be found in the installed directories, it is however, under ./work in a number of places and at &lt;/P&gt;&lt;P&gt;./sysroots/x86_64-linux/usr/include/libxml2/libxml/xmlreader.h&lt;/P&gt;&lt;P&gt;./sysroots/p2020rdb/usr/include/libxml2/libxml/xmlreader.h&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I get it installed into my sysroot when I run &lt;SPAN style="font-size: 13.3333330154419px;"&gt;./fsl-networking-eglibc-x86_64-ppce500v2-toolchain-QorIQ-SDK-V1.7.sh&amp;nbsp; ?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, while I am at it, I haven't found anywhere in the Freescale documentation where it explains these kinds of sequences of steps to add new libraries, header files, etc. Any pointers to the place in the documentation should prevent some future questions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks a lot,&lt;/P&gt;&lt;P&gt;Kevin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 May 2015 20:42:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Get-header-files-into-sysroot/m-p/400172#M2220</guid>
      <dc:creator>kevindankwardt</dc:creator>
      <dc:date>2015-05-04T20:42:09Z</dc:date>
    </item>
  </channel>
</rss>