<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: QoriQ DDR controller input AC timing</title>
    <link>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227633#M222</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am afraid tCISKEW is the only requirement for DQ/DQS input, setup and hold time are due to DQS to DQ skew.&lt;/P&gt;&lt;P&gt;CPO auto-calibration adjusts the time when the the DDR controller expects DQS preamble from the SDRAM. MCK does not matter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Mar 2013 07:23:25 GMT</pubDate>
    <dc:creator>lunminliang</dc:creator>
    <dc:date>2013-03-18T07:23:25Z</dc:date>
    <item>
      <title>QoriQ DDR controller input AC timing</title>
      <link>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227632#M221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the P1020 datasheets, the only AC parameter regarding the input timings is tDISKEW (and tCISKEW which is almost the same).&lt;/P&gt;&lt;P&gt;This parameter gives the amount of skew consumed by the controller between MDQS and MDQ/MECC.&lt;/P&gt;&lt;P&gt;It says this value should be substracted from the total timing budget. However, don't we need the input setup and hold time to&lt;/P&gt;&lt;P&gt;determine the timing budget at the controller input ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find any information about the timing relationship between MCK and DQS (like tDQSS and tDQSCK on the memory side).&lt;/P&gt;&lt;P&gt;Is this something we don't need to know ? Am I missing something ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Franck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Mar 2013 22:41:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227632#M221</guid>
      <dc:creator>fjullien</dc:creator>
      <dc:date>2013-03-15T22:41:05Z</dc:date>
    </item>
    <item>
      <title>Re: QoriQ DDR controller input AC timing</title>
      <link>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227633#M222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am afraid tCISKEW is the only requirement for DQ/DQS input, setup and hold time are due to DQS to DQ skew.&lt;/P&gt;&lt;P&gt;CPO auto-calibration adjusts the time when the the DDR controller expects DQS preamble from the SDRAM. MCK does not matter.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 07:23:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227633#M222</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2013-03-18T07:23:25Z</dc:date>
    </item>
    <item>
      <title>Re: QoriQ DDR controller input AC timing</title>
      <link>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227634#M223</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for those informations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Franck.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Mar 2013 09:47:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/QoriQ-DDR-controller-input-AC-timing/m-p/227634#M223</guid>
      <dc:creator>fjullien</dc:creator>
      <dc:date>2013-03-18T09:47:42Z</dc:date>
    </item>
  </channel>
</rss>