<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 file system in qorIQ processors</title>
    <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396220#M2184</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have Freescale Linux SDK v1.8 for QorIQ Processors that I am using to compile source images for p5040ds development system.&lt;/P&gt;&lt;P&gt;I want to create&amp;nbsp; root file system image (ramisk)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;document says to use following commands.&lt;/P&gt;&lt;P&gt; bitbake &amp;lt;image-target&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is image-target here ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Oct 2015 05:22:54 GMT</pubDate>
    <dc:creator>saurabhagarwal</dc:creator>
    <dc:date>2015-10-14T05:22:54Z</dc:date>
    <item>
      <title>file system in qorIQ processors</title>
      <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396220#M2184</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have Freescale Linux SDK v1.8 for QorIQ Processors that I am using to compile source images for p5040ds development system.&lt;/P&gt;&lt;P&gt;I want to create&amp;nbsp; root file system image (ramisk)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;document says to use following commands.&lt;/P&gt;&lt;P&gt; bitbake &amp;lt;image-target&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;what is image-target here ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 05:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396220#M2184</guid>
      <dc:creator>saurabhagarwal</dc:creator>
      <dc:date>2015-10-14T05:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: file system in qorIQ processors</title>
      <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396221#M2185</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;saurabh agarwal,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;fsl-image-minimal: A Barebones Starting Point for Products.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt; &lt;/SPAN&gt;It contains a small file set that allows Linux to boot and little else. It does not contain Freescale special SDK packages such as USDPAA, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-image-flash: A Small Flash Image for Managing Disks and Larger Images.&lt;/P&gt;&lt;P&gt;This is a small image that Freescale preprograms into the flash on development boards. It does not contain Freescale special SDK packages such as USDPAA, etc. On many boards, the image is stored in a NOR flash and is loaded into a RAM disk when Linux boots.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-image-full: A Full-Featured Image.&lt;/P&gt;&lt;P&gt;This is a large image that contains many standard Linux commands and features including native (target-resident) versions of the GNU tools including gcc and gdb. It contains all of the special Freescale SDK packages such as USDPAA, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-image-core: A Small Image with Freescale-Specific Packages Present&lt;/P&gt;&lt;P&gt;This is a small image somewhat like “fsl-image-minimal” except It contains all of the Freescale-specific SDK packages such as USDPAA, etc.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fsl-image-virt: An image for KVM deployment&lt;/P&gt;&lt;P&gt;This is an image which contains the specific packages needed to enable virtualization.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Users often use "bitbake fsl-image-core" for common usage.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 05:51:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396221#M2185</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2015-10-14T05:51:32Z</dc:date>
    </item>
    <item>
      <title>Re: file system in qorIQ processors</title>
      <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396222#M2186</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;i have some further queries.&lt;/P&gt;&lt;P&gt;I did run this command. Where can i find created image ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was reading FAQ about adding pre built binaries in file system. It says to rebuild file system run this command. &lt;/P&gt;&lt;P&gt;$ bitbake &amp;lt;rootfs-target&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is rootfs-target same as image-target ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 05:57:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396222#M2186</guid>
      <dc:creator>saurabhagarwal</dc:creator>
      <dc:date>2015-10-14T05:57:40Z</dc:date>
    </item>
    <item>
      <title>Re: file system in qorIQ processors</title>
      <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396223#M2187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please find images in the folder build_&amp;lt;platform&amp;gt;_release/tmp/deploy/images/.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 05:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396223#M2187</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2015-10-14T05:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: file system in qorIQ processors</title>
      <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396224#M2188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Yiping, &lt;/P&gt;&lt;P&gt;please also check my updated query.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 06:04:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396224#M2188</guid>
      <dc:creator>saurabhagarwal</dc:creator>
      <dc:date>2015-10-14T06:04:32Z</dc:date>
    </item>
    <item>
      <title>Re: file system in qorIQ processors</title>
      <link>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396225#M2189</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, "rootfs-target" is what I mentioned previously.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Adding pre-built binaries is done through package "merge-files", this package is included in these type rootfs images by default except fsl-image-minimal.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I you want to use add pre-built binaries in the minimal image, please also add "merge-files" in the variable IMAGE_INSTALL in meta-fsl-networking/images/fsl-image-minimal.bb.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Oct 2015 06:18:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/file-system-in-qorIQ-processors/m-p/396225#M2189</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2015-10-14T06:18:25Z</dc:date>
    </item>
  </channel>
</rss>