<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic ddr clock configuration through synchronous mode from external oscillator not from CPU in u-boot in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392970#M2166</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are having a P1021 based custom board, in which the clock input to DDR is through ddr synchronous mode from external oscillator not from CPU, i want to support this in U-boot.&lt;/P&gt;&lt;P&gt;I am not getting a clue where to make this change in u-boot so that it supports DDR clocking from external oscillator. Can some body please point me out on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shubha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 04:39:59 GMT</pubDate>
    <dc:creator>shubhasingh</dc:creator>
    <dc:date>2015-07-29T04:39:59Z</dc:date>
    <item>
      <title>ddr clock configuration through synchronous mode from external oscillator not from CPU in u-boot</title>
      <link>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392970#M2166</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are having a P1021 based custom board, in which the clock input to DDR is through ddr synchronous mode from external oscillator not from CPU, i want to support this in U-boot.&lt;/P&gt;&lt;P&gt;I am not getting a clue where to make this change in u-boot so that it supports DDR clocking from external oscillator. Can some body please point me out on this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Shubha&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 04:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392970#M2166</guid>
      <dc:creator>shubhasingh</dc:creator>
      <dc:date>2015-07-29T04:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: ddr clock configuration through synchronous mode from external oscillator not from CPU in u-boot</title>
      <link>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392971#M2167</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Clocking mode of the DDR is set on the board level, u-boot does not require any special change. Specifically the user should set proper 'cfg_ddr_pll[0:2]' POR configuration field in accordance with the input clock source (frequency), see section 4.5.3.2 of the Ref Manual for details.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 14:34:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392971#M2167</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-07-30T14:34:43Z</dc:date>
    </item>
    <item>
      <title>Re: ddr clock configuration through synchronous mode from external oscillator not from CPU in u-boot</title>
      <link>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392972#M2168</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Aug 2015 10:04:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/ddr-clock-configuration-through-synchronous-mode-from-external/m-p/392972#M2168</guid>
      <dc:creator>shubhasingh</dc:creator>
      <dc:date>2015-08-05T10:04:38Z</dc:date>
    </item>
  </channel>
</rss>