<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: freezing at kmem_cache_init when boot linux</title>
    <link>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388517#M2117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Use an external debugger to determine the PC, LR, etc. where the CPU is stuck.&amp;nbsp; Also double check that DDR has been configured correctly including timings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Dec 2014 04:14:35 GMT</pubDate>
    <dc:creator>scottwood</dc:creator>
    <dc:date>2014-12-04T04:14:35Z</dc:date>
    <item>
      <title>freezing at kmem_cache_init when boot linux</title>
      <link>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388516#M2116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;STRONG&gt;Hello&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I am not good at english.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I have a problem with booting.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I am&amp;nbsp; using p1011 cpu.&amp;nbsp; &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;console print kmem_cache_init and freeze &lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 03000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-3.12.19-rt30-QorIQ-SDK-V1.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Created:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2014-12-03&amp;nbsp;&amp;nbsp; 6:46:34 UTC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; PowerPC Linux Kernel Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 4114839 Bytes = 3.9 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Loading init Ramdisk from Legacy Image at 04000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; fsl-image-minimal-p1020rdb-20141&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Created:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2014-10-10&amp;nbsp;&amp;nbsp; 1:58:10 UTC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; PowerPC Linux RAMDisk Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 2962290 Bytes = 2.8 MiB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 05000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0x5000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Uncompressing Kernel Image ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Ramdisk to 1fb19000, end 1fdec372 ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Device Tree to 03ffa000, end 03fffb05 ... OK&lt;/P&gt;&lt;P&gt;setup_arch: bootmem&lt;/P&gt;&lt;P&gt;mpc85xx_rdb_setup_arch()&lt;/P&gt;&lt;P&gt;mpc85xx_qe_init: Could not find Quicc Engine node&lt;/P&gt;&lt;P&gt;MPC85xx RDB board from Freescale Semiconductor&lt;/P&gt;&lt;P&gt;arch: exit&lt;/P&gt;&lt;P&gt;Top of RAM: 0x20000000, Total RAM: 0x20000000&lt;/P&gt;&lt;P&gt;Memory hole size: 0MB&lt;/P&gt;&lt;P&gt;Zone ranges:&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [mem 0x00000000-0x1fffffff]&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal&amp;nbsp;&amp;nbsp; empty&lt;/P&gt;&lt;P&gt;&amp;nbsp; HighMem&amp;nbsp; empty&lt;/P&gt;&lt;P&gt;Movable zone start for each node&lt;/P&gt;&lt;P&gt;Early memory node ranges&lt;/P&gt;&lt;P&gt;&amp;nbsp; node&amp;nbsp;&amp;nbsp; 0: [mem 0x00000000-0x1fffffff]&lt;/P&gt;&lt;P&gt;On node 0 totalpages: 131072&lt;/P&gt;&lt;P&gt;free_area_init_node: node 0, pgdat c08038d4, node_mem_map c0942000&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA zone: 1024 pages used for memmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA zone: 0 pages reserved&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA zone: 131072 pages, LIFO batch:31&lt;/P&gt;&lt;P&gt;MMU: Allocated 1088 bytes of context maps for 255 contexts&lt;/P&gt;&lt;P&gt;pcpu-alloc: s0 r0 d32768 u32768 alloc=1*32768&lt;/P&gt;&lt;P&gt;pcpu-alloc: [0] 0&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 130048&lt;/P&gt;&lt;P&gt;Kernel command line: root=/dev/ram0 rw ramdisk_size=30000 mem=512M console=ttyS0,115200n8&lt;/P&gt;&lt;P&gt;PID hash table entries: 2048 (order: 1, 8192 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)&lt;/P&gt;&lt;P&gt;Sorting __ex_table...&lt;/P&gt;&lt;P&gt;Memory: 524016K/524288K available (5904K kernel code, 316K rwdata, 1808K rodata, 228K init, 1196K bss, 272K reserved, 0K highmem)&lt;/P&gt;&lt;P&gt;Kernel virtual memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xfffcf000..0xfffff000&amp;nbsp; : fixmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xff800000..0xffc00000&amp;nbsp; : highmem PTEs&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xff7fd000..0xff800000&amp;nbsp; : early ioremap&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xe1000000..0xff7fd000&amp;nbsp; : vmalloc &amp;amp; ioremap&lt;/P&gt;&lt;P&gt;kmem_cache_init&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;what should I do to solve this problem?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;thanks.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ps. If I change mem=512M to mem=128M&amp;nbsp; then it show more progress. &lt;BR /&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Dec 2014 08:31:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388516#M2116</guid>
      <dc:creator>kangdokhui</dc:creator>
      <dc:date>2014-12-03T08:31:48Z</dc:date>
    </item>
    <item>
      <title>Re: freezing at kmem_cache_init when boot linux</title>
      <link>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388517#M2117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Use an external debugger to determine the PC, LR, etc. where the CPU is stuck.&amp;nbsp; Also double check that DDR has been configured correctly including timings.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2014 04:14:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388517#M2117</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2014-12-04T04:14:35Z</dc:date>
    </item>
    <item>
      <title>Re: freezing at kmem_cache_init when boot linux</title>
      <link>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388518#M2118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you. &lt;/P&gt;&lt;P&gt;it was DDR setting problem. &lt;/P&gt;&lt;P&gt;I didn`t set correctly ddr configuration in u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now it works well. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Dec 2014 04:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/freezing-at-kmem-cache-init-when-boot-linux/m-p/388518#M2118</guid>
      <dc:creator>kangdokhui</dc:creator>
      <dc:date>2014-12-04T04:49:21Z</dc:date>
    </item>
  </channel>
</rss>