<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックNexus debug interface</title>
    <link>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388510#M2113</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any information available (e.g. application note / white paper) to have an example for the configuration of the various debug units in P5020?&lt;/P&gt;&lt;P&gt;I am trying to set up the device to output some information on the Nexus Aurora IF in order to monitor process resources (used corenet bandwith, ...).&lt;/P&gt;&lt;P&gt;Currently I am using a P5020DS for my tests.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 16 Mar 2015 15:24:33 GMT</pubDate>
    <dc:creator>maxgapp</dc:creator>
    <dc:date>2015-03-16T15:24:33Z</dc:date>
    <item>
      <title>Nexus debug interface</title>
      <link>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388510#M2113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any information available (e.g. application note / white paper) to have an example for the configuration of the various debug units in P5020?&lt;/P&gt;&lt;P&gt;I am trying to set up the device to output some information on the Nexus Aurora IF in order to monitor process resources (used corenet bandwith, ...).&lt;/P&gt;&lt;P&gt;Currently I am using a P5020DS for my tests.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Mar 2015 15:24:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388510#M2113</guid>
      <dc:creator>maxgapp</dc:creator>
      <dc:date>2015-03-16T15:24:33Z</dc:date>
    </item>
    <item>
      <title>Re: Nexus debug interface</title>
      <link>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388511#M2114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You may refer to the one in CodeWarrior installation directory as below:&lt;/P&gt;&lt;P&gt;C:\Freescale\CW_PA_v10.4.0\PA\CodeWarrior_Examples\Bareboard_Examples\e500mcPerformanceMonitor_eabi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this what you want?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2015 05:38:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388511#M2114</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-03-19T05:38:37Z</dc:date>
    </item>
    <item>
      <title>Re: Nexus debug interface</title>
      <link>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388512#M2115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;thank you for your advice. I am currently not using CodeWarrior, so I would have to download it first to have a look on the file you mentioned.&lt;/P&gt;&lt;P&gt;What I would like to do is using the Aurora serial debug interface to supply an external monitor with various information upon internal processing without the need to instrument the software running.&lt;/P&gt;&lt;P&gt;I am using a Lauterbach debugger currently, but I would like to have some examples on how the Hypervisor could set up the Nexus in order to send the information (trace, watchpoints, ...) on the Aurora so I could analyze it by means of a monitoring device (e.g. FPGA).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Max&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2015 10:32:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Nexus-debug-interface/m-p/388512#M2115</guid>
      <dc:creator>maxgapp</dc:creator>
      <dc:date>2015-03-19T10:32:16Z</dc:date>
    </item>
  </channel>
</rss>