<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P2020 Linux crash while booting</title>
    <link>https://community.nxp.com/t5/P-Series/P2020-Linux-crash-while-booting/m-p/386336#M2083</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You're using very old code.&amp;nbsp; Please try with a newer QorIQ SDK (v1.7) or with recent a upstream kernel and U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also double check that DDR timings and other things are correct for this board.&amp;nbsp; Don't just build for some random evaluation board -- especially a different one than the custom board was based on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Apr 2015 21:40:20 GMT</pubDate>
    <dc:creator>scottwood</dc:creator>
    <dc:date>2015-04-09T21:40:20Z</dc:date>
    <item>
      <title>P2020 Linux crash while booting</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-Linux-crash-while-booting/m-p/386335#M2082</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I got linux crash while kernel booting，the board is&amp;nbsp; custom according to P2020DS,&amp;nbsp; I used LTIB to compile the u-boot, uImage and rootFS according to P2020RDB.Thanks.&lt;/P&gt;&lt;P&gt;------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;## Booting kernel from Legacy Image at 01000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; Linux-2.6.32.13&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Created:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2015-04-08&amp;nbsp;&amp;nbsp; 8:38:29 UTC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; PowerPC Linux Kernel Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 1933527 Bytes =&amp;nbsp; 1.8 MB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Loading init Ramdisk from Legacy Image at 02000000 ...&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Name:&amp;nbsp;&amp;nbsp; uboot ext2 ramdisk rootfs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Created:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2015-04-08&amp;nbsp;&amp;nbsp; 1:33:10 UTC&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Image Type:&amp;nbsp;&amp;nbsp; PowerPC Linux RAMDisk Image (gzip compressed)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Data Size:&amp;nbsp;&amp;nbsp;&amp;nbsp; 6496718 Bytes =&amp;nbsp; 6.2 MB&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Load Address: 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Entry Point:&amp;nbsp; 00000000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Verifying Checksum ... OK&lt;/P&gt;&lt;P&gt;## Flattened Device Tree blob at 00c00000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Booting using the fdt blob at 0xc00000&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Uncompressing Kernel Image ... OK&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; Loading Ramdisk to 2f9cd000, end 2ffff1ce ... OK&lt;/P&gt;&lt;P&gt;Unable to update property :mac-address, err=FDT_ERR_BADPATH&lt;/P&gt;&lt;P&gt;Unable to update property :local-mac-address, err=FDT_ERR_BADPATH&lt;/P&gt;&lt;P&gt;WARNING: could not find 1588 compatible node fsl,gianfar-ptp-timer: FDT_ERR_NOTFOUND.&lt;/P&gt;&lt;P&gt;Using P2020 RDB machine description&lt;/P&gt;&lt;P&gt;Only using first contiguous memory region&lt;/P&gt;&lt;P&gt;Memory CAM mapping: 256/256/256 Mb, residual: 1280Mb&lt;/P&gt;&lt;P&gt;Linux version 2.6.32.13 (wanrenyong@localhost.localdomain) (gcc version 4.3.2 (GCC) ) #27 SMP Wed Apr 8 16:38:27 CST 2015&lt;/P&gt;&lt;P&gt;Found initrd at 0xef9cd000:0xeffff1ce&lt;/P&gt;&lt;P&gt;CPU maps initialized for 1 thread per core&lt;/P&gt;&lt;P&gt;bootconsole [udbg0] enabled&lt;/P&gt;&lt;P&gt;setup_arch: bootmem&lt;/P&gt;&lt;P&gt;mpc85xx_rdb_setup_arch()&lt;/P&gt;&lt;P&gt;MPC85xx RDB board from Freescale Semiconductor&lt;/P&gt;&lt;P&gt;arch: exit&lt;/P&gt;&lt;P&gt;Zone PFN ranges:&lt;/P&gt;&lt;P&gt;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000000 -&amp;gt; 0x00030000&lt;/P&gt;&lt;P&gt;&amp;nbsp; Normal&amp;nbsp;&amp;nbsp; 0x00030000 -&amp;gt; 0x00030000&lt;/P&gt;&lt;P&gt;&amp;nbsp; HighMem&amp;nbsp; 0x00030000 -&amp;gt; 0x00080000&lt;/P&gt;&lt;P&gt;Movable zone start PFN for each node&lt;/P&gt;&lt;P&gt;early_node_map[1] active PFN ranges&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0: 0x00000000 -&amp;gt; 0x00080000&lt;/P&gt;&lt;P&gt;MMU: Allocated 1088 bytes of context maps for 255 contexts&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 8 pages/cpu @c1c13000 s12072 r8192 d12504 u65536&lt;/P&gt;&lt;P&gt;pcpu-alloc: s12072 r8192 d12504 u65536 alloc=16*4096&lt;/P&gt;&lt;P&gt;pcpu-alloc: [0] 0 [0] 1 &lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 520192&lt;/P&gt;&lt;P&gt;Kernel command line: root=/dev/ram rw console=ttyS0,115200 ramdisk_size=200000&lt;/P&gt;&lt;P&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Memory: 2068076k/2097152k available (4024k kernel code, 28204k reserved, 196k data, 240k bss, 216k init)&lt;/P&gt;&lt;P&gt;Kernel virtual memory layout:&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xfffe0000..0xfffff000&amp;nbsp; : fixmap&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xff800000..0xffc00000&amp;nbsp; : highmem PTEs&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xff7fe000..0xff800000&amp;nbsp; : early ioremap&lt;/P&gt;&lt;P&gt;&amp;nbsp; * 0xf1000000..0xff7fe000&amp;nbsp; : vmalloc &amp;amp; ioremap&lt;/P&gt;&lt;P&gt;SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1&lt;/P&gt;&lt;P&gt;Hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;NR_IRQS:512&lt;/P&gt;&lt;P&gt;mpic: Setting up MPIC " OpenPIC&amp;nbsp; " version 1.2 at ffe40000, max 2 CPUs&lt;/P&gt;&lt;P&gt;mpic: ISU size: 256, shift: 8, mask: ff&lt;/P&gt;&lt;P&gt;mpic: Initializing for 256 sources&lt;/P&gt;&lt;P&gt;clocksource: timebase mult[5000000] shift[22] registered&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x25&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;ftrace: allocating 9366 entries in 28 pages&lt;/P&gt;&lt;P&gt;mpic: requesting IPIs ... &lt;/P&gt;&lt;P&gt;Processor 1 found.&lt;/P&gt;&lt;P&gt;Brought up 2 CPUs&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;Switching to clocksource timebase&lt;/P&gt;&lt;P&gt;Trying to unpack rootfs image as initramfs...&lt;/P&gt;&lt;P&gt;rootfs image is not initramfs (no cpio magic); looks like an initrd&lt;/P&gt;&lt;P&gt;Freeing initrd memory: 6344k freed&lt;/P&gt;&lt;P&gt;------------[ cut here ]------------&lt;/P&gt;&lt;P&gt;kernel BUG at mm/vmscan.c:2453!&lt;/P&gt;&lt;P&gt;Oops: Exception in kernel mode, sig: 5 [#1]&lt;/P&gt;&lt;P&gt;SMP NR_CPUS=2 P2020 RDB&lt;/P&gt;&lt;P&gt;Modules linked in:&lt;/P&gt;&lt;P&gt;NIP: c00c2ec4 LR: c00c2ea0 CTR: c0041460&lt;/P&gt;&lt;P&gt;REGS: ef455eb0 TRAP: 0700&amp;nbsp;&amp;nbsp; Not tainted&amp;nbsp; (2.6.32.13)&lt;/P&gt;&lt;P&gt;MSR: 00029000 &amp;lt;EE,ME,CE&amp;gt;&amp;nbsp; CR: 22244044&amp;nbsp; XER: 20000000&lt;/P&gt;&lt;P&gt;TASK = ef458000[1] 'swapper' THREAD: ef454000 CPU: 0&lt;/P&gt;&lt;P&gt;GPR00: 00000001 ef455f60 ef458000 fffffdff ef4584f0 00000000 00000000 00000001 &lt;/P&gt;&lt;P&gt;GPR08: ef454040 c0420000 c041d9c0 ef455f60 42244048 2cdb20e0 7ff90100 00000000 &lt;/P&gt;&lt;P&gt;GPR16: 00000000 7ff8405c 7ff8405c 7ffb1268 00000000 00000000 00000000 00000000 &lt;/P&gt;&lt;P&gt;GPR24: c03e0000 00000000 c03c86c8 c0420000 00000000 c04060a0 fffffdff ef455f60 &lt;/P&gt;&lt;P&gt;NIP [c00c2ec4] kswapd_run+0x80/0xc4&lt;/P&gt;&lt;P&gt;LR [c00c2ea0] kswapd_run+0x5c/0xc4&lt;/P&gt;&lt;P&gt;Call Trace:&lt;/P&gt;&lt;P&gt;[ef455f60] [c00c2ea0] kswapd_run+0x5c/0xc4 (unreliable)&lt;/P&gt;&lt;P&gt;[ef455f80] [c03c86e8] kswapd_init+0x20/0x3c&lt;/P&gt;&lt;P&gt;[ef455f90] [c0001dd8] do_one_initcall+0x4c/0x224&lt;/P&gt;&lt;P&gt;[ef455fc0] [c03b8418] kernel_init+0x190/0x204&lt;/P&gt;&lt;P&gt;[ef455ff0] [c0011b18] kernel_thread+0x4c/0x68&lt;/P&gt;&lt;P&gt;Instruction dump:&lt;/P&gt;&lt;P&gt;7f86e378 4cc63182 4bfaba99 3800f000 7f830040 7c7e1b78 409d0038 3d20c042 &lt;/P&gt;&lt;P&gt;907d0e54 8009dbe0 7c000034 5400d97e &amp;lt;0f000000&amp;gt; 3c60c037 7f84e378 386397ec &lt;/P&gt;&lt;P&gt;---[ end trace 31fd0ba7d8756001 ]---&lt;/P&gt;&lt;P&gt;Kernel panic - not syncing: Attempted to kill init!&lt;/P&gt;&lt;P&gt;Call Trace:&lt;/P&gt;&lt;P&gt;[ef455c60] [c000805c] show_stack+0x70/0x1e0 (unreliable)&lt;/P&gt;&lt;P&gt;[ef455cb0] [c030f05c] dump_stack+0x2c/0x44&lt;/P&gt;&lt;P&gt;[ef455cc0] [c030f114] panic+0xa0/0x190&lt;/P&gt;&lt;P&gt;[ef455d10] [c0050970] do_exit+0x508/0x668&lt;/P&gt;&lt;P&gt;[ef455d60] [c000edb0] kernel_bad_stack+0x0/0x68&lt;/P&gt;&lt;P&gt;[ef455d90] [c000f0a0] _exception+0x104/0x1b8&lt;/P&gt;&lt;P&gt;[ef455e80] [c000f788] program_check_exception+0xa4/0x5f0&lt;/P&gt;&lt;P&gt;[ef455ea0] [c00123b4] ret_from_except_full+0x0/0x4c&lt;/P&gt;&lt;P&gt;[ef455f60] [c00c2ea0] kswapd_run+0x5c/0xc4&lt;/P&gt;&lt;P&gt;[ef455f80] [c03c86e8] kswapd_init+0x20/0x3c&lt;/P&gt;&lt;P&gt;[ef455f90] [c0001dd8] do_one_initcall+0x4c/0x224&lt;/P&gt;&lt;P&gt;[ef455fc0] [c03b8418] kernel_init+0x190/0x204&lt;/P&gt;&lt;P&gt;[ef455ff0] [c0011b18] kernel_thread+0x4c/0x68&lt;/P&gt;&lt;P&gt;Rebooting in 180 seconds..&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Apr 2015 08:55:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-Linux-crash-while-booting/m-p/386335#M2082</guid>
      <dc:creator>aonewan</dc:creator>
      <dc:date>2015-04-08T08:55:58Z</dc:date>
    </item>
    <item>
      <title>Re: P2020 Linux crash while booting</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-Linux-crash-while-booting/m-p/386336#M2083</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You're using very old code.&amp;nbsp; Please try with a newer QorIQ SDK (v1.7) or with recent a upstream kernel and U-Boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also double check that DDR timings and other things are correct for this board.&amp;nbsp; Don't just build for some random evaluation board -- especially a different one than the custom board was based on.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 21:40:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-Linux-crash-while-booting/m-p/386336#M2083</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2015-04-09T21:40:20Z</dc:date>
    </item>
  </channel>
</rss>