<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: Error building p1020rdb yocto project</title>
    <link>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384743#M2045</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Binh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tar balls "git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz" and "git2_git.am.freescale.net.gitolite.libppc.git.tar.gz" are sources where Yocto bitbake build requires.&lt;/P&gt;&lt;P&gt;If the source tar ball md5sum is same with the value in the recipe, bitbake will not do "fetch" task, so your build environment works abnormally, did you do some modifications after install the ISO? For example, modify source tar ball or do cleanall command.&lt;/P&gt;&lt;P&gt;Please check md5 values of these two source tar balls in /opt/fsl/sources folder, whether they are same with the default.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;5a297d3ed23e8c7f35ba355c4b9a309d&lt;/STRONG&gt;&amp;nbsp; sources/git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz&lt;/P&gt;&lt;P&gt;[b25805@sun QorIQ-SDK-V1.6-20140619-yocto]$ md5sum sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;bddb108e5f2c1bd61b1cee4b418a46a0&lt;/STRONG&gt;&amp;nbsp; sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, it's better to install the Cache Binary ISO along with SOURCE ISO to avoid to build everything from the scratch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Oct 2014 03:54:39 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2014-10-13T03:54:39Z</dc:date>
    <item>
      <title>Error building p1020rdb yocto project</title>
      <link>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384742#M2044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to build the following yocto image, fsl-image-full but I got this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[shadow@orcas]$ bitbake fsl-image-full&lt;/P&gt;&lt;P&gt;WARNING: Host distribution "Unknown" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.&lt;/P&gt;&lt;P&gt;Loading cache: 100% |###############################################################################################| ETA:&amp;nbsp; 00:00:00&lt;/P&gt;&lt;P&gt;Loaded 2204 entries from dependency cache.&lt;/P&gt;&lt;P&gt;NOTE: Resolving any missing task queue dependencies&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Build Configuration:&lt;/P&gt;&lt;P&gt;BB_VERSION&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "1.22.0"&lt;/P&gt;&lt;P&gt;BUILD_SYS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "x86_64-linux"&lt;/P&gt;&lt;P&gt;NATIVELSBSTRING&amp;nbsp;&amp;nbsp; = "Unknown"&lt;/P&gt;&lt;P&gt;TARGET_SYS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "powerpc-fsl-linux-gnuspe"&lt;/P&gt;&lt;P&gt;MACHINE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "p1020rdb"&lt;/P&gt;&lt;P&gt;DISTRO&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "fsl-networking"&lt;/P&gt;&lt;P&gt;DISTRO_VERSION&amp;nbsp;&amp;nbsp;&amp;nbsp; = "1.6"&lt;/P&gt;&lt;P&gt;TUNE_FEATURES&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "m32 spe ppce500v2"&lt;/P&gt;&lt;P&gt;TARGET_FPU&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "ppc-efd"&lt;/P&gt;&lt;P&gt;meta&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-yocto&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-yocto-bsp&amp;nbsp;&amp;nbsp;&amp;nbsp; = "(detachedfromfsl-sdk-v1.6):0d2ce44c2b0f8cc9699e30cca2c24655be89d58b"&lt;/P&gt;&lt;P&gt;meta-fsl-ppc&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "(detachedfromfsl-sdk-v1.6):6cf59d9de63a9fc5f8942c0d10c622898f4315ce"&lt;/P&gt;&lt;P&gt;meta-fsl-ppc-toolchain = "(detachedfromfsl-sdk-v1.6):a546e42f86e7d57de19e27907365d170b13fc18f"&lt;/P&gt;&lt;P&gt;meta-fsl-networking &lt;/P&gt;&lt;P&gt;meta-fsl-networking = "(detachedfrom8dec9c6):8dec9c690188cce5305ef5055f91e5cfa35c63f4"&lt;/P&gt;&lt;P&gt;meta-virtualization &lt;/P&gt;&lt;P&gt;meta-virtualization = "(detachedfromfsl-sdk-v1.6):8044073f63a0d99541a43ac5f2f6d789f94c7c7c"&lt;/P&gt;&lt;P&gt;meta-oe&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-networking&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-webserver&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-ruby&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-filesystems&amp;nbsp; = "(detachedfromfsl-sdk-v1.6):b86007f742a1b829ccc8d76e485bb3f789cefaa4"&lt;/P&gt;&lt;P&gt;meta-java&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = "(detachedfromfsl-sdk-v1.6):d01f7d39e513790ddce20e6724723722119a3700"&lt;/P&gt;&lt;P&gt;meta-openstack&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;meta-openstack-compute-deploy &lt;/P&gt;&lt;P&gt;meta-openstack-controller-deploy &lt;/P&gt;&lt;P&gt;meta-openstack-qemu = "(detachedfromfsl-sdk-v1.6):f627404399a134672e0b5e26a0d9b794a6f8adf4"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: Preparing runqueue&lt;/P&gt;&lt;P&gt;NOTE: Executing SetScene Tasks&lt;/P&gt;&lt;P&gt;NOTE: Executing RunQueue Tasks&lt;/P&gt;&lt;P&gt;WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/sdk/hyperrelay.git, attempting MIRRORS if available&lt;/P&gt;&lt;P&gt;WARNING: Failed to fetch URL git://git.am.freescale.net/gitolite/libppc.git, attempting MIRRORS if available&lt;/P&gt;&lt;P&gt;ERROR: Fetcher failure: Fetch command failed with exit code 128, output:&lt;/P&gt;&lt;P&gt;Cloning into bare repository '/opt/fsl/yocto/build_p1020rdb_release/../sources/git2/git.am.freescale.net.gitolite.sdk.hyperrelay.git'...&lt;/P&gt;&lt;P&gt;2014/10/09 15:21:32 socat[29235] E CONNECT git.am.freescale.net:9418: Service Unavailable&lt;/P&gt;&lt;P&gt;fatal: Could not read from remote repository.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure you have the correct access rights&lt;/P&gt;&lt;P&gt;and the repository exists.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/sdk/hyperrelay.git'. Unable to fetch URL from any source.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /opt/fsl/build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/hyperrelay/git-r0/temp/log.do_fetch.29205&lt;/P&gt;&lt;P&gt;ERROR: Task 527 (/opt/fsl/meta-fsl-networking/recipes-extended/hyperrelay/hyperrelay_git.bb, do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;ERROR: Fetcher failure: Fetch command failed with exit code 128, output:&lt;/P&gt;&lt;P&gt;Cloning into bare repository '/opt/fsl/yocto/build_p1020rdb_release/../sources/git2/git.am.freescale.net.gitolite.libppc.git'...&lt;/P&gt;&lt;P&gt;2014/10/09 15:21:32 socat[29232] E CONNECT git.am.freescale.net:9418: Service Unavailable&lt;/P&gt;&lt;P&gt;fatal: Could not read from remote repository.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure you have the correct access rights&lt;/P&gt;&lt;P&gt;and the repository exists.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: Function failed: Fetcher failure for URL: 'git://git.am.freescale.net/gitolite/libppc.git'. Unable to fetch URL from any source.&lt;/P&gt;&lt;P&gt;ERROR: Logfile of failure stored in: /opt/fsl/build_p1020rdb_release/tmp/work/ppce500v2-fsl-linux-gnuspe/libppc/git-r0/temp/log.do_fetch.29203&lt;/P&gt;&lt;P&gt;ERROR: Task 751 (/opt/fsl/meta-fsl-networking/recipes-bsp/libppc/libppc_git.bb, do_fetch) failed with exit code '1'&lt;/P&gt;&lt;P&gt;NOTE: Tasks Summary: Attempted 838 tasks of which 798 didn't need to be rerun and 2 failed.&lt;/P&gt;&lt;P&gt;Waiting for 0 running tasks to finish:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Summary: 2 tasks failed:&lt;/P&gt;&lt;P&gt;&amp;nbsp; /opt/fsl/meta-fsl-networking/recipes-extended/hyperrelay/hyperrelay_git.bb, do_fetch&lt;/P&gt;&lt;P&gt;&amp;nbsp; /opt/fsl/meta-fsl-networking/recipes-bsp/libppc/libppc_git.bb, do_fetch&lt;/P&gt;&lt;P&gt;Summary: There were 3 WARNING messages shown.&lt;/P&gt;&lt;P&gt;Summary: There were 4 ERROR messages shown, returning a non-zero exit code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The source sdk iso does not contain the souces for these packages.&lt;/P&gt;&lt;P&gt;The only file it has in the sources directory are:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz&lt;/P&gt;&lt;P&gt;git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz.done&lt;/P&gt;&lt;P&gt;git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;git2_git.am.freescale.net.gitolite.libppc.git.tar.gz.done&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is from the source sdk iso: QorIQ-SDK-V1.6-SOURCE-20140619-yocto.iso&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyone know where I can get the source to libppc and hyperrelay?&lt;/P&gt;&lt;P&gt;I believe these are the only missing packages for a successful build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- binh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Oct 2014 20:49:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384742#M2044</guid>
      <dc:creator>binh</dc:creator>
      <dc:date>2014-10-10T20:49:40Z</dc:date>
    </item>
    <item>
      <title>Re: Error building p1020rdb yocto project</title>
      <link>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384743#M2045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Binh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The tar balls "git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz" and "git2_git.am.freescale.net.gitolite.libppc.git.tar.gz" are sources where Yocto bitbake build requires.&lt;/P&gt;&lt;P&gt;If the source tar ball md5sum is same with the value in the recipe, bitbake will not do "fetch" task, so your build environment works abnormally, did you do some modifications after install the ISO? For example, modify source tar ball or do cleanall command.&lt;/P&gt;&lt;P&gt;Please check md5 values of these two source tar balls in /opt/fsl/sources folder, whether they are same with the default.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;5a297d3ed23e8c7f35ba355c4b9a309d&lt;/STRONG&gt;&amp;nbsp; sources/git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz&lt;/P&gt;&lt;P&gt;[b25805@sun QorIQ-SDK-V1.6-20140619-yocto]$ md5sum sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;bddb108e5f2c1bd61b1cee4b418a46a0&lt;/STRONG&gt;&amp;nbsp; sources/git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition, it's better to install the Cache Binary ISO along with SOURCE ISO to avoid to build everything from the scratch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Oct 2014 03:54:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384743#M2045</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-10-13T03:54:39Z</dc:date>
    </item>
    <item>
      <title>Re: Error building p1020rdb yocto project</title>
      <link>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384744#M2046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The md5sum matches:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[shadow@orcas]$ md5sum git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz&lt;/P&gt;&lt;P&gt;5a297d3ed23e8c7f35ba355c4b9a309d&amp;nbsp; git2_git.am.freescale.net.gitolite.sdk.hyperrelay.git.tar.gz&lt;/P&gt;&lt;P&gt;[shadow@orcas]$ md5sum git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;bddb108e5f2c1bd61b1cee4b418a46a0&amp;nbsp; git2_git.am.freescale.net.gitolite.libppc.git.tar.gz&lt;/P&gt;&lt;P&gt;[shadow@orcas]$&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I didn't make any changes except to local.conf. These were the steps I took:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- I untarred yocto.tar.gz&lt;/P&gt;&lt;P&gt;- source fsl-setup-poky -m p1020rdb&lt;/P&gt;&lt;P&gt;- modified local.conf&lt;/P&gt;&lt;P&gt;- bitbake fsl-image-full&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- binh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Oct 2014 14:06:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384744#M2046</guid>
      <dc:creator>binh</dc:creator>
      <dc:date>2014-10-13T14:06:43Z</dc:date>
    </item>
    <item>
      <title>Re: Error building p1020rdb yocto project</title>
      <link>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384745#M2047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Binh,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not sure where you modified local.conf file, did you modify source download dir in local.conf?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to your description, it seems that you didn't use the formal installation procedure, I wrote an application note about how to use Yocto SDK, please refer to section 1 of &lt;A href="https://community.nxp.com/docs/DOC-102509"&gt;QorIQ Linux SDK 1.6 Working With Yocto&lt;/A&gt;. Please note to install both "Source" and "Cache binary" ISOs, and use "install" script which will do necessary checking.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 03:25:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384745#M2047</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-10-16T03:25:38Z</dc:date>
    </item>
    <item>
      <title>Re: Error building p1020rdb yocto project</title>
      <link>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384746#M2048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I added this to local.conf:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;INHERIT += "rm_work"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In any case, I reinstalled using the install script and it built.&lt;/P&gt;&lt;P&gt;Now I have problems booting the image, it would kernel panic.&lt;/P&gt;&lt;P&gt;I'll start another post about that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- binh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Oct 2014 10:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-building-p1020rdb-yocto-project/m-p/384746#M2048</guid>
      <dc:creator>binh</dc:creator>
      <dc:date>2014-10-16T10:55:08Z</dc:date>
    </item>
  </channel>
</rss>