<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: CECR[RST] bit won't clear.</title>
    <link>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384564#M2042</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;QE may halt if it's clocks frequencies are out of range. Please check QE PLL and VCO frequency (and also frequencies of serial interfaces) . &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;QE may halt because of bus error (before init_tx_rx command or as the result of this command). Check SDMA Status register SDSR. If error is set, check SDTA1/SDTA2/SDTM1/SDTM2 registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;The QE never crashes!&lt;/P&gt;&lt;P&gt;- It can stop completely on SDMA faults. You should always have an error handler for this!&lt;/P&gt;&lt;P&gt;- It works with all data/parameters you give it. Wrong parameters may cause fault!&lt;/P&gt;&lt;P&gt;- MURAM Parameter overlaps cause mostly very interesting effects of highly statistical nature.&lt;/P&gt;&lt;P&gt;- Structure alignment messups are the 2nd most common problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure that QE has been running before a new command was issued? Have you try other QE protocols running (e.g. UART)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.&lt;/P&gt;&lt;P&gt;Hint. On bootup with disabled QE:&lt;/P&gt;&lt;P&gt;Set complete MURAM to some “odd” value (not zeroes!), e.g., 0x55 that can easily be identified in broken pointers or missing initializations.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Oct 2014 11:56:28 GMT</pubDate>
    <dc:creator>LPP</dc:creator>
    <dc:date>2014-10-13T11:56:28Z</dc:date>
    <item>
      <title>CECR[RST] bit won't clear.</title>
      <link>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384563#M2041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any reason why the powequicc risc processor wont clear the CECR[FLAG] bit when a command is issued?&amp;nbsp; I have issued a command and am polling on this bit for completion but it never clears.&amp;nbsp; Only a CECR[RST] =1 clears it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Oct 2014 17:47:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384563#M2041</guid>
      <dc:creator>eng5678</dc:creator>
      <dc:date>2014-10-10T17:47:04Z</dc:date>
    </item>
    <item>
      <title>Re: CECR[RST] bit won't clear.</title>
      <link>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384564#M2042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1.&lt;/P&gt;&lt;P&gt;QE may halt if it's clocks frequencies are out of range. Please check QE PLL and VCO frequency (and also frequencies of serial interfaces) . &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.&lt;/P&gt;&lt;P&gt;QE may halt because of bus error (before init_tx_rx command or as the result of this command). Check SDMA Status register SDSR. If error is set, check SDTA1/SDTA2/SDTM1/SDTM2 registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.&lt;/P&gt;&lt;P&gt;The QE never crashes!&lt;/P&gt;&lt;P&gt;- It can stop completely on SDMA faults. You should always have an error handler for this!&lt;/P&gt;&lt;P&gt;- It works with all data/parameters you give it. Wrong parameters may cause fault!&lt;/P&gt;&lt;P&gt;- MURAM Parameter overlaps cause mostly very interesting effects of highly statistical nature.&lt;/P&gt;&lt;P&gt;- Structure alignment messups are the 2nd most common problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you sure that QE has been running before a new command was issued? Have you try other QE protocols running (e.g. UART)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4.&lt;/P&gt;&lt;P&gt;Hint. On bootup with disabled QE:&lt;/P&gt;&lt;P&gt;Set complete MURAM to some “odd” value (not zeroes!), e.g., 0x55 that can easily be identified in broken pointers or missing initializations.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Oct 2014 11:56:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384564#M2042</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2014-10-13T11:56:28Z</dc:date>
    </item>
    <item>
      <title>Re: CECR[RST] bit won't clear.</title>
      <link>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384565#M2043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The root problem for this question was corrected by loading microcode into the quicc engine.&amp;nbsp; Our experience has been primarily with Powerquicc 2 CPMs (MPC82XX) which have the microcode preloaded.&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Nov 2014 20:41:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/CECR-RST-bit-won-t-clear/m-p/384565#M2043</guid>
      <dc:creator>eng5678</dc:creator>
      <dc:date>2014-11-13T20:41:29Z</dc:date>
    </item>
  </channel>
</rss>