<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 P1021 NAND Flash Interface</title>
    <link>https://community.nxp.com/t5/P-Series/P1021-NAND-Flash-Interface/m-p/382969#M2015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to understand the maximum size of NAND Flash that can be interfaced with P1021. As per the reference manual there are two kinds of page size supported &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Small page NAND Flash (528 Bytes - 512 bytes as main region and 16 bytes as spare region)&lt;/LI&gt;&lt;LI&gt;Large page NAND Flash (2112 bytes - 2048 bytes as main region and 64 bytes as spare region)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I intend to connect 1GB NAND Flash but it has&amp;nbsp; page size of 4320 bytes (4096 as main region + 224 bytes as spare region). Please let me know if it is possible to interface chips which have larger page size then the one Ref Manual mentions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 02 Jan 2015 08:22:48 GMT</pubDate>
    <dc:creator>rajniks</dc:creator>
    <dc:date>2015-01-02T08:22:48Z</dc:date>
    <item>
      <title>P1021 NAND Flash Interface</title>
      <link>https://community.nxp.com/t5/P-Series/P1021-NAND-Flash-Interface/m-p/382969#M2015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to understand the maximum size of NAND Flash that can be interfaced with P1021. As per the reference manual there are two kinds of page size supported &lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Small page NAND Flash (528 Bytes - 512 bytes as main region and 16 bytes as spare region)&lt;/LI&gt;&lt;LI&gt;Large page NAND Flash (2112 bytes - 2048 bytes as main region and 64 bytes as spare region)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I intend to connect 1GB NAND Flash but it has&amp;nbsp; page size of 4320 bytes (4096 as main region + 224 bytes as spare region). Please let me know if it is possible to interface chips which have larger page size then the one Ref Manual mentions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Raj&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 02 Jan 2015 08:22:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1021-NAND-Flash-Interface/m-p/382969#M2015</guid>
      <dc:creator>rajniks</dc:creator>
      <dc:date>2015-01-02T08:22:48Z</dc:date>
    </item>
    <item>
      <title>Re: P1021 NAND Flash Interface</title>
      <link>https://community.nxp.com/t5/P-Series/P1021-NAND-Flash-Interface/m-p/382970#M2016</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid not mentioning larger size in the reference manual is not support, it's not possible to interface 4K page size NAND to FCM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 04 Jan 2015 03:31:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1021-NAND-Flash-Interface/m-p/382970#M2016</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-01-04T03:31:49Z</dc:date>
    </item>
  </channel>
</rss>