<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: P1010-RDB won't boot from norflash in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/P1010-RDB-won-t-boot-from-norflash/m-p/378115#M1980</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sothavy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For P1010RDB-PA&lt;/P&gt;&lt;P&gt;• SW4[1:4] = 1111 and SW6[4] = 0 for 16-bit NOR Flash boot.&lt;/P&gt;&lt;P&gt;• SW4[1:4] = 1011 and SW6[4] = 0 for 8-bit NOR Flash boot.&lt;/P&gt;&lt;P&gt;• u-boot start address of default bank is 0xeff80000.&lt;/P&gt;&lt;P&gt;• u-boot start address of alternate bank is 0xeef80000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could use the following command to switch from NAND to NOR boot.&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c dev 0&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c mw 18 1 f1&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c mw 18 3 f0&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00011 0&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00014 2&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00015 5&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00016 3&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00017 f&lt;/P&gt;&lt;P&gt;=&amp;gt; reset&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For P1010RDB-PB&lt;/P&gt;&lt;P&gt;SW4[1:4]= 1111 and SW3[3:4]= 00 for NOR boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 05 Nov 2014 13:09:13 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2014-11-05T13:09:13Z</dc:date>
    <item>
      <title>P1010-RDB won't boot from norflash</title>
      <link>https://community.nxp.com/t5/P-Series/P1010-RDB-won-t-boot-from-norflash/m-p/378114#M1979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I can't get it to boot from norflash but it boots up fine from nandflash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I set the switches on my board to the following to get it to boot from the norflash but my console doesn't show anything.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The switches are set to the following:&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;SW4[1-4]: 1111&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;SW6[4]: 0&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;From what I can gather from the documentation, it is possible that SW6[4] is overridden by I2C1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I missing something or is it due to I2C1?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 17:16:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010-RDB-won-t-boot-from-norflash/m-p/378114#M1979</guid>
      <dc:creator>s0m31</dc:creator>
      <dc:date>2014-11-04T17:16:44Z</dc:date>
    </item>
    <item>
      <title>Re: P1010-RDB won't boot from norflash</title>
      <link>https://community.nxp.com/t5/P-Series/P1010-RDB-won-t-boot-from-norflash/m-p/378115#M1980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sothavy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For P1010RDB-PA&lt;/P&gt;&lt;P&gt;• SW4[1:4] = 1111 and SW6[4] = 0 for 16-bit NOR Flash boot.&lt;/P&gt;&lt;P&gt;• SW4[1:4] = 1011 and SW6[4] = 0 for 8-bit NOR Flash boot.&lt;/P&gt;&lt;P&gt;• u-boot start address of default bank is 0xeff80000.&lt;/P&gt;&lt;P&gt;• u-boot start address of alternate bank is 0xeef80000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could use the following command to switch from NAND to NOR boot.&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c dev 0&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c mw 18 1 f1&lt;/P&gt;&lt;P&gt;=&amp;gt; i2c mw 18 3 f0&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00011 0&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00014 2&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00015 5&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00016 3&lt;/P&gt;&lt;P&gt;=&amp;gt; mw.b ffb00017 f&lt;/P&gt;&lt;P&gt;=&amp;gt; reset&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For P1010RDB-PB&lt;/P&gt;&lt;P&gt;SW4[1:4]= 1111 and SW3[3:4]= 00 for NOR boot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 13:09:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010-RDB-won-t-boot-from-norflash/m-p/378115#M1980</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-11-05T13:09:13Z</dc:date>
    </item>
  </channel>
</rss>