<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: how to create 8 partitions using hypervisor in P4080DS</title>
    <link>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369404#M1884</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) where do I find the hv.dts file? I cannot find it in the SDK&lt;/P&gt;&lt;P&gt;You may find it in &lt;A href="https://community.nxp.com/thread/345277"&gt;Where is the hv.dts file in Freescale SDK 1.6 for P4080DS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) after I modify this hv.dts file, do I need to rebuild the image?&lt;/P&gt;&lt;P&gt;Yes, I think so. As this is only the textual representation of device trees.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3) how do I update this change, do I need to rebuild the image and flash it onto the board?&lt;/P&gt;&lt;P&gt;Yes, I thinks this depends on your deployment method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please someone else correct me if you don't think so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Mar 2015 07:40:57 GMT</pubDate>
    <dc:creator>lunminliang</dc:creator>
    <dc:date>2015-03-13T07:40:57Z</dc:date>
    <item>
      <title>how to create 8 partitions using hypervisor in P4080DS</title>
      <link>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369403#M1883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have successfully installed the hypervisor on P4080DS following the documentation. But it only shows 2 partitions, one with 7 CPU, one with 1 CPU. &lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;The project I am doing now requires me to create 8 partitions on P4080ds. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't find a documentation on how to partition the system.&amp;nbsp; I only found this by Yiping.&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-wiki-small" data-containerid="2009" data-containertype="14" data-objectid="102249" data-objecttype="102" href="https://community.freescale.com/docs/DOC-102249"&gt;https://community.freescale.com/docs/DOC-102249&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But there are a few points now very clear.&lt;/P&gt;&lt;P&gt;(1) where do I find the hv.dts file? I cannot find it in the SDK&lt;/P&gt;&lt;P&gt;(2) after I modify this hv.dts file, do I need to rebuild the image?&lt;/P&gt;&lt;P&gt;(3) how do I update this change, do I need to rebuild the image and flash it onto the board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Thank you for your help.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter Zheng Zhipeng&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2015 12:24:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369403#M1883</guid>
      <dc:creator>peterzheng</dc:creator>
      <dc:date>2015-03-09T12:24:41Z</dc:date>
    </item>
    <item>
      <title>Re: how to create 8 partitions using hypervisor in P4080DS</title>
      <link>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369404#M1884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) where do I find the hv.dts file? I cannot find it in the SDK&lt;/P&gt;&lt;P&gt;You may find it in &lt;A href="https://community.nxp.com/thread/345277"&gt;Where is the hv.dts file in Freescale SDK 1.6 for P4080DS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(2) after I modify this hv.dts file, do I need to rebuild the image?&lt;/P&gt;&lt;P&gt;Yes, I think so. As this is only the textual representation of device trees.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(3) how do I update this change, do I need to rebuild the image and flash it onto the board?&lt;/P&gt;&lt;P&gt;Yes, I thinks this depends on your deployment method.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please someone else correct me if you don't think so.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2015 07:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369404#M1884</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-03-13T07:40:57Z</dc:date>
    </item>
    <item>
      <title>Re: how to create 8 partitions using hypervisor in P4080DS</title>
      <link>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369405#M1885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lunmin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your answer. However, if I would like to partition the L3 cache of P4080DS in CodeWarrior. Do you know how to do that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, using some cache management instruction.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2015 08:01:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369405#M1885</guid>
      <dc:creator>peterzheng</dc:creator>
      <dc:date>2015-03-13T08:01:28Z</dc:date>
    </item>
    <item>
      <title>Re: how to create 8 partitions using hypervisor in P4080DS</title>
      <link>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369406#M1886</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Lunmin,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) I am unable to find the hv.dts file at the location you mentioned. Can I just use the dts file you provided in the attachment?&lt;/P&gt;&lt;P&gt;(2) After modification, should I use DTC tool to compile, can you show me the steps?&lt;/P&gt;&lt;P&gt;(3) I use TFTP to transfer deploy the image. Is it enough if I just deploy the DTB file? Or do I need to re-deploy the UImage as well?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 15 Mar 2015 07:55:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/how-to-create-8-partitions-using-hypervisor-in-P4080DS/m-p/369406#M1886</guid>
      <dc:creator>peterzheng</dc:creator>
      <dc:date>2015-03-15T07:55:08Z</dc:date>
    </item>
  </channel>
</rss>