<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Using MPIC  when CPC is set as SRAM P4080</title>
    <link>https://community.nxp.com/t5/P-Series/Using-MPIC-when-CPC-is-set-as-SRAM-P4080/m-p/363895#M1840</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPIC can be used without any relation to CPC mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 30 Oct 2014 08:52:20 GMT</pubDate>
    <dc:creator>LPP</dc:creator>
    <dc:date>2014-10-30T08:52:20Z</dc:date>
    <item>
      <title>Using MPIC  when CPC is set as SRAM P4080</title>
      <link>https://community.nxp.com/t5/P-Series/Using-MPIC-when-CPC-is-set-as-SRAM-P4080/m-p/363894#M1839</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using the CPC as SRAM, and I would like to know whether I can&amp;nbsp; use the MPIC (Multicore Programmable Interrupt Controller) while the SRAM configuration is enabled? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hymalai Bello&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 23:46:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Using-MPIC-when-CPC-is-set-as-SRAM-P4080/m-p/363894#M1839</guid>
      <dc:creator>hymalaibello</dc:creator>
      <dc:date>2014-10-29T23:46:03Z</dc:date>
    </item>
    <item>
      <title>Re: Using MPIC  when CPC is set as SRAM P4080</title>
      <link>https://community.nxp.com/t5/P-Series/Using-MPIC-when-CPC-is-set-as-SRAM-P4080/m-p/363895#M1840</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;MPIC can be used without any relation to CPC mode.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 08:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Using-MPIC-when-CPC-is-set-as-SRAM-P4080/m-p/363895#M1840</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2014-10-30T08:52:20Z</dc:date>
    </item>
  </channel>
</rss>