<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Linux booting problem in P4080 based system.</title>
    <link>https://community.nxp.com/t5/P-Series/Linux-booting-problem-in-P4080-based-system/m-p/361551#M1824</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Above kernel booting problem solved when i passed only 2GB ddr3 size in u-boot bootargs which actually has 4GB ddr3 memory. I've enabled 4GB(2GB per ddr3 controller) in u-boot with using 36-bit physical addressing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also in u-boot bootup , it says 2GB left unmapped, which later on came to know that P4080 platform specific ddr initialization is using max 2GB size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, the problem is when i don't specify 2GB bootargs memory size,here kernel is crashing giving above error message.&lt;/P&gt;&lt;P&gt;I've enabled "large physical address support" and SWIOTLB options in kernel also, still giving same error. Device tree file also using 36-bit physical addressing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything still we have to enable to use 4GB memory in Linux? Please share your ideas guys..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Amit Shah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 22 May 2015 13:44:52 GMT</pubDate>
    <dc:creator>amitshah1</dc:creator>
    <dc:date>2015-05-22T13:44:52Z</dc:date>
    <item>
      <title>Linux booting problem in P4080 based system.</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-booting-problem-in-P4080-based-system/m-p/361550#M1823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm working on P4080 based system with Linux running on it.&lt;/P&gt;&lt;P&gt;I'm facing an issue @ linux boot-up. Please share me your ideas regarding this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It comes as:&lt;/P&gt;&lt;P&gt;===================================================================================&lt;/P&gt;&lt;P&gt;Machine check in kernel mode. &lt;/P&gt;&lt;P&gt;Caused by (from MCSR=8000): Load Error Report &lt;/P&gt;&lt;P&gt;Oops: Machine check, sig: 7 [#1] &lt;/P&gt;&lt;P&gt;SMP NR_CPUS=8 CoreNet Generic &lt;/P&gt;&lt;P&gt;Modules linked in: &lt;/P&gt;&lt;P&gt;CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a #23 &lt;/P&gt;&lt;P&gt;task: ee084a30 ti: efbae000 task.ti: ee0a2000 &lt;/P&gt;&lt;P&gt;NIP: c01ef070 LR: c01ef060 CTR: 00000000 &lt;/P&gt;&lt;P&gt;REGS: efbaff10 TRAP: 0204&amp;nbsp;&amp;nbsp; Not tainted&amp;nbsp; (3.12.19-rt30-QorIQ-SDK-V1.6+gc29fe1a) &lt;/P&gt;&lt;P&gt;MSR: 00029002 &amp;lt;CE,EE,ME&amp;gt;&amp;nbsp; CR: 84844e48&amp;nbsp; XER: 00000000 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;GPR00: c01ef01c ee0a3c30 ee084a30 f1049040 c0325214 c03b9ec4 ee1d2ba0 00000fe4 &lt;/P&gt;&lt;P&gt;GPR08: 38241215 00000000 f104a278 38241215 84844e88 00000000 c00027f0 00000000 &lt;/P&gt;&lt;P&gt;GPR16: 00000000 20000000 00000000 c039222c 00500001 ed010d20 00000002 c02a230c &lt;/P&gt;&lt;P&gt;GPR24: c03b1044 c02a21f0 c0389fb8 ee2810c0 00000000 ee1d6400 00000000 f1048000 &lt;/P&gt;&lt;P&gt;NIP [c01ef070] n_tty_open+0x70/0x130 &lt;/P&gt;&lt;P&gt;LR [c01ef060] n_tty_open+0x60/0x130 &lt;/P&gt;&lt;P&gt;Call Trace: &lt;/P&gt;&lt;P&gt;[ee0a3c30] [c01ef01c] n_tty_open+0x1c/0x130 (unreliable) &lt;/P&gt;&lt;P&gt;[ee0a3c50] [c01f3c1c] tty_ldisc_open.isra.6+0x5c/0xa0 &lt;/P&gt;&lt;P&gt;[ee0a3c60] [c01f4544] tty_ldisc_setup+0x24/0xc0 &lt;/P&gt;&lt;P&gt;[ee0a3c80] [c01eb698] tty_init_dev+0xb8/0x1e0 &lt;/P&gt;&lt;P&gt;[ee0a3ca0] [c01ec3b0] tty_open+0x330/0x680 &lt;/P&gt;&lt;P&gt;[ee0a3d00] [c00eaedc] chrdev_open+0xbc/0x1c0 &lt;/P&gt;&lt;P&gt;[ee0a3d30] [c00e3dc0] do_dentry_open.isra.15+0x190/0x2b0 &lt;/P&gt;&lt;P&gt;[ee0a3d50] [c00e3f0c] finish_open+0x2c/0x60 &lt;/P&gt;&lt;P&gt;[ee0a3d60] [c00f504c] do_last.isra.47+0x3fc/0xbe0 &lt;/P&gt;&lt;P&gt;[ee0a3dd0] [c00f58e4] path_openat+0xb4/0x640 &lt;/P&gt;&lt;P&gt;[ee0a3e30] [c00f6cb0] do_filp_open+0x30/0x90 &lt;/P&gt;&lt;P&gt;[ee0a3eb0] [c00e52f8] do_sys_open+0x148/0x280 &lt;/P&gt;&lt;P&gt;[ee0a3ef0] [c03558fc] kernel_init_freeable+0x160/0x1d0 &lt;/P&gt;&lt;P&gt;[ee0a3f20] [c0002808] kernel_init+0x18/0x170 &lt;/P&gt;&lt;P&gt;[ee0a3f40] [c000fca4] ret_from_kernel_thread+0x5c/0x64 &lt;/P&gt;&lt;P&gt;Instruction dump: &lt;/P&gt;&lt;P&gt;913f0034 388451f8 4be8e5a9 3c80c032 387f2270 7fc5f378 38845214 4be8e595 &lt;/P&gt;&lt;P&gt;93fd01a0 3bc00000 93df2244 387f1040 &amp;lt;893f003d&amp;gt; 38800000 93df0004 38a00200 &lt;/P&gt;&lt;P&gt;---[ end trace 91dd2f21b34be299 ]--- &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel panic - not syncing: Attempted to kill init! exitcode=0x00000007 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rebooting in 180 seconds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;===================================================================================&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Amit Shah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 08:48:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-booting-problem-in-P4080-based-system/m-p/361550#M1823</guid>
      <dc:creator>amitshah1</dc:creator>
      <dc:date>2015-03-30T08:48:27Z</dc:date>
    </item>
    <item>
      <title>Re: Linux booting problem in P4080 based system.</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-booting-problem-in-P4080-based-system/m-p/361551#M1824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Above kernel booting problem solved when i passed only 2GB ddr3 size in u-boot bootargs which actually has 4GB ddr3 memory. I've enabled 4GB(2GB per ddr3 controller) in u-boot with using 36-bit physical addressing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also in u-boot bootup , it says 2GB left unmapped, which later on came to know that P4080 platform specific ddr initialization is using max 2GB size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But, the problem is when i don't specify 2GB bootargs memory size,here kernel is crashing giving above error message.&lt;/P&gt;&lt;P&gt;I've enabled "large physical address support" and SWIOTLB options in kernel also, still giving same error. Device tree file also using 36-bit physical addressing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything still we have to enable to use 4GB memory in Linux? Please share your ideas guys..&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Amit Shah&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 22 May 2015 13:44:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-booting-problem-in-P4080-based-system/m-p/361551#M1824</guid>
      <dc:creator>amitshah1</dc:creator>
      <dc:date>2015-05-22T13:44:52Z</dc:date>
    </item>
  </channel>
</rss>