<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: P1022 Custom board: Radeon problem</title>
    <link>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341049#M1580</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;Christian Zigotzky,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;In your Kernel configuration file, you configure the extra firmware location as the following.&lt;/P&gt;&lt;P&gt;CONFIG_EXTRA_FIRMWARE="radeon/R700_rlc.bin radeon/RV710_uvd.bin radeon/RV770_uvd.bin radeon/CYPRESS_me.bin radeon/CYPRESS_pfp.bin radeon/CYPRESS_rlc.bin radeon/CYPRESS_smc.bin radeon/CYPRESS_uvd.bin radeon/JUNIPER_me.bin radeon/JUNIPER_pfp.bin radeon/JUNIPER_rlc.bin radeon/JUNIPER_smc.bin radeon/REDWOOD_me.bin radeon/REDWOOD_pfp.bin radeon/REDWOOD_rlc.bin radeon/REDWOOD_smc.bin radeon/BTC_rlc.bin radeon/BARTS_me.bin radeon/BARTS_mc.bin radeon/BARTS_pfp.bin radeon/BARTS_smc.bin radeon/SUMO_uvd.bin radeon/CAICOS_me.bin radeon/CAICOS_mc.bin radeon/CAICOS_pfp.bin radeon/CAICOS_smc.bin radeon/TURKS_me.bin radeon/TURKS_mc.bin radeon/TURKS_pfp.bin radeon/TURKS_smc.bin radeon/CEDAR_me.bin radeon/CEDAR_pfp.bin radeon/CEDAR_rlc.bin radeon/CEDAR_smc.bin"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_EXTRA_FIRMWARE_DIR="/lib/firmware"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure the firmware is built into filesystem, and the path configured as "/lib/firmware/radeon" is correct, otherwise you need to modify Kernel configuration file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jan 2015 07:22:54 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2015-01-16T07:22:54Z</dc:date>
    <item>
      <title>P1022 Custom board: Radeon problem</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341047#M1578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I bought a P1022 custom board, last year.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Technical details:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;P1022, Version: 1.1&lt;/P&gt;&lt;P&gt;2 core e500v2 1.2GHz revision 5.1&lt;/P&gt;&lt;P&gt;4 GB DDR3 RAM&lt;/P&gt;&lt;P&gt;PCIe x4 with x16 connector&lt;/P&gt;&lt;P&gt;U-Boot 2014.04-00124-g2c02fcb (Sep 20 2014 - 11:36:22)&lt;/P&gt;&lt;P&gt;OS: Debian 7.7 PowerPC and Debian 8.0 PowerPCSPE&lt;/P&gt;&lt;P&gt;Kernel 3.8.13-rt9 (config as attachment)&lt;/P&gt;&lt;P&gt;Radeon HD5450 1GB DDR3 VRAM&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Debian 7.7 PowerPC and Debian 8.0 PowerPCSPE boot with the kernel 3.8.13-rt9 in the text mode without any problems. I can use X11 via fslfb (LCD) with the display resolution of 1024x768. But I can't use Debian with the Radeon HD5450. On U-Boot I have output with the Radeon but after the start of the Linux kernel, the screen has no output. But I saw with the serial console, that Linux booted without any problems and started gdm3 but unfortunately without screen output. I tried a lot of xorg configs and I played a lot with boot arguments for example video=radeonfb:1600x1200@60 etc but without any success. What I have to do to get X11 with the Radeon HD5450?&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337218"&gt;custom_board_3.8.13-rt9.config.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Jan 2015 20:18:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341047#M1578</guid>
      <dc:creator>ppc-fan</dc:creator>
      <dc:date>2015-01-13T20:18:12Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Custom board: Radeon problem</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341048#M1579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It doesn't look like I'm running KMS:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="plain" __jive_macro_name="code" class="_jivemacro_uid_14212397353502506 jive_text_macro jive_macro_code" jivemacro_uid="_14212397353502506" modifiedtitle="true"&gt;
&lt;P&gt;[&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 14.868]&amp;nbsp; (II)&amp;nbsp; [KMS] drm report modesetting isn't supported.&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think the firmware of my Radeon HD5450 graphics card wasn't loaded because of the 36bit addressing but it is in the kernel. Is it possible to load a Radeon firmware with a Linux kernel on a P1022 board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 12:55:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341048#M1579</guid>
      <dc:creator>ppc-fan</dc:creator>
      <dc:date>2015-01-14T12:55:19Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Custom board: Radeon problem</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341049#M1580</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;Christian Zigotzky,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG class="font-color-meta"&gt;&lt;SPAN class="replyToName"&gt;&lt;/SPAN&gt;&lt;/STRONG&gt;In your Kernel configuration file, you configure the extra firmware location as the following.&lt;/P&gt;&lt;P&gt;CONFIG_EXTRA_FIRMWARE="radeon/R700_rlc.bin radeon/RV710_uvd.bin radeon/RV770_uvd.bin radeon/CYPRESS_me.bin radeon/CYPRESS_pfp.bin radeon/CYPRESS_rlc.bin radeon/CYPRESS_smc.bin radeon/CYPRESS_uvd.bin radeon/JUNIPER_me.bin radeon/JUNIPER_pfp.bin radeon/JUNIPER_rlc.bin radeon/JUNIPER_smc.bin radeon/REDWOOD_me.bin radeon/REDWOOD_pfp.bin radeon/REDWOOD_rlc.bin radeon/REDWOOD_smc.bin radeon/BTC_rlc.bin radeon/BARTS_me.bin radeon/BARTS_mc.bin radeon/BARTS_pfp.bin radeon/BARTS_smc.bin radeon/SUMO_uvd.bin radeon/CAICOS_me.bin radeon/CAICOS_mc.bin radeon/CAICOS_pfp.bin radeon/CAICOS_smc.bin radeon/TURKS_me.bin radeon/TURKS_mc.bin radeon/TURKS_pfp.bin radeon/TURKS_smc.bin radeon/CEDAR_me.bin radeon/CEDAR_pfp.bin radeon/CEDAR_rlc.bin radeon/CEDAR_smc.bin"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CONFIG_EXTRA_FIRMWARE_DIR="/lib/firmware"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please make sure the firmware is built into filesystem, and the path configured as "/lib/firmware/radeon" is correct, otherwise you need to modify Kernel configuration file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jan 2015 07:22:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341049#M1580</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2015-01-16T07:22:54Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Custom board: Radeon problem</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341050#M1581</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yiping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your answer. The firmwares aren't the problem. They are in the kernel. I activated DRM in the kernel config. The kernel boots without any problems but if X11 starts then I get a scrambled screen. No output on the radeon or a scambled screen. Could it be that we have 36bit addressing on a 32bit CPU????? I saw a video about a P1022 board with a graphics card:&amp;nbsp; &lt;A href="http://www.freescale.com/webapp/video_vault/videoSummary.sp?code=FTF11NET_685_VID" title="http://www.freescale.com/webapp/video_vault/videoSummary.sp?code=FTF11NET_685_VID"&gt;WireSpring Digital Signage P1022 Processor - |Freescale&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Christian&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Jan 2015 08:46:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341050#M1581</guid>
      <dc:creator>ppc-fan</dc:creator>
      <dc:date>2015-01-17T08:46:40Z</dc:date>
    </item>
    <item>
      <title>Re: P1022 Custom board: Radeon problem</title>
      <link>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341051#M1582</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;At the boot time there is an error about a ring 0 test: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;radeon 0000:01:00.0: fence driver on ring 0 use gpu addr 0x0000000040000c00 and cpu addr 0xee270c00 &lt;/P&gt;&lt;P&gt;radeon 0000:01:00.0: fence driver on ring 3 use gpu addr 0x0000000040000c0c and cpu addr 0xee270c0c &lt;/P&gt;&lt;P&gt;[drm:r600_ring_test] &lt;STRONG class="moz-txt-star"&gt;&lt;SPAN class="moz-txt-tag"&gt;*&lt;/SPAN&gt;ERROR&lt;SPAN class="moz-txt-tag"&gt;*&lt;/SPAN&gt;&lt;/STRONG&gt; radeon: ring 0 test failed (scratch(0x8504)=0xCAFEDEAD). &lt;/P&gt;&lt;P&gt;radeon 0000:01:00.0: disabling GPU acceleration &lt;/P&gt;&lt;P&gt;radeon 0000:01:00.0: ee79a600 unpin not necessary &lt;/P&gt;&lt;P&gt;[drm] Radeon Display Connectors &lt;/P&gt;&lt;P&gt;[drm] radeon: power management initialized &lt;/P&gt;&lt;P&gt;radeon 0000:01:00.0: registered panic notifier&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jan 2015 10:27:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1022-Custom-board-Radeon-problem/m-p/341051#M1582</guid>
      <dc:creator>ppc-fan</dc:creator>
      <dc:date>2015-01-19T10:27:59Z</dc:date>
    </item>
  </channel>
</rss>