<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SATA init issues on P5020 with kernel 3.17-rc3 in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340310#M1569</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-Boot prints the SoC version in the boot messages.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Sep 2014 20:40:00 GMT</pubDate>
    <dc:creator>scottwood</dc:creator>
    <dc:date>2014-09-10T20:40:00Z</dc:date>
    <item>
      <title>SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340306#M1565</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Has anyone here successfully built and booted a recent kernel from mainline? I have one built, however upon boot, sata init fails. Are there any known SATA-related erratum that I should be patching for?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Sep 2014 17:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340306#M1565</guid>
      <dc:creator>RabbitHoleComp</dc:creator>
      <dc:date>2014-09-04T17:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340307#M1566</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Alex Perez,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Would you please provide your u-boot and Kernel boot log?&lt;/P&gt;&lt;P&gt;What is the revision of P5020 used? &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 10:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340307#M1566</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-09-10T10:46:46Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340308#M1567</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/yipingwang"&gt;yipingwang&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sure, I can provide a kernel boot log. The P5020 I am using is production/shipping silicon. If you can tell me how to verify (via /proc or similar mechanism) which version it is, I'll be happy to double-check.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 16:18:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340308#M1567</guid>
      <dc:creator>RabbitHoleComp</dc:creator>
      <dc:date>2014-09-10T16:18:22Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340309#M1568</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In &lt;A href="https://community.nxp.com/thread/318917"&gt;Custom kernel for T4240qds - boot issues&lt;/A&gt; you said that the patches I linked to resolved your SATA problems -- are there any remaining issues?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 20:36:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340309#M1568</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2014-09-10T20:36:05Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340310#M1569</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-Boot prints the SoC version in the boot messages.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 20:40:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340310#M1569</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2014-09-10T20:40:00Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340311#M1570</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, those patches definitely resolve my SATA issues, however no PCI devices are enumerating on the bus (lspci returns nothing)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As for silicon revision, I am at 2.0:&lt;/P&gt;&lt;PRE&gt;
&lt;P&gt;U-Boot 2014.04-00110-g021fb01-dirty (Aug 20 2014 - 12:43:46)&lt;/P&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt;CPU0:&amp;nbsp; P5020, Version: 2.0, (0x82200020)&lt;/P&gt;
&lt;P&gt;Core:&amp;nbsp; e5500, Version: 1.2, (0x80240012)&lt;/P&gt;

&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 00:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340311#M1570</guid>
      <dc:creator>RabbitHoleComp</dc:creator>
      <dc:date>2014-09-11T00:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340312#M1571</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/scottwood"&gt;scottwood&lt;/A&gt;, I see that the necessary SATA patches have made it in to mainline as of 3.18, however as previously stated, I have a machine which (using both 3.17-rc3 AND 3.18.1, does not enumerate any PCI devices on the tree. Are there any known patchsets to resolve this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Dec 2014 19:00:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340312#M1571</guid>
      <dc:creator>RabbitHoleComp</dc:creator>
      <dc:date>2014-12-29T19:00:12Z</dc:date>
    </item>
    <item>
      <title>Re: SATA init issues on P5020 with kernel 3.17-rc3</title>
      <link>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340313#M1572</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please post a new topic for the PCI issue, with a boot log and other relevant information.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 29 Dec 2014 21:46:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SATA-init-issues-on-P5020-with-kernel-3-17-rc3/m-p/340313#M1572</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2014-12-29T21:46:44Z</dc:date>
    </item>
  </channel>
</rss>