<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: P1010RDB LEDs</title>
    <link>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325158#M1393</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I found this code in u-boot\arch\powerpc\lib\board.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if defined(CONFIG_STATUS_LED) &amp;amp;&amp;amp; defined(STATUS_LED_BOOT)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status_led_set(STATUS_LED_BOOT, STATUS_LED_BLINKING);&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to do what you want I don't see a flag used so that this will be executed only &lt;/P&gt;&lt;P&gt;for one processor, this code is used for the all processors from the PowerPC family. The&lt;/P&gt;&lt;P&gt;CONFIG_STATUS_LED flag is used to enable the blinking feature in particular.&lt;/P&gt;&lt;P&gt;Maybe this can be a starting point for you,&lt;/P&gt;&lt;P&gt;Catalin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Jul 2014 12:31:23 GMT</pubDate>
    <dc:creator>catalindemergia</dc:creator>
    <dc:date>2014-07-28T12:31:23Z</dc:date>
    <item>
      <title>P1010RDB LEDs</title>
      <link>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325156#M1391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good afternoon,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to the P1010 and the RDB.&amp;nbsp; Are there any usable LEDs on the board that can be actuated from early boot, say in the bootrom?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jamie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 19:36:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325156#M1391</guid>
      <dc:creator>jamiefinney</dc:creator>
      <dc:date>2014-07-25T19:36:36Z</dc:date>
    </item>
    <item>
      <title>Re: P1010RDB LEDs</title>
      <link>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325157#M1392</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you trying to flashing LEDs by yourself from early boot? I have checked the P1010RDBPBUG.pdf Rev.0, and did not find one usable for the purpose, so I am afraid no. Correct me if this is not your meaning.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 02:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325157#M1392</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2014-07-28T02:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: P1010RDB LEDs</title>
      <link>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325158#M1393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I found this code in u-boot\arch\powerpc\lib\board.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if defined(CONFIG_STATUS_LED) &amp;amp;&amp;amp; defined(STATUS_LED_BOOT)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; status_led_set(STATUS_LED_BOOT, STATUS_LED_BLINKING);&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This seems to do what you want I don't see a flag used so that this will be executed only &lt;/P&gt;&lt;P&gt;for one processor, this code is used for the all processors from the PowerPC family. The&lt;/P&gt;&lt;P&gt;CONFIG_STATUS_LED flag is used to enable the blinking feature in particular.&lt;/P&gt;&lt;P&gt;Maybe this can be a starting point for you,&lt;/P&gt;&lt;P&gt;Catalin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jul 2014 12:31:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010RDB-LEDs/m-p/325158#M1393</guid>
      <dc:creator>catalindemergia</dc:creator>
      <dc:date>2014-07-28T12:31:23Z</dc:date>
    </item>
  </channel>
</rss>