<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: COP/JTAG in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324163#M1383</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thinks yes, what's your problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See Section 8.3 Using JTAG Configuration File to Specify Multiple Linked Devices on a JTAG Chain, in Targeting_PA_Processors.pdf, the document is located in the CW installation C:\Freescale\CW_PA_v10.3.3\PA\Help\PDF.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jul 2014 01:46:33 GMT</pubDate>
    <dc:creator>lunminliang</dc:creator>
    <dc:date>2014-07-24T01:46:33Z</dc:date>
    <item>
      <title>COP/JTAG</title>
      <link>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324162#M1382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;Is it possible to use a COP connector (J29 in the P1010RDB)&amp;nbsp; for the boundary scan test?&lt;/P&gt;&lt;P&gt;In my design a JTAG chain consist of a CPLD, P1010, and FPGA.&lt;/P&gt;&lt;P&gt;Will a debugging of&amp;nbsp; P1010 through COP still work, even when the P1010 is in the middle of a JTAG chain?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Jul 2014 16:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324162#M1382</guid>
      <dc:creator>tomaszkrupski</dc:creator>
      <dc:date>2014-07-23T16:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: COP/JTAG</title>
      <link>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324163#M1383</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I thinks yes, what's your problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;See Section 8.3 Using JTAG Configuration File to Specify Multiple Linked Devices on a JTAG Chain, in Targeting_PA_Processors.pdf, the document is located in the CW installation C:\Freescale\CW_PA_v10.3.3\PA\Help\PDF.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 01:46:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324163#M1383</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2014-07-24T01:46:33Z</dc:date>
    </item>
    <item>
      <title>Re: COP/JTAG</title>
      <link>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324164#M1384</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tomasz,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is possible to debug P1010 in the JTAG chain.&lt;/P&gt;&lt;P&gt;First please make sure TDI and TDO of the JTAG header and all the devices in the chain are connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you use CodeWarrior, you need to define JTAG configuration file for the scan chain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The CodeWarrior debugger&amp;nbsp; supports targets with non-Freescale devices on the scan&lt;/P&gt;&lt;P&gt;chain. Each non-Freescale device is declared as "generic" and needs three parameters:&lt;/P&gt;&lt;P&gt;JTAG Instruction Length; Bypass Command; and Bypass Length. The values for these&lt;/P&gt;&lt;P&gt;three parameters are available in the device's data sheet or from its manufacturer.&lt;/P&gt;&lt;P&gt;For example, the JTAG Configuration File for this scan chain could be as the following.&lt;/P&gt;&lt;P&gt;Generic 4 1 0xF&lt;/P&gt;&lt;P&gt;P1010&lt;/P&gt;&lt;P&gt;Generic 5 1 0x1F&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 08:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/COP-JTAG/m-p/324164#M1384</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-07-25T08:28:57Z</dc:date>
    </item>
  </channel>
</rss>