<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: Assign memory address to DDR</title>
    <link>https://community.nxp.com/t5/P-Series/Assign-memory-address-to-DDR/m-p/317772#M1251</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you have to specify:&lt;/P&gt;&lt;P&gt;the base address that you want from Local Access Window Base Address Register&lt;/P&gt;&lt;P&gt;the size (1 GB in your case) from the Local Access Window Attributes Register - it has the SIZE field in it, bits 26-31&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Catalin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Jun 2014 07:25:41 GMT</pubDate>
    <dc:creator>catalindemergia</dc:creator>
    <dc:date>2014-06-12T07:25:41Z</dc:date>
    <item>
      <title>Assign memory address to DDR</title>
      <link>https://community.nxp.com/t5/P-Series/Assign-memory-address-to-DDR/m-p/317771#M1250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The size of my DDR chip is 4GB, can I only assign 1GB memory address to it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Min Zhao&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 01:39:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Assign-memory-address-to-DDR/m-p/317771#M1250</guid>
      <dc:creator>敏赵</dc:creator>
      <dc:date>2014-06-12T01:39:04Z</dc:date>
    </item>
    <item>
      <title>Re: Assign memory address to DDR</title>
      <link>https://community.nxp.com/t5/P-Series/Assign-memory-address-to-DDR/m-p/317772#M1251</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, you have to specify:&lt;/P&gt;&lt;P&gt;the base address that you want from Local Access Window Base Address Register&lt;/P&gt;&lt;P&gt;the size (1 GB in your case) from the Local Access Window Attributes Register - it has the SIZE field in it, bits 26-31&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards,&lt;/P&gt;&lt;P&gt;Catalin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Jun 2014 07:25:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Assign-memory-address-to-DDR/m-p/317772#M1251</guid>
      <dc:creator>catalindemergia</dc:creator>
      <dc:date>2014-06-12T07:25:41Z</dc:date>
    </item>
  </channel>
</rss>