<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic I Cannot Build A UBIFS Root File System in SDK 1.2/P1010 in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211032#M111</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use ubifs as the rootfs. The CPU is P1010, SDK is 1.2 yocto. According to the documentations in SDK, I modified&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) the "IMAGE_FSTYPES" in &amp;lt;sdk_path&amp;gt;/meta-fsl-ppc-private/images/fsl-image-flash.bb,&lt;/P&gt;&lt;P&gt;(2) and then "bitbake fsl-image-core" to build a rootfs image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is not any error message during listed process. So I think I should find an image in &amp;lt;sdk_path&amp;gt;/build_p1010rdb_release/tmp/deploy/images be named fsl-image-core-p1010rdb-yyyymmddhhmmss-rootfs.ubifs, but I cannot. However, I DO find a ubinize.cfg in this folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone knows how should I do to make a rootfs in ubifs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 18 Dec 2012 10:59:02 GMT</pubDate>
    <dc:creator>augustuschen</dc:creator>
    <dc:date>2012-12-18T10:59:02Z</dc:date>
    <item>
      <title>I Cannot Build A UBIFS Root File System in SDK 1.2/P1010</title>
      <link>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211032#M111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would like to use ubifs as the rootfs. The CPU is P1010, SDK is 1.2 yocto. According to the documentations in SDK, I modified&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(1) the "IMAGE_FSTYPES" in &amp;lt;sdk_path&amp;gt;/meta-fsl-ppc-private/images/fsl-image-flash.bb,&lt;/P&gt;&lt;P&gt;(2) and then "bitbake fsl-image-core" to build a rootfs image.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is not any error message during listed process. So I think I should find an image in &amp;lt;sdk_path&amp;gt;/build_p1010rdb_release/tmp/deploy/images be named fsl-image-core-p1010rdb-yyyymmddhhmmss-rootfs.ubifs, but I cannot. However, I DO find a ubinize.cfg in this folder.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anyone knows how should I do to make a rootfs in ubifs?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Dec 2012 10:59:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211032#M111</guid>
      <dc:creator>augustuschen</dc:creator>
      <dc:date>2012-12-18T10:59:02Z</dc:date>
    </item>
    <item>
      <title>Re: I Cannot Build A UBIFS Root File System in SDK 1.2/P1010</title>
      <link>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211033#M112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This (ubifs) is not tested in Freescale's SDK. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 Jan 2013 16:49:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211033#M112</guid>
      <dc:creator>mattsm</dc:creator>
      <dc:date>2013-01-02T16:49:47Z</dc:date>
    </item>
    <item>
      <title>Re: I Cannot Build A UBIFS Root File System in SDK 1.2/P1010</title>
      <link>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211034#M113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to know what is tested? Is there a document indicating? Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 02:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211034#M113</guid>
      <dc:creator>wenlantang</dc:creator>
      <dc:date>2013-01-04T02:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: I Cannot Build A UBIFS Root File System in SDK 1.2/P1010</title>
      <link>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211035#M114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The default build images on the targets we provided (fsl-image-minimal,core,lsb-sdk) should all be tested. That being said, getting ubifs to work should not be all that much effort but I can't comment on exactly what's needed at this point.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect you might be missing user space tools to create ubi file systems from a Linux host, something equivalent to mkfs.ubifs for example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-M&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Jan 2013 03:34:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/I-Cannot-Build-A-UBIFS-Root-File-System-in-SDK-1-2-P1010/m-p/211035#M114</guid>
      <dc:creator>mattsm</dc:creator>
      <dc:date>2013-01-04T03:34:46Z</dc:date>
    </item>
  </channel>
</rss>