<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Running Linux on 8GB P5020</title>
    <link>https://community.nxp.com/t5/P-Series/Running-Linux-on-8GB-P5020/m-p/304498#M1089</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running our P5020 board with 8GB of memory, and having a number of problems with Linux. Our kernel is based off the sdk-v1.5 tag in the Freescale GIT tree. With 4GB of memory every driver worked, but with 8GB the following drivers have failed: MMC, USB, and SATA. In each case the on-chip device only supports 32-bit addressing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've fixed MMC by disabling DMA when the board has more than 4GB. Has anybody got USB and SATA working in large memory scenarios?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 3 using fsl-ehci&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 4 using fsl-ehci&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 4, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 5 using fsl-ehci&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 5, error -32&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: unable to enumerate USB device on port 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ata2: Signature Update detected @ 504 msecs&lt;/P&gt;&lt;P&gt;ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)&lt;/P&gt;&lt;P&gt;ata2.00: failed to IDENTIFY (INIT_DEV_PARAMS failed, err_mask=0x80)&lt;/P&gt;&lt;P&gt;ata2: limiting SATA link speed to 1.5 Gbps&lt;/P&gt;&lt;P&gt;ata2: Signature Update detected @ 504 msecs&lt;/P&gt;&lt;P&gt;ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)&lt;/P&gt;&lt;P&gt;ata2.00: failed to IDENTIFY (INIT_DEV_PARAMS failed, err_mask=0x80)&lt;/P&gt;&lt;P&gt;ata2: Signature Update detected @ 504 msecs&lt;/P&gt;&lt;P&gt;ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 26 Mar 2014 10:06:06 GMT</pubDate>
    <dc:creator>adriancox</dc:creator>
    <dc:date>2014-03-26T10:06:06Z</dc:date>
    <item>
      <title>Running Linux on 8GB P5020</title>
      <link>https://community.nxp.com/t5/P-Series/Running-Linux-on-8GB-P5020/m-p/304498#M1089</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm running our P5020 board with 8GB of memory, and having a number of problems with Linux. Our kernel is based off the sdk-v1.5 tag in the Freescale GIT tree. With 4GB of memory every driver worked, but with 8GB the following drivers have failed: MMC, USB, and SATA. In each case the on-chip device only supports 32-bit addressing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've fixed MMC by disabling DMA when the board has more than 4GB. Has anybody got USB and SATA working in large memory scenarios?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 3 using fsl-ehci&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: device descriptor read/64, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 4 using fsl-ehci&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 4, error -32&lt;/P&gt;&lt;P&gt;usb 1-1: new high-speed USB device number 5 using fsl-ehci&lt;/P&gt;&lt;P&gt;usb 1-1: device not accepting address 5, error -32&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: unable to enumerate USB device on port 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ata2: Signature Update detected @ 504 msecs&lt;/P&gt;&lt;P&gt;ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)&lt;/P&gt;&lt;P&gt;ata2.00: failed to IDENTIFY (INIT_DEV_PARAMS failed, err_mask=0x80)&lt;/P&gt;&lt;P&gt;ata2: limiting SATA link speed to 1.5 Gbps&lt;/P&gt;&lt;P&gt;ata2: Signature Update detected @ 504 msecs&lt;/P&gt;&lt;P&gt;ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)&lt;/P&gt;&lt;P&gt;ata2.00: failed to IDENTIFY (INIT_DEV_PARAMS failed, err_mask=0x80)&lt;/P&gt;&lt;P&gt;ata2: Signature Update detected @ 504 msecs&lt;/P&gt;&lt;P&gt;ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 10:06:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Running-Linux-on-8GB-P5020/m-p/304498#M1089</guid>
      <dc:creator>adriancox</dc:creator>
      <dc:date>2014-03-26T10:06:06Z</dc:date>
    </item>
    <item>
      <title>Re: Running Linux on 8GB P5020</title>
      <link>https://community.nxp.com/t5/P-Series/Running-Linux-on-8GB-P5020/m-p/304499#M1090</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Fixed it - in moving to our own board file a typo had disabled SWIOTLB initialisation for platform devices.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Mar 2014 16:19:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Running-Linux-on-8GB-P5020/m-p/304499#M1090</guid>
      <dc:creator>adriancox</dc:creator>
      <dc:date>2014-03-26T16:19:47Z</dc:date>
    </item>
  </channel>
</rss>