<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Unable to use IPFWD application suite</title>
    <link>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297175#M1045</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ipfwd_config is used in USDPAA IPFWD application, please check whether you missed the following steps.&lt;/P&gt;&lt;P&gt;1. Boot up P4080 with usdpaa device tree, and use fmc to configure FMAN policy, for example&lt;/P&gt;&lt;P&gt;cd /usr/etc&lt;/P&gt;&lt;P&gt;fmc -c us_config_serdes_0xe.xml -p us_policy_hash_ipv4_src_dst_32_fq.xml -a.&lt;/P&gt;&lt;P&gt;2. Setup ipfwd_app and make sure it start successfully.&lt;/P&gt;&lt;P&gt;ipfwd_app 1..7 -i fm1-10g,fm2-gb2&lt;/P&gt;&lt;P&gt;3. On the target, use ipfwd_config to add ip and routes configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. On two machine configure ip, gw, arp for gw and route information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your problem remains, please kindly share your Linux console log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping Wang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 20 Apr 2014 13:14:48 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2014-04-20T13:14:48Z</dc:date>
    <item>
      <title>Unable to use IPFWD application suite</title>
      <link>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297171#M1041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ipfwd_config first asks for flow id but fails to recognize when provided. Kindly guide how to deal with this?&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Execution log&lt;/P&gt;&lt;P&gt;==========&lt;/P&gt;&lt;P&gt;root@p4080ds:/usr/etc# ipfwd_config -P 1904 -B -s 192.168.27.2 -d 192.168.28.2 -g 192.168.28.2&lt;/P&gt;&lt;P&gt;ERR:Route Entry Operation failed as mandatory parameters missing; --f or -f&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@p4080ds:/usr/etc# ipfwd_config -P 1904 -B -s 192.168.27.2 -d 192.168.28.2 -g 192.168.28.2 -f 1&lt;/P&gt;&lt;P&gt;-B: -f: (PROGRAM ERROR) Option should have been recognized!?&lt;/P&gt;&lt;P&gt;Try `-B --help' or `-B --usage' for more information.&lt;/P&gt;&lt;P&gt;root@p4080ds:/usr/etc#&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Apr 2014 17:48:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297171#M1041</guid>
      <dc:creator>fahadarslan</dc:creator>
      <dc:date>2014-04-15T17:48:12Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to use IPFWD application suite</title>
      <link>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297172#M1042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Using the modified command, route entry can be made without facing above error. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@p4080ds:/usr/etc# ipfwd_config -P 1904 -B -s 192.168.27.2 -c 1 -d 192.168.28.2&amp;nbsp; -n 1 -g 192.168.28.2&lt;/P&gt;&lt;P&gt;Route Entry Added successfully&lt;/P&gt;&lt;P&gt;root@p4080ds:~# &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;where&lt;/P&gt;&lt;P&gt;-c count for source IP address and &lt;/P&gt;&lt;P&gt;-n count for destination IP address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But after following all steps, two machines connected through P4080DS are still not able to ping each other!&lt;/P&gt;&lt;P&gt;Any suggestions?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 17 Apr 2014 17:22:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297172#M1042</guid>
      <dc:creator>fahadarslan</dc:creator>
      <dc:date>2014-04-17T17:22:11Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to use IPFWD application suite</title>
      <link>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297173#M1043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Arslan&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This could be because ipfwd application does not have correct ARP entries for source and destination machines.&lt;/P&gt;&lt;P&gt;Can you capture the packets using tcpdump or wireshark on the port connected to destination machine and see if it is receiving ethernet pkts from P4080 with correct destination mac address?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Vakul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2014 07:32:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297173#M1043</guid>
      <dc:creator>vakulgarg</dc:creator>
      <dc:date>2014-04-18T07:32:43Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to use IPFWD application suite</title>
      <link>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297174#M1044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sure, let me try capturing the packets.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Apr 2014 07:36:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297174#M1044</guid>
      <dc:creator>fahadarslan</dc:creator>
      <dc:date>2014-04-18T07:36:34Z</dc:date>
    </item>
    <item>
      <title>Re: Unable to use IPFWD application suite</title>
      <link>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297175#M1045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;ipfwd_config is used in USDPAA IPFWD application, please check whether you missed the following steps.&lt;/P&gt;&lt;P&gt;1. Boot up P4080 with usdpaa device tree, and use fmc to configure FMAN policy, for example&lt;/P&gt;&lt;P&gt;cd /usr/etc&lt;/P&gt;&lt;P&gt;fmc -c us_config_serdes_0xe.xml -p us_policy_hash_ipv4_src_dst_32_fq.xml -a.&lt;/P&gt;&lt;P&gt;2. Setup ipfwd_app and make sure it start successfully.&lt;/P&gt;&lt;P&gt;ipfwd_app 1..7 -i fm1-10g,fm2-gb2&lt;/P&gt;&lt;P&gt;3. On the target, use ipfwd_config to add ip and routes configurations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. On two machine configure ip, gw, arp for gw and route information.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If your problem remains, please kindly share your Linux console log.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping Wang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 20 Apr 2014 13:14:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unable-to-use-IPFWD-application-suite/m-p/297175#M1045</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2014-04-20T13:14:48Z</dc:date>
    </item>
  </channel>
</rss>