<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: Communication failure using PCA9615 Differential I2C Bus Extender</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190984#M9972</link>
    <description>&lt;P&gt;I will try to change the IC , i will order some ICs , and test them&lt;/P&gt;</description>
    <pubDate>Mon, 30 Nov 2020 14:27:19 GMT</pubDate>
    <dc:creator>Ehab_Hamayel</dc:creator>
    <dc:date>2020-11-30T14:27:19Z</dc:date>
    <item>
      <title>Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1186977#M9895</link>
      <description>&lt;P&gt;I have used PCA9615 differential I2C bus driver in one design to extend the I2C bus over CAT5 cable. (datasheet&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://www.nxp.com/docs/en/data-sheet/PCA9615.pdf" rel="nofollow noreferrer" target="_blank"&gt;https://www.nxp.com/docs/en/data-sheet/PCA9615.pdf&lt;/A&gt;)&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;The design has been done according to the datasheet recommendation and with the help of a reference design of a popular open-source board manufactured by Sparkfun which I used as a demo board, before starting the design.&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Unfortunately, the design didn't work well in my case, as the communication doesn't establish when connecting a pair of PCA9615 using CAT5 cable.&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;EM&gt;I have attached my schematic and layout of the board, and the connection topology I used.&lt;/EM&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Here are some observations:&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;It seems when connecting the PCA9615 boards over the ethernet cable (tested it using 1 m long cable), both SDA and SCL lines get pulled low, so there is no connection over I2C.&lt;/LI&gt;&lt;LI&gt;The termination resistors have been calculated according to the datasheet recommendations (yielding 88.5Ohm parallel resistance close to the 100Ohm indicated in the datasheet, it should work since SparkFun's module uses the same values as I)&lt;/LI&gt;&lt;LI&gt;I tested it for the pin-to-pin continuity for one board to another and it's correct.&lt;/LI&gt;&lt;LI&gt;Every board is designed with three I2C inputs, if I connected to two I2C devices on the same board without connecting the second board, then it works fine, which means no problem from the I2C side.&lt;/LI&gt;&lt;LI&gt;I have tested the voltage levels on both boards and they indicate correct voltage levels (5V in my case)&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;I would appreciate any help or suggestion regarding this problem.&lt;/P&gt;</description>
      <pubDate>Sat, 21 Nov 2020 14:15:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1186977#M9895</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-21T14:15:26Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1187065#M9897</link>
      <description>&lt;P&gt;Hi&lt;/P&gt;
&lt;P&gt;1:What's the VDDA and VDDB value?&lt;/P&gt;
&lt;P&gt;2:Your schematic only half&amp;nbsp; pair&amp;nbsp; of PCA9615,the other half has same circuit with your attached?&lt;/P&gt;
&lt;P&gt;3:You also need follow the timing of PCA9615 as datasheet page8 Fig6.&lt;/P&gt;</description>
      <pubDate>Mon, 23 Nov 2020 01:56:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1187065#M9897</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-23T01:56:39Z</dc:date>
    </item>
    <item>
      <title>Re Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1187424#M9904</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;SPAN class=""&gt;guoweisun,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;Regarding your questions, here are the answers:&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN class=""&gt;The VDDA and VDDB are tied together and both have 4.86V when using Vcc= 5V and a CAT5e cable of 2m.&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;Yes, identical board, they are connected using RJ45 connectors / pin-to-pin, such as 1 to 1, 2 to 2, etc...&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN class=""&gt;I will verify the timing of the signals and upload a picture of it ASAP.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN class=""&gt;&amp;nbsp;- could you please confirm whether the schematic design is correct or has any design problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;- In my design, the En pin is left unconnected, assuming it has an internal pull-up and always in &lt;U&gt;&lt;EM&gt;Active state&lt;/EM&gt;&lt;/U&gt;,&amp;nbsp;Could this cause a problem?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class=""&gt;- using PCA9615 and with reference to the timing requirement, does it demand any change on the original software? (assuming the code is originally attended to be used with direct I2C bus.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;</description>
      <pubDate>Mon, 23 Nov 2020 10:52:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1187424#M9904</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-23T10:52:11Z</dc:date>
    </item>
    <item>
      <title>Re: Re Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1187764#M9912</link>
      <description>&lt;P&gt;&lt;SPAN&gt;1:R1/R5/R2/R6=600ohm.R3/R4=100ohm.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2: EN can’t be floating please following the timing also in datasheet.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 01:12:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1187764#M9912</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-24T01:12:55Z</dc:date>
    </item>
    <item>
      <title>Re: Re Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1188200#M9915</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Thanks for your answer.&lt;/P&gt;&lt;P&gt;But from my previous experience&amp;nbsp;using Sparkfun's PCA9615 two years ago, the En pin is optional to use, and I left it floating, and it worked, also the datasheet mentioned the En pin is internally pulled up to VDDA, and an internal control circuit manages the operation sequence, please correct me if I'm wrong on this.&lt;/P&gt;&lt;P&gt;Is it possible to give me an example code for the correct operation sequence? (I'm using STM32F103 MCU), because I'm planning to mass-produce this module and I have told the PCB manufacture to suspend the production until I found what's wrong with the design.&lt;/P&gt;&lt;P&gt;-----&lt;/P&gt;&lt;P&gt;Thank you very much,&lt;/P&gt;</description>
      <pubDate>Tue, 24 Nov 2020 12:47:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1188200#M9915</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-24T12:47:32Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1188575#M9917</link>
      <description>&lt;P&gt;HI&lt;/P&gt;
&lt;P&gt;1:If you use the hot swap function,you need follow this timing and EN configuration.&lt;/P&gt;
&lt;P&gt;2: This device no registers setting so we don't have the code example.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 25 Nov 2020 03:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1188575#M9917</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-25T03:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1189282#M9928</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;1. I'm not using hot-swap, both boards are being connected and powered before running the code.&lt;/P&gt;&lt;P&gt;2. in the&amp;nbsp;User manual for the dI2C demo board [Doc.&amp;nbsp;UM10856], NXP demonstrates a usage example of PCA9615 without the En pin, and I did to using Sparkfun's PCA9615 I2C extender and it worked.&lt;/P&gt;&lt;P&gt;3. I was meaning an MCU general code (or pseudo-code) to achieve the starting sequence that you mention, but it doesn't work too! here is the procedure:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;EN pin: Low upon MCU reset, then High after a certain delay.&lt;/LI&gt;&lt;LI&gt;SDA, SCL: sending stop bit, followed by Idle state.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;testing the Differential bus using the oscilloscope, I got the following when using VddB=5V:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;DSDAM,DSCLM = 2.8V&lt;/LI&gt;&lt;LI&gt;DSDAP,&amp;nbsp;DSCLP = 2.45V&lt;/LI&gt;&lt;/UL&gt;</description>
      <pubDate>Wed, 25 Nov 2020 21:34:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1189282#M9928</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-25T21:34:55Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190104#M9938</link>
      <description>&lt;P&gt;In the UM10856 the PCA9614/5/6 schematic the EN is pull up to VDDA not floating. I suggest you refer to the schematic of UM10856 page4.&lt;/P&gt;
&lt;P&gt;For the MCU code which is no available&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Fri, 27 Nov 2020 06:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190104#M9938</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-27T06:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190800#M9960</link>
      <description>&lt;P&gt;&lt;SPAN class="caseEventBody"&gt;&lt;SPAN class="caseEventRow"&gt;&lt;SPAN class="feeditemtext cxfeeditemtext"&gt;Anyway I post my suggestion here again hope you can understand!&lt;BR /&gt;1: If you use the hot swap please refer to page8 Fig6 timing spec.&lt;BR /&gt;2:If not use hot swap function please pull up this EN pin to VDDA with resistor 10K.&lt;BR /&gt;3:For the schematic please refer to UM10856 page4 especially the difference line's resistors value.&lt;BR /&gt;4: we don't have any code about this PCA9615.&lt;BR /&gt;5:After do above steps,if still issue please check device PCA9615,do you buy this device directly from NXP or NXP distributors?&lt;BR /&gt;6:You can also find any difference between your schematic and Sparkfun's PCA961,or use Sparkfun's PCA9615 into your board to verify your system work or not.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 09:06:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190800#M9960</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-30T09:06:08Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190864#M9962</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;i will try to pull up the En pin to VDD through 10KR as you suggested on the last try.&lt;/P&gt;&lt;P&gt;if it doesn't work I will replace the IC with an IC which has a different production date.&lt;/P&gt;&lt;P&gt;with regard to your question about the supplier, I have sourced the IC from a trusted Chinese supplier since the PCBA is done in China too, but I don't think the IC is a copy or fake since the price is almost the same as listed on some popular stores like Digikey.&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 10:24:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190864#M9962</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-30T10:24:00Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190867#M9963</link>
      <description>&lt;P&gt;Refer to our schematic in the UM10856 especially the divider resistor of difference lines.&lt;/P&gt;
&lt;P&gt;In your system if remove the PCA9615 related circuit and decrease the communicate distance,do the IIC communication work successfully?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 10:28:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190867#M9963</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-30T10:28:37Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190902#M9964</link>
      <description>&lt;P&gt;&lt;STRONG&gt;"Refer to our schematic in the UM10856 especially the divider resistor of difference lines."&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;I have referred to the schematic and changed the resistor network values to something similar, but it doesn't work.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;"In your system if remove the PCA9615 related circuit and decrease the communicate distance, do the IIC communication work successfully?"&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Eliminating the PCA9615 boards, and connecting the I2C&amp;nbsp; master to slave directly over I2C directly, workers without any problem .&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 11:18:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190902#M9964</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-30T11:18:03Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190907#M9965</link>
      <description>&lt;P&gt;Very strange!&lt;/P&gt;
&lt;P&gt;Do you use the Sparkfun's PCA9615 board to try in your system?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 11:29:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190907#M9965</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-30T11:29:52Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190911#M9966</link>
      <description>&lt;P&gt;I marked it Solved by mistake, sorry for that.&lt;/P&gt;&lt;P&gt;I used SparkFun's PCA9615 board previously (a year ago) it was so good.&lt;/P&gt;&lt;P&gt;I couldn't think of any problem but the IC itself in my design&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 11:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190911#M9966</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-30T11:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190936#M9968</link>
      <description>&lt;P&gt;So now you can solder the Sparkfun's PCA9615 IC into your board to try and verify this IC.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 12:55:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190936#M9968</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-30T12:55:49Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190951#M9969</link>
      <description>&lt;P&gt;Any update when you change the PCA9615,or can you eliminate the solder issue in your board?&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 13:31:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190951#M9969</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-11-30T13:31:08Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190984#M9972</link>
      <description>&lt;P&gt;I will try to change the IC , i will order some ICs , and test them&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 14:27:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1190984#M9972</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-11-30T14:27:19Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1191154#M9975</link>
      <description>&lt;P&gt;You can quickly change Spakrfun's PCA9615 into your board and get the result.&lt;/P&gt;
&lt;P&gt;If not this PCA9615's issue,we can find others reason but need eliminate this firstly.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 00:52:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1191154#M9975</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-12-01T00:52:06Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1191690#M9986</link>
      <description>&lt;P&gt;I haven’t yet because I have placed an order for 10 pcs of the PCA9615 yesterday, and I will wait till they arrive. But now, I’m pretty sure the problem with the IC itself.&lt;/P&gt;&lt;P&gt;Also, I no longer have SparkFun's PCA9615 boards. It was a year ago. By the way, I've placed an order for a couple of boards and waiting for them to arrive, I will use them as demo boards&lt;/P&gt;&lt;P&gt;I’m highly appreciating your assistant with my case, and I will inform you if it works for me.&lt;/P&gt;&lt;P&gt;*Regarding your suggestion of pulling the En pin to VDD using 10KR, I have applied it to a few boards, but it didn’t make any difference.&lt;/P&gt;</description>
      <pubDate>Tue, 01 Dec 2020 14:49:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1191690#M9986</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-12-01T14:49:21Z</dc:date>
    </item>
    <item>
      <title>Re: Communication failure using PCA9615 Differential I2C Bus Extender</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1197440#M10026</link>
      <description>&lt;P&gt;&lt;STRONG&gt;**The problem Has been solved&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;The cause of the problem is the non-compatibility of the PCA9615 and the I2C buffer IC (PCA9515B) that I’m using in the I2C master board.&lt;/P&gt;&lt;P&gt;After removing the PCA9515B and connecting the PCA9615 directly with the MCU, the system worked as supposed to be.&lt;/P&gt;</description>
      <pubDate>Thu, 10 Dec 2020 14:03:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Communication-failure-using-PCA9615-Differential-I2C-Bus/m-p/1197440#M10026</guid>
      <dc:creator>Ehab_Hamayel</dc:creator>
      <dc:date>2020-12-10T14:03:14Z</dc:date>
    </item>
  </channel>
</rss>