<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックCodeWarrior USB TAP can not connect</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-TAP-can-not-connect/m-p/1190616#M9951</link>
    <description>&lt;P&gt;When I use the CodeWarrior USB TAP to connect MCP8309,it&lt;BR /&gt;always returns "Please check your JTAG clock speed",so I&lt;BR /&gt;change another CodeWarrior USB TAP,it works well!&lt;/P&gt;&lt;P&gt;My trouble&lt;BR /&gt;is How to&amp;nbsp; repair it?&lt;/P&gt;</description>
    <pubDate>Mon, 30 Nov 2020 04:58:33 GMT</pubDate>
    <dc:creator>yqypower</dc:creator>
    <dc:date>2020-11-30T04:58:33Z</dc:date>
    <item>
      <title>CodeWarrior USB TAP can not connect</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-TAP-can-not-connect/m-p/1190616#M9951</link>
      <description>&lt;P&gt;When I use the CodeWarrior USB TAP to connect MCP8309,it&lt;BR /&gt;always returns "Please check your JTAG clock speed",so I&lt;BR /&gt;change another CodeWarrior USB TAP,it works well!&lt;/P&gt;&lt;P&gt;My trouble&lt;BR /&gt;is How to&amp;nbsp; repair it?&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 04:58:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-TAP-can-not-connect/m-p/1190616#M9951</guid>
      <dc:creator>yqypower</dc:creator>
      <dc:date>2020-11-30T04:58:33Z</dc:date>
    </item>
    <item>
      <title>Re: CodeWarrior USB TAP can not connect</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-TAP-can-not-connect/m-p/1190666#M9954</link>
      <description>&lt;P&gt;Did you use CodeWarrior 10.5.1 or CodeWarrior 8.8?&lt;/P&gt;
&lt;P&gt;Is the problem USB TAP a CodeWarrior TAP which integrates both USB and Ethernet ports?&lt;/P&gt;
&lt;P&gt;Is there valid RCW on MPC8309 custom board?&lt;/P&gt;
&lt;P&gt;Please open CCS console from Start-&amp;gt;Freescale CodeWarrior-&amp;gt;CodeWarrior Connection Server and type the following commands to do more verification.&lt;/P&gt;
&lt;P&gt;(bin) 3 % delete all&lt;BR /&gt;(bin) 4 % config cc cwtap&lt;BR /&gt;(bin) 5 % show cc&lt;BR /&gt;CodeWarrior TAP executable differs from local file.&lt;BR /&gt;CodeWarrior TAP Boot Loader version 1.0.1&lt;BR /&gt;CodeWarrior TAP OS version 1.0.1&lt;BR /&gt;Sending code to CodeWarrior TAP.........done&lt;BR /&gt;Running package script&lt;BR /&gt;0: CodeWarrior TAP (cwtap) CC software ver. {0.0}&lt;BR /&gt;(bin) 6 % source IDcode.tcl&lt;/P&gt;
&lt;P&gt;Scanning for available TAPs connected via USB.....&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++&lt;BR /&gt;+&lt;BR /&gt;+ Available Remote Connections&lt;BR /&gt;+&lt;BR /&gt;+ 1 - CodeWarriorTAP - 00:04:9f:02:f1:ea&lt;BR /&gt;+ 2 - CodeWarriorTAP - &amp;lt;Specify IP Address&amp;gt;&lt;BR /&gt;+ 3 - EthernetTAP - &amp;lt;Specify IP Address&amp;gt;&lt;BR /&gt;+ 4 - GigabitTAP - &amp;lt;Specify IP Address&amp;gt;&lt;BR /&gt;+&lt;BR /&gt;+ x - Exit Script without Changes&lt;BR /&gt;+&lt;BR /&gt;++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++++&lt;/P&gt;
&lt;P&gt;Specify connection:&lt;BR /&gt;1&lt;/P&gt;
&lt;P&gt;Configuring TAP Interface....&lt;/P&gt;
&lt;P&gt;Configured Connection: cwtap : 00:04:9f:02:f1:ea&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 30 Nov 2020 06:18:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/CodeWarrior-USB-TAP-can-not-connect/m-p/1190666#M9954</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-11-30T06:18:05Z</dc:date>
    </item>
  </channel>
</rss>