<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: FLEXBUILD-LS1012AFRWY Error</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181248#M9842</link>
    <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;Thanks for your assistance which helps me to complete the whole process successfully. However, I still have some questions as follows:&lt;/P&gt;&lt;P&gt;Q1: I supposed there is a stage that the build would show me a "&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt;" so I can add some drivers into the Linux kernel, but there is not, what should I do?&lt;/P&gt;&lt;P&gt;Q2: I found there are 2 firmware image files as follows, what is the difference between them? Which one should I use?&lt;/P&gt;&lt;P&gt;firmware_ls1012afrwy_512mb_uboot_qspiboot.img&lt;BR /&gt;firmware_ls1012afrwy_uboot_qspiboot.img&lt;/P&gt;&lt;P&gt;Q3: If I want to use flex-installer to program the corresponding images to SD card, where is the &lt;STRONG&gt;bootpartition_LS_arm64_lts_5.4.tgz&lt;/STRONG&gt; file, or how do I build it?&lt;/P&gt;&lt;P&gt;Q4: Since the full build process is taking horribly long, is there any shorter re-entry point if I make the following changes for my coming projects?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Add some drivers to the Linux kernel&lt;/LI&gt;&lt;LI&gt;Change the hardware to:&lt;BR /&gt;- Ethernet PHY: RTL8211B 2.5G PHY (Also how to modify the device tree?)&lt;BR /&gt;- SDHC1: SD Card&lt;BR /&gt;- SDHC2: eMMC (Also how to modify the device tree?)&lt;BR /&gt;- Boot Sequence: SD --&amp;gt; eMMC&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
    <pubDate>Wed, 11 Nov 2020 06:30:46 GMT</pubDate>
    <dc:creator>Steve81800</dc:creator>
    <dc:date>2020-11-11T06:30:46Z</dc:date>
    <item>
      <title>FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1179694#M9804</link>
      <description>&lt;P&gt;Dear Experts,&lt;/P&gt;&lt;P&gt;I am trying to build the new kernel for LS1012AFRWY. I have my Ubuntu 18.04 running in the VMware guest on Win 7. The build process was aborted, please see attached log file, can you help? Thank you!&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Sat, 07 Nov 2020 11:55:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1179694#M9804</guid>
      <dc:creator>Steve81800</dc:creator>
      <dc:date>2020-11-07T11:55:13Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1179862#M9811</link>
      <description>&lt;P&gt;We usually use the following command sequence under Virtual machine (200GB HDD and 4GB memory).&lt;/P&gt;
&lt;P&gt;Install Ubuntu 18.04.&lt;/P&gt;
&lt;P&gt;Install all updates for this Ubuntu.&lt;/P&gt;
&lt;P&gt;Install and build LSDK2004 using the following command sequence:&lt;/P&gt;
&lt;OL&gt;
&lt;LI&gt;sudo apt-get install git&lt;/LI&gt;
&lt;LI&gt;tar xvzf flexbuild_lsdk2004_update_290520.tgz&lt;/LI&gt;
&lt;LI&gt;Change directory and issue: source setup.env&lt;/LI&gt;
&lt;LI&gt;flex-builder -i mkrfs -a arm64&lt;/LI&gt;
&lt;LI&gt;flex-builder -c linux -a arm64&lt;/LI&gt;
&lt;LI&gt;flex-builder -i mkfw -m ls1012afrwy -b qspi&lt;/LI&gt;
&lt;/OL&gt;</description>
      <pubDate>Mon, 09 Nov 2020 05:50:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1179862#M9811</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-11-09T05:50:41Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1180035#M9816</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;Thanks for your information. I did what you suggested. However, it was aborted as the attached log file. I copied the error portions as follows for you:&lt;/P&gt;&lt;P&gt;error: RPC failed; curl 56 GnuTLS recv error (-54): Error in the pull function.&lt;BR /&gt;fatal: The remote end hung up unexpectedly&lt;BR /&gt;fatal: early EOF&lt;BR /&gt;fatal: index-pack failed&lt;BR /&gt;make[2]: Entering directory '/home/steve/Desktop/flexbuild_lsdk2004_update_290520/packages/linux'&lt;BR /&gt;make[2]: *** /home/steve/Desktop/flexbuild_lsdk2004_update_290520/packages/linux/linux: No such file or directory. Stop.&lt;BR /&gt;make[2]: Leaving directory '/home/steve/Desktop/flexbuild_lsdk2004_update_290520/packages/linux'&lt;BR /&gt;Makefile:26: recipe for target 'build_kernel' failed&lt;BR /&gt;make[1]: *** [build_kernel] Error 2&lt;BR /&gt;make[1]: Leaving directory '/home/steve/Desktop/flexbuild_lsdk2004_update_290520/packages/linux'&lt;BR /&gt;Makefile:22: recipe for target 'linux' failed&lt;BR /&gt;make: *** [linux] Error 2&lt;BR /&gt;make: Leaving directory '/home/steve/Desktop/flexbuild_lsdk2004_update_290520'&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Mon, 09 Nov 2020 10:22:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1180035#M9816</guid>
      <dc:creator>Steve81800</dc:creator>
      <dc:date>2020-11-09T10:22:50Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1180472#M9828</link>
      <description>&lt;P&gt;See the following page about error message in your log (RPC failed; result=56):&lt;BR /&gt;&lt;A href="https://confluence.atlassian.com/stashkb/git-clone-fails-error-rpc-failed-result-56-http-code-200-693897332.html" target="_blank"&gt;https://confluence.atlassian.com/stashkb/git-clone-fails-error-rpc-failed-result-56-http-code-200-693897332.html&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 10 Nov 2020 05:16:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1180472#M9828</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-11-10T05:16:00Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181179#M9838</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;Thanks for your assistance which helps me to complete the whole process successfully. However, I still have some questions as follows:&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q1: I supposed there is a stage that the build would show me a "&lt;FONT face="courier new,courier"&gt;make menuconfig&lt;/FONT&gt;" so I can add some drivers into the Linux kernel, but there is not, what should I do?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q2: I found there are 2 firmware image files as follows, what is the difference between them? Which one should I use?&lt;/STRONG&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;firmware_ls1012afrwy_512mb_uboot_qspiboot.img&lt;/LI&gt;&lt;LI&gt;firmware_ls1012afrwy_uboot_qspiboot.img&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;STRONG&gt;Q3: If I want to use &lt;FONT face="courier new,courier"&gt;flex-installer&lt;/FONT&gt; to program the corresponding images to SD card, where is the&amp;nbsp;&lt;FONT face="courier new,courier"&gt;bootpartition_LS_arm64_lts_5.4.tgz &lt;/FONT&gt;&lt;/STRONG&gt;&lt;STRONG&gt;file? or how do I build it?&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Q4: Since the full build process is taking horribly long, is there any shorter re-entry point if I make the following changes for my coming projects?&lt;/STRONG&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Add some drivers to the Linux kernel&lt;/LI&gt;&lt;LI&gt;Change the hardware to:&lt;/LI&gt;&lt;/OL&gt;&lt;UL&gt;&lt;LI&gt;Ethernet PHY: RTL8211B 2.5G PHY (Also how to modify the device tree?)&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;SDHC1: SD Card&lt;/LI&gt;&lt;LI&gt;SDHC2: eMMC&amp;nbsp;(Also how to modify the device tree?)&amp;nbsp;&lt;/LI&gt;&lt;LI&gt;Boot Sequence: SD --&amp;gt; eMMC&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 03:36:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181179#M9838</guid>
      <dc:creator>Steve81800</dc:creator>
      <dc:date>2020-11-11T03:36:59Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181248#M9842</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;Thanks for your assistance which helps me to complete the whole process successfully. However, I still have some questions as follows:&lt;/P&gt;&lt;P&gt;Q1: I supposed there is a stage that the build would show me a "&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt;" so I can add some drivers into the Linux kernel, but there is not, what should I do?&lt;/P&gt;&lt;P&gt;Q2: I found there are 2 firmware image files as follows, what is the difference between them? Which one should I use?&lt;/P&gt;&lt;P&gt;firmware_ls1012afrwy_512mb_uboot_qspiboot.img&lt;BR /&gt;firmware_ls1012afrwy_uboot_qspiboot.img&lt;/P&gt;&lt;P&gt;Q3: If I want to use flex-installer to program the corresponding images to SD card, where is the &lt;STRONG&gt;bootpartition_LS_arm64_lts_5.4.tgz&lt;/STRONG&gt; file, or how do I build it?&lt;/P&gt;&lt;P&gt;Q4: Since the full build process is taking horribly long, is there any shorter re-entry point if I make the following changes for my coming projects?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Add some drivers to the Linux kernel&lt;/LI&gt;&lt;LI&gt;Change the hardware to:&lt;BR /&gt;- Ethernet PHY: RTL8211B 2.5G PHY (Also how to modify the device tree?)&lt;BR /&gt;- SDHC1: SD Card&lt;BR /&gt;- SDHC2: eMMC (Also how to modify the device tree?)&lt;BR /&gt;- Boot Sequence: SD --&amp;gt; eMMC&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 06:30:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181248#M9842</guid>
      <dc:creator>Steve81800</dc:creator>
      <dc:date>2020-11-11T06:30:46Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181257#M9844</link>
      <description>&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;Thanks for your assistance which helps me to complete the whole process successfully. However, I still have some questions as follows:&lt;/P&gt;&lt;P&gt;Q1: I supposed there is a stage that the build would show me a "&lt;STRONG&gt;make menuconfig&lt;/STRONG&gt;" so I can add some drivers into the Linux kernel, but there is not, what should I do?&lt;/P&gt;&lt;P&gt;Q2: I found there are 2 firmware image files as follows, what is the difference between them? Which one should I use?&lt;/P&gt;&lt;P&gt;firmware_ls1012afrwy_512mb_uboot_qspiboot.img&lt;BR /&gt;firmware_ls1012afrwy_uboot_qspiboot.img&lt;BR /&gt;Q3: If I want to use &lt;STRONG&gt;flex-installer&lt;/STRONG&gt; to program the corresponding images to SD card, where is the &lt;STRONG&gt;bootpartition_LS_arm64_lts_5.4.tgz&lt;/STRONG&gt; file, or how do I build it?&lt;/P&gt;&lt;P&gt;Q4: Since the full build process is taking horribly long, is there any shorter re-entry point if I make the following changes for my coming projects?&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;Add some drivers to the Linux kernel&lt;/LI&gt;&lt;LI&gt;Change the hardware to:&lt;/LI&gt;&lt;/OL&gt;&lt;UL&gt;&lt;LI&gt;Ethernet PHY: RTL8211B 2.5G PHY (Also how to modify the device tree?)&lt;/LI&gt;&lt;LI&gt;SDHC1: SD Card&lt;/LI&gt;&lt;LI&gt;SDHC2: eMMC (Also how to modify the device tree?)&lt;/LI&gt;&lt;LI&gt;Boot Sequence: SD --&amp;gt; eMMC&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Steve&lt;/P&gt;</description>
      <pubDate>Wed, 11 Nov 2020 06:40:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1181257#M9844</guid>
      <dc:creator>Steve81800</dc:creator>
      <dc:date>2020-11-11T06:40:23Z</dc:date>
    </item>
    <item>
      <title>Re: FLEXBUILD-LS1012AFRWY Error</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1182719#M9855</link>
      <description>&lt;P&gt;Q2:&lt;/P&gt;
&lt;P&gt;The FRWY board schematics 30191 revs A and B had 512MB DDR3L. The Rev C board schematic has 256MB.&lt;BR /&gt;Rev A and B were early versions of this board.&lt;BR /&gt;The Rev C board has been shipping for a while now, and so a customer is more likely to have a Rev C.&lt;BR /&gt;&lt;BR /&gt;The boards are shipped with a sticker on the underside indicating the schematic "SCH" revision. For the Rev C board, the sticker says "SCH-32169 REV C". Please see attached photo.&lt;BR /&gt;&lt;BR /&gt;firmware_ls1012afrwy_512mb_uboot_qspiboot.img should be used if you have a Rev A or Rev B schematic board.&lt;BR /&gt;firmware_ls1012afrwy_uboot_qspiboot.img should be used if you have a SCH Rev C board.&lt;/P&gt;</description>
      <pubDate>Fri, 13 Nov 2020 02:35:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/FLEXBUILD-LS1012AFRWY-Error/m-p/1182719#M9855</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2020-11-13T02:35:19Z</dc:date>
    </item>
  </channel>
</rss>