<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SA604 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177863#M9776</link>
    <description>&lt;P&gt;Thanks for your reply and information.&lt;/P&gt;</description>
    <pubDate>Wed, 04 Nov 2020 10:02:10 GMT</pubDate>
    <dc:creator>Santhibhushan</dc:creator>
    <dc:date>2020-11-04T10:02:10Z</dc:date>
    <item>
      <title>SA604</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177307#M9768</link>
      <description>&lt;P&gt;I would like to use SA604A for FM demodulation. I have FM modulated signal at 2.4MHz. Can i give directly to IF AMP -IN (pin-16) and then from IF AMP -OUT(pin-14) to&amp;nbsp;pin-12 through 2.4MHz filter.&lt;/P&gt;&lt;P&gt;Can I get FM demodulated signal from pin-6 (audio out)? Also RSSI?&lt;/P&gt;</description>
      <pubDate>Tue, 03 Nov 2020 12:59:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177307#M9768</guid>
      <dc:creator>Santhibhushan</dc:creator>
      <dc:date>2020-11-03T12:59:39Z</dc:date>
    </item>
    <item>
      <title>Re: SA604</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177795#M9775</link>
      <description>&lt;P&gt;FM signal at 2.4MHz can be demodulated using SA604A as described. Typical data rate is up to 100kbit/s.&lt;/P&gt;
&lt;P&gt;Pin 7 (UNMUTE_AUD_OUTP) can be used for demodulated FM data stream. Pin 6 has similar function, but, it is more suitable for audio output since it support muting.&lt;/P&gt;
&lt;P&gt;RSSI signal can be used to control the level of the input signal or to demodulate ASK signal.&lt;/P&gt;
&lt;P&gt;Reference documents:&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1994.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1994.pdf&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1995.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1995.pdf&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1996.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1996.pdf&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1997.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1997.pdf&lt;/A&gt;&lt;BR /&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN1993.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN1993.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Pavel&lt;/P&gt;
&lt;P&gt;NXP TIC&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 09:05:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177795#M9775</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2020-11-04T09:05:20Z</dc:date>
    </item>
    <item>
      <title>Re: SA604</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177863#M9776</link>
      <description>&lt;P&gt;Thanks for your reply and information.&lt;/P&gt;</description>
      <pubDate>Wed, 04 Nov 2020 10:02:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SA604/m-p/1177863#M9776</guid>
      <dc:creator>Santhibhushan</dc:creator>
      <dc:date>2020-11-04T10:02:10Z</dc:date>
    </item>
  </channel>
</rss>