<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: MPC8360_INITIALIZATION issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8360-INITIALIZATION-issue/m-p/165898#M969</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PCI_MODE determines which pins the chip uses for its clock source.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In "PCI Host Mode" the CLKIN pin is the master clock. In "PCI Agent Mode" the PCI_CLK/PCI_SYNC_IN pin is the master clock.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't have PCI_MODE connected then the chip doesn't know which clock to use. Yes, not connecting it would explain why it won't initialise.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 13 Sep 2011 06:32:51 GMT</pubDate>
    <dc:creator>TomE</dc:creator>
    <dc:date>2011-09-13T06:32:51Z</dc:date>
    <item>
      <title>MPC8360_INITIALIZATION issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8360-INITIALIZATION-issue/m-p/165897#M968</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;I have used MPC8360 in a design.&lt;/P&gt;&lt;P&gt;However I am having issue in Initializing the processor using Code Warrior.&lt;/P&gt;&lt;P&gt;I have tried all RSW&amp;nbsp; modes from 000-111.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;There is a hardware fallacy that has been found.The PCI_MODE pin of the processor is&amp;nbsp; accidentaly not connected .According to Datasheet it must be connected to either VCC thru Pull up or pulled Down.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Just want to know clearly if not Connecting PCI_MODE pin can stop the processor from initializing.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have attched the debugger Log for reference.It seems that Processor is failing during Read Operation.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please provide some Pointers ASAP.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Sep 2011 18:30:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8360-INITIALIZATION-issue/m-p/165897#M968</guid>
      <dc:creator>rana_kspl</dc:creator>
      <dc:date>2011-09-09T18:30:50Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8360_INITIALIZATION issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8360-INITIALIZATION-issue/m-p/165898#M969</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;PCI_MODE determines which pins the chip uses for its clock source.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;In "PCI Host Mode" the CLKIN pin is the master clock. In "PCI Agent Mode" the PCI_CLK/PCI_SYNC_IN pin is the master clock.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If you don't have PCI_MODE connected then the chip doesn't know which clock to use. Yes, not connecting it would explain why it won't initialise.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Sep 2011 06:32:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8360-INITIALIZATION-issue/m-p/165898#M969</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2011-09-13T06:32:51Z</dc:date>
    </item>
  </channel>
</rss>