<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PN7150 High Bitrate in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1170517#M9663</link>
    <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using a PN7150 to communicate with an NFC endpoint that supports the ISO-DEP protocol. I was reading the user manual and it states that "... the ISO-DEP RF interface activation for technology NFC-A is incompatible with bit rates higher than 106kbps...". But it also states that higher bit rates can be used for NFC-A technologies.&lt;/P&gt;&lt;P&gt;Is there a workaround that will allow me to configure the transmission of the&amp;nbsp;PPS command by the Host or by the PN7150, to allow the higher bit-rates?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
    <pubDate>Tue, 20 Oct 2020 19:08:18 GMT</pubDate>
    <dc:creator>wilmer_suarez</dc:creator>
    <dc:date>2020-10-20T19:08:18Z</dc:date>
    <item>
      <title>PN7150 High Bitrate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1170517#M9663</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I'm using a PN7150 to communicate with an NFC endpoint that supports the ISO-DEP protocol. I was reading the user manual and it states that "... the ISO-DEP RF interface activation for technology NFC-A is incompatible with bit rates higher than 106kbps...". But it also states that higher bit rates can be used for NFC-A technologies.&lt;/P&gt;&lt;P&gt;Is there a workaround that will allow me to configure the transmission of the&amp;nbsp;PPS command by the Host or by the PN7150, to allow the higher bit-rates?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Tue, 20 Oct 2020 19:08:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1170517#M9663</guid>
      <dc:creator>wilmer_suarez</dc:creator>
      <dc:date>2020-10-20T19:08:18Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 High Bitrate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173233#M9704</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/82535"&gt;@wilmer_suarez&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Hope you are doing great, as you correctly state, the reader supports 106, 212,424 and 848 speeds, in the user manual you can also find in section 6.3.6 the explanation of this and a&amp;nbsp; part of the NCI specs,&amp;nbsp; how the&amp;nbsp;PI_BIT_RATE&amp;nbsp; can be used to do this.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jonathaniglesia_0-1603726485788.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128300i1310AA5CD9CE8CC2/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jonathaniglesia_0-1603726485788.png" alt="jonathaniglesia_0-1603726485788.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 15:34:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173233#M9704</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-10-26T15:34:51Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 High Bitrate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173268#M9705</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/65988"&gt;@Jonathan_Iglesias&lt;/a&gt;,&lt;/P&gt;&lt;P&gt;Section 6.3.6 also states:&lt;/P&gt;&lt;P&gt;"Everything is prepared (see the RF configuration parameter PI_BIT_RATE), &lt;STRONG&gt;except for the ISO-DEP RF Interface activation&lt;/STRONG&gt;. As currently defined in [NCI], the ISO-DEP RF interface activation for technology NFC-A is i&lt;STRONG&gt;ncompatible with bit rates higher than 106kbps&lt;/STRONG&gt;, since this requires to handle the PPS commands exchange, which is not addressed in [NCI]."&lt;/P&gt;&lt;P&gt;If I set the&amp;nbsp;PI_BIT_RATE to 848 kbps, would it maintain when communicating through the ISO-DEP RF interface?&lt;/P&gt;&lt;P&gt;If no, is there another way to handle the PPS exchange, either through the DH or the NFCC?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 16:48:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173268#M9705</guid>
      <dc:creator>wilmer_suarez</dc:creator>
      <dc:date>2020-10-26T16:48:50Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 High Bitrate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173355#M9708</link>
      <description>&lt;P&gt;yes you are correct, so in the same chapter there are some modifications&amp;nbsp; that are the ones I sent in my first reply:&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="jonathaniglesia_0-1603747518242.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/128323i9182C6B470F49E58/image-size/medium?v=v2&amp;amp;px=400" role="button" title="jonathaniglesia_0-1603747518242.png" alt="jonathaniglesia_0-1603747518242.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;so there is a little modifications (first reply) from the ISO-DEP.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Have a great day ! &lt;LI-EMOJI id="lia_grinning-face-with-smiling-eyes" title=":grinning_face_with_smiling_eyes:"&gt;&lt;/LI-EMOJI&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 21:26:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173355#M9708</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-10-26T21:26:03Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 High Bitrate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173380#M9710</link>
      <description>&lt;P&gt;Ah, sorry. I misunderstood the wording in the manual. So, by "an allowed value higher than 0x00" means any of the 4 standard rates?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 22:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173380#M9710</guid>
      <dc:creator>wilmer_suarez</dc:creator>
      <dc:date>2020-10-26T22:23:34Z</dc:date>
    </item>
    <item>
      <title>Re: PN7150 High Bitrate</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173382#M9711</link>
      <description>&lt;P&gt;yes that is correct, other value of bit rate.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Jonathan&lt;/P&gt;</description>
      <pubDate>Mon, 26 Oct 2020 22:26:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PN7150-High-Bitrate/m-p/1173382#M9711</guid>
      <dc:creator>Jonathan_Iglesias</dc:creator>
      <dc:date>2020-10-26T22:26:00Z</dc:date>
    </item>
  </channel>
</rss>