<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 Re: Cross Compilation in MPC8313RDB</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165029#M965</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Thanks abartky,&lt;BR /&gt;&lt;BR /&gt;Your information on compiling the packages is targetted for building a new kernel image and transferring this on to the board. In my case, I am looking at builing a kernel module which is going to be an addon module on the currently installed kernel. I am looking at building a module file (.ko) from a single .c file. I want to use it on the board. I do not want to change any currently installed packages or the board's kernel image. &lt;A href="http://forums.freescale.com/../view_profile?user.id=7103" rel="nofollow" target="_blank"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;thanks&lt;BR /&gt;Ak&lt;BR /&gt;&lt;BR /&gt;PS: I have built the same kernel module on the Desktop machine. I am trying to get the same on the MPC8313 board.&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 21 Nov 2007 02:26:22 GMT</pubDate>
    <dc:creator>ak79</dc:creator>
    <dc:date>2007-11-21T02:26:22Z</dc:date>
    <item>
      <title>Cross Compilation in MPC8313RDB</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165027#M963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Hi,&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;I am trying to build an Kernel module for MPC8313RDB on a suse machine. When I ran the make it did not generate .ko file (kernel module) and this does not give any kind of error or warning messages. I am not able to find where the error is or where I am going wrong. can some one please help me resolve this issue.&lt;BR /&gt;&lt;BR /&gt;MY computer OS: Suse 10.3 with 2.6.18 kernel&lt;BR /&gt;My Board OS: Linux with 2.6.20 kernel&lt;BR /&gt;&lt;BR /&gt;The makefile has:&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; KERNELDIR := /Board/ltib-mpc8313erdb-20070824/rootfs/lib/modules/2.6.20/build&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; PWD := $(shell pwd)&lt;BR /&gt;&lt;BR /&gt;default:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; $(MAKE) -C $(KERNELDIR) M=$(PWD) modules&lt;BR /&gt;&lt;BR /&gt;On running make command I see this:&lt;BR /&gt;&lt;BR /&gt;(none):/Board/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/driver # make&lt;BR /&gt;make -C /Board/ltib-mpc8313erdb-20070824/rootfs/lib/modules/2.6.20/build M=/Board/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/driver modules&lt;BR /&gt;make[1]: Entering directory `/Board/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20'&lt;BR /&gt;&amp;nbsp; Building modules, stage 2.&lt;BR /&gt;&amp;nbsp; MODPOST 0 modules&lt;BR /&gt;make[1]: Leaving directory `/Board/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20'&lt;BR /&gt;(none):/Board/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/driver #&lt;BR /&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;Ak&lt;BR /&gt;&lt;BR /&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Nov 2007 07:07:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165027#M963</guid>
      <dc:creator>ak79</dc:creator>
      <dc:date>2007-11-17T07:07:01Z</dc:date>
    </item>
    <item>
      <title>Re: Cross Compilation in MPC8313RDB</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165028#M964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;Ak,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;When it comes to compiling, building, etc. on the MPC8313E-RDB (or other Freescale boards) on a Linux Development system using the Freescale BSP, the key thing IMHO to remember is that what you need to do is build for the target, not the way that you usually build Linux where you are building for the same machine you are running on.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Because of that paradigm, if you go to a directory and try and run standard make, gcc, or other linux commands, they will execute in the context of building for your host machine, not as a cross compile.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;So IMHO, if you want to develop kernel or user mode programs for the MPC8313E-RDB, you will need to use the Freescale Linux Target Image Builder (LTIB), let it do the work as far as setting the right environment variables, using the right compiler, etc. and not try and setup all the environment variables, cross compilers, etc. on your own. In theory it probably could be done, but using LTIB is a lot less work.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;So for your case, where you wish to compile, build, etc. for the kernel, if you have edited your files correctly and make changes (assuming you've done the step of telling LTIB to build and leave the kernel sources), if you go to your LTIB main directory and type "./ltib" it will setup the proper environment variables, prep the kernel for building, compile, link, setup, etc. to the point where it creates a file call "uImage" which is the actual kernel to load on the target board.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;If you want to execute individual steps, LTIB allows for step by step development by allowing command line options when you call the ./ltib script. So for example, to do a step by step build of the kernel you can do an initial setup, compile and build by executing:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib -p kernel -m scbuild&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;To perform the "install step" (which does further setup of the kernel): you use:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib -p kernel -m scinstall&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;To perform the "deploy step" (which also calls the install step, and does the full binary build of the kernel): you use:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib -p kernel -m scdeploy&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;If you want to cut to the chase and just build the kernel as a complete step, but leave everything else alone, you can use:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib -p kernel&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;There is a pretty good description of the command line options and how to use them at &lt;A href="https://community.nxp.com/www.bitshrine.org" target="test_blank"&gt;www.bitshrine.org&lt;/A&gt; which is the home page for the open source LTIB. In particular, you should download and read the instructions from the FAQ. Here is the direct link to it:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;A href="http://www.bitshrine.org/autodocs/LtibFaq.html" rel="nofollow" target="_blank"&gt;http://www.bitshrine.org/autodocs/LtibFaq.html&lt;/A&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;In particular pay attention to the steps mentioned in the "How do I make changes to a package and capture them" section which lists the step by step process of using LTIB (the kernel is treated as a single package).&lt;/P&gt;&lt;P&gt;In my case I have made several modifications to the Ethernet/IEEE-1588 gianfar.c code for my project and have used the above steps when I do my incremental compiles and builds for my MPC8313E-RDB kernel modifications.&lt;/P&gt;&lt;P&gt;Hope this helps :smileyhappy:&lt;/P&gt;&lt;P&gt;Cheers,&lt;/P&gt;&lt;P&gt;abartky&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Nov 2007 09:17:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165028#M964</guid>
      <dc:creator>abartky</dc:creator>
      <dc:date>2007-11-17T09:17:00Z</dc:date>
    </item>
    <item>
      <title>Re: Cross Compilation in MPC8313RDB</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165029#M965</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Thanks abartky,&lt;BR /&gt;&lt;BR /&gt;Your information on compiling the packages is targetted for building a new kernel image and transferring this on to the board. In my case, I am looking at builing a kernel module which is going to be an addon module on the currently installed kernel. I am looking at building a module file (.ko) from a single .c file. I want to use it on the board. I do not want to change any currently installed packages or the board's kernel image. &lt;A href="http://forums.freescale.com/../view_profile?user.id=7103" rel="nofollow" target="_blank"&gt;&lt;SPAN&gt;&lt;/SPAN&gt;&lt;/A&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;BR /&gt;thanks&lt;BR /&gt;Ak&lt;BR /&gt;&lt;BR /&gt;PS: I have built the same kernel module on the Desktop machine. I am trying to get the same on the MPC8313 board.&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Nov 2007 02:26:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Cross-Compilation-in-MPC8313RDB/m-p/165029#M965</guid>
      <dc:creator>ak79</dc:creator>
      <dc:date>2007-11-21T02:26:22Z</dc:date>
    </item>
  </channel>
</rss>