<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Write custom data to flash in LPC55S28 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Write-custom-data-to-flash-in-LPC55S28/m-p/1161599#M9506</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to write custom data to LPC55S28 flash area and treating it like writing to EEPROM? If yes, is there any sample code that I can refer to?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ridzuan&lt;/P&gt;</description>
    <pubDate>Thu, 01 Oct 2020 03:28:47 GMT</pubDate>
    <dc:creator>Ridzuan</dc:creator>
    <dc:date>2020-10-01T03:28:47Z</dc:date>
    <item>
      <title>Write custom data to flash in LPC55S28</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Write-custom-data-to-flash-in-LPC55S28/m-p/1161599#M9506</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is it possible to write custom data to LPC55S28 flash area and treating it like writing to EEPROM? If yes, is there any sample code that I can refer to?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Ridzuan&lt;/P&gt;</description>
      <pubDate>Thu, 01 Oct 2020 03:28:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Write-custom-data-to-flash-in-LPC55S28/m-p/1161599#M9506</guid>
      <dc:creator>Ridzuan</dc:creator>
      <dc:date>2020-10-01T03:28:47Z</dc:date>
    </item>
    <item>
      <title>Re: Write custom data to flash in LPC55S28</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Write-custom-data-to-flash-in-LPC55S28/m-p/1163022#M9531</link>
      <description>&lt;P&gt;Hello ,&lt;/P&gt;
&lt;P&gt;Hope you are doing well.&lt;/P&gt;
&lt;P&gt;I'd recommend to check our examples in the SDK. Many make use of the flash area. In addition if you would like to use different commands in the flash to store data, you may refer to the flashiap1 example in the driver_examples folder when importing an SDK example.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-center" image-alt="nxf51209_0-1601914811026.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/126770i01BD96589C5B9B8B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="nxf51209_0-1601914811026.png" alt="nxf51209_0-1601914811026.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Here you will find an example to write, read and erase blocks in the flash area.&lt;/P&gt;
&lt;P&gt;Hope this helps!&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Sabina&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;
&lt;P&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;/P&gt;
&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 05 Oct 2020 16:20:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Write-custom-data-to-flash-in-LPC55S28/m-p/1163022#M9531</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-10-05T16:20:56Z</dc:date>
    </item>
  </channel>
</rss>