<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックPWM  CHIP TEA1751T</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-CHIP-TEA1751T/m-p/1150144#M9243</link>
    <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Failed production module replicated on the Production floor by Engineering&lt;/P&gt;&lt;P&gt;Engineer considered the temperature variable to be a possible cause&lt;/P&gt;&lt;P&gt;MOD temperature taken down to 10degrees C in the oven and power on test attempted.&amp;nbsp; MOD failed to power on.&lt;/P&gt;&lt;P&gt;Repeatable results from the same batch allowed Engineering to identify a replicate of the failure mode consistently.&lt;/P&gt;&lt;P&gt;Engineering have determined a contributing component to be PWM chip TEA1751 (ACP100326) found in multiple 3A and 5A Litone MODs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;PWM Chip alone is not the only cause – this was proved by swapping the chip from a failed MOD with a MOD that passed:&lt;/P&gt;&lt;P&gt;1.Swapping chip between a PASSING and FAILING PCA above and applied direct cooling of chip and 10°C oven test&lt;BR /&gt;Swapped the TEA1751T PWM chip from a “PASSING” G2405N,Sept 2019, board to a “FAILING” G2403N April 2020 the results were:&lt;/P&gt;&lt;P&gt;–Managed to induce a fail on the G2405N with G2403N TEA1751T but this was much more difficult and appeared to only pass through a failure temperature when warming-up from being cooled&lt;/P&gt;&lt;P&gt;–G2405N PASSED with the swapped TEA1751T from FAILED G2403N&lt;BR /&gt;And&lt;BR /&gt;G2403N PASSED with the swapped TEA1751T from PASSED G2405N&lt;/P&gt;&lt;P&gt;When testing at board level it was confirmed that the PWM chip TEA1751T (ACP100326) was sensitive to cold and could be cooled directly to FAIL on the G2403N April 2020&lt;BR /&gt;The G2405N PCA could not be made to fail cooling the chip directly&lt;/P&gt;&lt;P&gt;What has changed? Is the chip performing as per its specification?&amp;nbsp; If not, what has changed? What else has changed to make this issue become more apparent now?&lt;/P&gt;&lt;P&gt;Could NXP support us in creating a screening method for the chip or improve their screening? Have they seen this issue with other customers?&lt;/P&gt;</description>
    <pubDate>Tue, 08 Sep 2020 07:27:21 GMT</pubDate>
    <dc:creator>William777</dc:creator>
    <dc:date>2020-09-08T07:27:21Z</dc:date>
    <item>
      <title>PWM  CHIP TEA1751T</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-CHIP-TEA1751T/m-p/1150144#M9243</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Failed production module replicated on the Production floor by Engineering&lt;/P&gt;&lt;P&gt;Engineer considered the temperature variable to be a possible cause&lt;/P&gt;&lt;P&gt;MOD temperature taken down to 10degrees C in the oven and power on test attempted.&amp;nbsp; MOD failed to power on.&lt;/P&gt;&lt;P&gt;Repeatable results from the same batch allowed Engineering to identify a replicate of the failure mode consistently.&lt;/P&gt;&lt;P&gt;Engineering have determined a contributing component to be PWM chip TEA1751 (ACP100326) found in multiple 3A and 5A Litone MODs.&amp;nbsp;&lt;/P&gt;&lt;P&gt;PWM Chip alone is not the only cause – this was proved by swapping the chip from a failed MOD with a MOD that passed:&lt;/P&gt;&lt;P&gt;1.Swapping chip between a PASSING and FAILING PCA above and applied direct cooling of chip and 10°C oven test&lt;BR /&gt;Swapped the TEA1751T PWM chip from a “PASSING” G2405N,Sept 2019, board to a “FAILING” G2403N April 2020 the results were:&lt;/P&gt;&lt;P&gt;–Managed to induce a fail on the G2405N with G2403N TEA1751T but this was much more difficult and appeared to only pass through a failure temperature when warming-up from being cooled&lt;/P&gt;&lt;P&gt;–G2405N PASSED with the swapped TEA1751T from FAILED G2403N&lt;BR /&gt;And&lt;BR /&gt;G2403N PASSED with the swapped TEA1751T from PASSED G2405N&lt;/P&gt;&lt;P&gt;When testing at board level it was confirmed that the PWM chip TEA1751T (ACP100326) was sensitive to cold and could be cooled directly to FAIL on the G2403N April 2020&lt;BR /&gt;The G2405N PCA could not be made to fail cooling the chip directly&lt;/P&gt;&lt;P&gt;What has changed? Is the chip performing as per its specification?&amp;nbsp; If not, what has changed? What else has changed to make this issue become more apparent now?&lt;/P&gt;&lt;P&gt;Could NXP support us in creating a screening method for the chip or improve their screening? Have they seen this issue with other customers?&lt;/P&gt;</description>
      <pubDate>Tue, 08 Sep 2020 07:27:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-CHIP-TEA1751T/m-p/1150144#M9243</guid>
      <dc:creator>William777</dc:creator>
      <dc:date>2020-09-08T07:27:21Z</dc:date>
    </item>
    <item>
      <title>Re: PWM  CHIP TEA1751T</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PWM-CHIP-TEA1751T/m-p/1151022#M9258</link>
      <description>&lt;P&gt;Hi William,&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#000000"&gt;we have received a similar request from ELMEDENE, from Edward&lt;SPAN&gt;. I have sent the description of the issue to a quality engineer. For his answer please see the description.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;DESCRIPTION&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;FONT color="#00CCFF"&gt;Checking with testfab where the customer need to ship the samples, will let you know.&lt;/FONT&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;With Best Regards,&lt;/P&gt;
&lt;P&gt;Jozef&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 09 Sep 2020 10:18:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PWM-CHIP-TEA1751T/m-p/1151022#M9258</guid>
      <dc:creator>JozefKozon</dc:creator>
      <dc:date>2020-09-09T10:18:51Z</dc:date>
    </item>
  </channel>
</rss>