<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Zigbee Test Client (ZTC)  Serial Port protocol Description in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Zigbee-Test-Client-ZTC-Serial-Port-protocol-Description/m-p/163254#M911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the OTA Update feature offered by the latest Beekit version to update the firmware of MC1322x Boards.&lt;/P&gt;&lt;P&gt;This is the scenario: I have a NCB that act as an OTA Server and an SRB that act as an OTA Client.&lt;/P&gt;&lt;P&gt;If I use Test Tool 12.0.0 to update the firmware of the SRB board everything works fine and I can change the firmware of the SRB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Test Tool is&amp;nbsp;available﻿ only for Windows OS and I need to connect the boards to a Linux machine.&lt;/P&gt;&lt;P&gt;So&amp;nbsp;I'm trying to write an app under Linux OS (Ubuntu 11.04) to interact with the NCB over the UART and use the OTA update feature.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any reference manual that explains which is the protocol used by ZTC to communicate over the UART.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 30 Aug 2011 19:54:44 GMT</pubDate>
    <dc:creator>Loris83</dc:creator>
    <dc:date>2011-08-30T19:54:44Z</dc:date>
    <item>
      <title>Zigbee Test Client (ZTC)  Serial Port protocol Description</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Zigbee-Test-Client-ZTC-Serial-Port-protocol-Description/m-p/163254#M911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the OTA Update feature offered by the latest Beekit version to update the firmware of MC1322x Boards.&lt;/P&gt;&lt;P&gt;This is the scenario: I have a NCB that act as an OTA Server and an SRB that act as an OTA Client.&lt;/P&gt;&lt;P&gt;If I use Test Tool 12.0.0 to update the firmware of the SRB board everything works fine and I can change the firmware of the SRB.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Test Tool is&amp;nbsp;available﻿ only for Windows OS and I need to connect the boards to a Linux machine.&lt;/P&gt;&lt;P&gt;So&amp;nbsp;I'm trying to write an app under Linux OS (Ubuntu 11.04) to interact with the NCB over the UART and use the OTA update feature.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there any reference manual that explains which is the protocol used by ZTC to communicate over the UART.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 30 Aug 2011 19:54:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Zigbee-Test-Client-ZTC-Serial-Port-protocol-Description/m-p/163254#M911</guid>
      <dc:creator>Loris83</dc:creator>
      <dc:date>2011-08-30T19:54:44Z</dc:date>
    </item>
    <item>
      <title>Re: Zigbee Test Client (ZTC)  Serial Port protocol Description</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Zigbee-Test-Client-ZTC-Serial-Port-protocol-Description/m-p/163255#M912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;OTAP structure is described here, for the structure see capter 2&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/rf_if/doc/user_guide/802154MACOTAPUG.pdf?fsrch=1&amp;amp;sr=1" rel="nofollow" target="_blank"&gt;http://cache.freescale.com/files/rf_if/doc/user_guide/802154MACOTAPUG.pdf?fsrch=1&amp;amp;sr=1&lt;/A&gt;&lt;/P&gt;&lt;P&gt;hope this will help&lt;/P&gt;&lt;P&gt;Pavel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Jan 2012 06:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Zigbee-Test-Client-ZTC-Serial-Port-protocol-Description/m-p/163255#M912</guid>
      <dc:creator>pavel_sadek</dc:creator>
      <dc:date>2012-01-11T06:05:50Z</dc:date>
    </item>
  </channel>
</rss>