<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCA9685 LED Registers in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9685-LED-Registers/m-p/1080770#M9086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PCA9685 datasheet states under heading "7.3.4 ALL_LED_ON and ALL_LED_OFF control" the following: "The LEDn_ON and LEDnOFF counts can vary from 0 to 4095. The LEDn_ON and LEDn_OFF count registers should never be programmed with the same values."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an experiment, we set LEDn_ON to 0 and LEDn_OFF to 0, and the result was 0 output, the same as setting bit4 of the LEDn_OFF_H register. So, it is almost as if the Full Off bit is not required.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, to get full on, bit4 of the LEDn_ON_H register does need to be set to get full output. Otherwise, you get 1 cycle of off condition for "FFF".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 11 Aug 2020 21:28:07 GMT</pubDate>
    <dc:creator>tba10596</dc:creator>
    <dc:date>2020-08-11T21:28:07Z</dc:date>
    <item>
      <title>PCA9685 LED Registers</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9685-LED-Registers/m-p/1080769#M9085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;All:&lt;/P&gt;&lt;P&gt;I am going to state an assumption - please tell me if I am correct.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE class="j-table jiveBorder" style="border: 1px solid #c6c6c6;" width="100%"&gt;&lt;THEAD&gt;&lt;TR style="background-color: #efefef;"&gt;&lt;TH&gt;&lt;/TH&gt;&lt;TH&gt;Zero&lt;/TH&gt;&lt;TH&gt;Max&lt;/TH&gt;&lt;TH&gt;PWM&lt;/TH&gt;&lt;/TR&gt;&lt;/THEAD&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;LEDn_ON_L&lt;/TD&gt;&lt;TD&gt;0x00&lt;/TD&gt;&lt;TD&gt;0x00&lt;/TD&gt;&lt;TD&gt;0x00&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;SPAN&gt;LEDn_ON_H&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD&gt;0x00&lt;/TD&gt;&lt;TD&gt;0x10&amp;nbsp;&lt;/TD&gt;&lt;TD&gt;0x00&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;SPAN&gt;LEDn_OFF_L&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD&gt;0x00&lt;/TD&gt;&lt;TD&gt;0xFF&lt;/TD&gt;&lt;TD&gt;0xWM&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;&lt;SPAN&gt;LEDn_OFF_H&lt;/SPAN&gt;&lt;/TD&gt;&lt;TD&gt;0x10&amp;nbsp;&lt;/TD&gt;&lt;TD&gt;0x0F&lt;/TD&gt;&lt;TD&gt;0x0P&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. If I want zero output, I need to set bit 4 in the LEDn_OFF_H. All other contents of these 4 registers are ignored by PCA chip.&lt;/P&gt;&lt;P&gt;2. If I want max output, I need to set bit 4 in the LEDn_ON_H. Again, all other contents are ignored by PCA chip.&lt;/P&gt;&lt;P&gt;3. A valid PWM is greater than 0 and less than 0xFFF (12-bit max number).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Todd Anderson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 18:25:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9685-LED-Registers/m-p/1080769#M9085</guid>
      <dc:creator>tba10596</dc:creator>
      <dc:date>2020-08-10T18:25:34Z</dc:date>
    </item>
    <item>
      <title>Re: PCA9685 LED Registers</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCA9685-LED-Registers/m-p/1080770#M9086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The PCA9685 datasheet states under heading "7.3.4 ALL_LED_ON and ALL_LED_OFF control" the following: "The LEDn_ON and LEDnOFF counts can vary from 0 to 4095. The LEDn_ON and LEDn_OFF count registers should never be programmed with the same values."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As an experiment, we set LEDn_ON to 0 and LEDn_OFF to 0, and the result was 0 output, the same as setting bit4 of the LEDn_OFF_H register. So, it is almost as if the Full Off bit is not required.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, to get full on, bit4 of the LEDn_ON_H register does need to be set to get full output. Otherwise, you get 1 cycle of off condition for "FFF".&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 21:28:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCA9685-LED-Registers/m-p/1080770#M9086</guid>
      <dc:creator>tba10596</dc:creator>
      <dc:date>2020-08-11T21:28:07Z</dc:date>
    </item>
  </channel>
</rss>