<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: enable boot partion 1 to boot MFGTOOLs in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/enable-boot-partion-1-to-boot-MFGTOOLs/m-p/1072431#M9033</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;SUNASIR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just for test one can try to run these commands from linux, as mfg tool is small linux image.&lt;/P&gt;&lt;P&gt;Also one can look at other emmc programming options:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/programming-emmc-on-i-mx6/" title="https://boundarydevices.com/programming-emmc-on-i-mx6/"&gt;https://boundarydevices.com/programming-emmc-on-i-mx6/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 08 Aug 2020 12:05:48 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2020-08-08T12:05:48Z</dc:date>
    <item>
      <title>enable boot partion 1 to boot MFGTOOLs</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/enable-boot-partion-1-to-boot-MFGTOOLs/m-p/1072430#M9032</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;while rootfs i mx 6 sololite board by mfgtools&amp;nbsp; following error is showing.&lt;/P&gt;&lt;P&gt;32768, 98304, 163840, 229376, 294912, 819200, 884736, 1605632&lt;/P&gt;&lt;P&gt;Writing inode tables: done&lt;BR /&gt;Creating journal (32768 blocks): done&lt;BR /&gt;Writing superblocks and filesystem accounting information: done&lt;/P&gt;&lt;P&gt;This filesystem will be automatically checked every 32 mounts or&lt;BR /&gt;180 days, whichever comes first. Use tune2fs -c or -i to override.&lt;BR /&gt;UTP: sending Success to kernel for command $ sh mksdcard.sh /dev/mmcblk0.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ sleep 8'&lt;BR /&gt;UTP: executing "sleep 8"&lt;BR /&gt;UTP: sending Success to kernel for command $ sleep 8.&lt;BR /&gt;utp_poll: pass returned.&lt;BR /&gt;UTP: received command '$ echo 8 &amp;gt; /sys/devices/platform/sdhci-esdhc-imx.1/mmc_ho&lt;BR /&gt;st/mmc1/mmc1:0001/boot_config '&lt;BR /&gt;UTP: executing "echo 8 &amp;gt; /sys/devices/platform/sdhci-esdhc-imx.1/mmc_host/mmc1/m&lt;BR /&gt;mc1:0001/boot_config "&lt;BR /&gt;sh: can't create /sys/devices/platform/sdhci-esdhc-imx.1/mmc_host/mmc1/mmc1:0001&lt;BR /&gt;/boot_config: nonexistent directory&lt;BR /&gt;UTP: sending Non-success to kernel for command $ echo 8 &amp;gt; /sys/devices/platform/&lt;BR /&gt;sdhci-esdhc-imx.1/mmc_host/mmc1/mmc1:0001/boot_config .&lt;BR /&gt;utp_poll: exit with status 256&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 07 Aug 2020 14:11:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/enable-boot-partion-1-to-boot-MFGTOOLs/m-p/1072430#M9032</guid>
      <dc:creator>sunasir333</dc:creator>
      <dc:date>2020-08-07T14:11:58Z</dc:date>
    </item>
    <item>
      <title>Re: enable boot partion 1 to boot MFGTOOLs</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/enable-boot-partion-1-to-boot-MFGTOOLs/m-p/1072431#M9033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;SUNASIR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;just for test one can try to run these commands from linux, as mfg tool is small linux image.&lt;/P&gt;&lt;P&gt;Also one can look at other emmc programming options:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://boundarydevices.com/programming-emmc-on-i-mx6/" title="https://boundarydevices.com/programming-emmc-on-i-mx6/"&gt;https://boundarydevices.com/programming-emmc-on-i-mx6/&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 08 Aug 2020 12:05:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/enable-boot-partion-1-to-boot-MFGTOOLs/m-p/1072431#M9033</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2020-08-08T12:05:48Z</dc:date>
    </item>
  </channel>
</rss>