<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic PCF2129T Battery Issue in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044303#M8829</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom board, need a date and time datas so I am using PCF2129T with I2C communication. I am using 3.3V CR2032 cells. The problem is that, when I plug a cell lower than 3.3V, system is ok, working properly but if cell's voltage is over 3.3V all datas are being zero, all registers become 0. What could be the problem ?&amp;nbsp; You can see the schematic below, +VBAT is connected to VBAT pin of LPC54608.&amp;nbsp;&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;Tried it two different modes, results same:&lt;/P&gt;&lt;P&gt;000&amp;nbsp; :&amp;nbsp;battery switch-over function is enabled in standard mode; battery low detection function is enabled&lt;/P&gt;&lt;P&gt;011&amp;nbsp; :&amp;nbsp;battery switch-over function is enabled in direct switching mode; battery low detection function is enabled&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115772i814757173DF055B6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2020 11:42:30 GMT</pubDate>
    <dc:creator>fatihozen</dc:creator>
    <dc:date>2020-07-14T11:42:30Z</dc:date>
    <item>
      <title>PCF2129T Battery Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044303#M8829</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a custom board, need a date and time datas so I am using PCF2129T with I2C communication. I am using 3.3V CR2032 cells. The problem is that, when I plug a cell lower than 3.3V, system is ok, working properly but if cell's voltage is over 3.3V all datas are being zero, all registers become 0. What could be the problem ?&amp;nbsp; You can see the schematic below, +VBAT is connected to VBAT pin of LPC54608.&amp;nbsp;&lt;/P&gt;&lt;P&gt;(&lt;/P&gt;&lt;P&gt;Tried it two different modes, results same:&lt;/P&gt;&lt;P&gt;000&amp;nbsp; :&amp;nbsp;battery switch-over function is enabled in standard mode; battery low detection function is enabled&lt;/P&gt;&lt;P&gt;011&amp;nbsp; :&amp;nbsp;battery switch-over function is enabled in direct switching mode; battery low detection function is enabled&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/115772i814757173DF055B6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2020 11:42:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044303#M8829</guid>
      <dc:creator>fatihozen</dc:creator>
      <dc:date>2020-07-14T11:42:30Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2129T Battery Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044304#M8830</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Disconnect the VBAT with LPC54608 and promise the VDD/VBAT is always on when do this test.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2020 03:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044304#M8830</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-07-15T03:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2129T Battery Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044305#M8831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is on the PCB, How can I disconnect Vbat with LPC54608 ? Is this hardware problem ?&amp;nbsp;Could be there any solution with software ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2020 05:04:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044305#M8831</guid>
      <dc:creator>fatihozen</dc:creator>
      <dc:date>2020-07-16T05:04:35Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2129T Battery Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044306#M8832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If no power on reset event,this issue will no happen,so need you check the power path.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jul 2020 06:16:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2129T-Battery-Issue/m-p/1044306#M8832</guid>
      <dc:creator>guoweisun</dc:creator>
      <dc:date>2020-07-16T06:16:13Z</dc:date>
    </item>
  </channel>
</rss>