<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Ethernet throughput using LWIP + FreeRTOS in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-throughput-using-LWIP-FreeRTOS/m-p/1037917#M8780</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing the ethernet throughput of NxP LPC54018 MCU on OM40003 development board and observing poor throughput.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Environment details:&lt;/STRONG&gt;&lt;BR /&gt;Tool: MCUXpresso v 11.0.0 build Id 2516&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Project details:&lt;/STRONG&gt;&lt;BR /&gt;Selected MCU LPC54018&lt;BR /&gt;Target board not selected&lt;BR /&gt;Selected Device package: LPC54018JET180&lt;BR /&gt;Operating System: Amazon-FreeRTOS (10.2.0)&lt;BR /&gt;Drivers: lpc_enet (2.1.3) in addition to other auto select drivers.&lt;BR /&gt;CMSIS Drivers: None&lt;BR /&gt;Utilities: None&lt;BR /&gt;Middleware: LwIP TCPIP Networking Stack (2.1.2)&lt;BR /&gt;Board Components: phylan8720a(1.0.0)&lt;BR /&gt;Abstraction Layer: None&lt;BR /&gt;Software ComponentsL None&lt;BR /&gt;Library Type(and hosting variant): Redlib(none)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the above settings of the project and referring SDK example project "lpcxpresso54018_lwip_ping_freertos" I created application which sends ICMP ping echo to a target IP address using lwip_sendto( ) API in while loop.&lt;/P&gt;&lt;P&gt;The time taken for lwip_sendto() to execute and come out for next call in loop is more than 20 milliseconds as can be seen from wireshark logs in the screenshot and also when I measured using timer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any&amp;nbsp;suggestions on what settings are required for achieving best througput?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards&lt;BR /&gt;Mayoor&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103356i5BD2A8E2157A6774/image-size/large?v=v2&amp;amp;px=999" title="LPC54018 ethernet throughput_001.png" alt="LPC54018 ethernet throughput_001.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 03 Mar 2020 07:21:59 GMT</pubDate>
    <dc:creator>mayoor_p</dc:creator>
    <dc:date>2020-03-03T07:21:59Z</dc:date>
    <item>
      <title>Ethernet throughput using LWIP + FreeRTOS</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-throughput-using-LWIP-FreeRTOS/m-p/1037917#M8780</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am testing the ethernet throughput of NxP LPC54018 MCU on OM40003 development board and observing poor throughput.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Environment details:&lt;/STRONG&gt;&lt;BR /&gt;Tool: MCUXpresso v 11.0.0 build Id 2516&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Project details:&lt;/STRONG&gt;&lt;BR /&gt;Selected MCU LPC54018&lt;BR /&gt;Target board not selected&lt;BR /&gt;Selected Device package: LPC54018JET180&lt;BR /&gt;Operating System: Amazon-FreeRTOS (10.2.0)&lt;BR /&gt;Drivers: lpc_enet (2.1.3) in addition to other auto select drivers.&lt;BR /&gt;CMSIS Drivers: None&lt;BR /&gt;Utilities: None&lt;BR /&gt;Middleware: LwIP TCPIP Networking Stack (2.1.2)&lt;BR /&gt;Board Components: phylan8720a(1.0.0)&lt;BR /&gt;Abstraction Layer: None&lt;BR /&gt;Software ComponentsL None&lt;BR /&gt;Library Type(and hosting variant): Redlib(none)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With the above settings of the project and referring SDK example project "lpcxpresso54018_lwip_ping_freertos" I created application which sends ICMP ping echo to a target IP address using lwip_sendto( ) API in while loop.&lt;/P&gt;&lt;P&gt;The time taken for lwip_sendto() to execute and come out for next call in loop is more than 20 milliseconds as can be seen from wireshark logs in the screenshot and also when I measured using timer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any&amp;nbsp;suggestions on what settings are required for achieving best througput?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;With Regards&lt;BR /&gt;Mayoor&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103356i5BD2A8E2157A6774/image-size/large?v=v2&amp;amp;px=999" title="LPC54018 ethernet throughput_001.png" alt="LPC54018 ethernet throughput_001.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 03 Mar 2020 07:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-throughput-using-LWIP-FreeRTOS/m-p/1037917#M8780</guid>
      <dc:creator>mayoor_p</dc:creator>
      <dc:date>2020-03-03T07:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet throughput using LWIP + FreeRTOS</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-throughput-using-LWIP-FreeRTOS/m-p/1037918#M8781</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Mayoor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know that the Ethernet is bus architecture, all nodes have the same priority, each node uses Carrier-sense multiple access with collision detection method to access Ethernet, I do not think there is method to increase the througput via software configuration.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 09:46:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Ethernet-throughput-using-LWIP-FreeRTOS/m-p/1037918#M8781</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-03-18T09:46:46Z</dc:date>
    </item>
  </channel>
</rss>