<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic floating point in mamba in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/floating-point-in-mamba/m-p/162256#M862</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using mpc5674&amp;nbsp;mamba, and noticed there is no exception happens when dividing by 0:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int i=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i=1/i&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The result of above code is i=0x7fffffff, and no exception.&lt;/P&gt;&lt;P&gt;From assemble code, compiler uses divw for the division. divw does not update overflow flow.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I expect to have exception for dividing by 0, what should I configure to enable this exception? or what kind of compiling option should be used to guarantee this exception?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 Aug 2011 01:15:05 GMT</pubDate>
    <dc:creator>sadou</dc:creator>
    <dc:date>2011-08-26T01:15:05Z</dc:date>
    <item>
      <title>floating point in mamba</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/floating-point-in-mamba/m-p/162256#M862</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using mpc5674&amp;nbsp;mamba, and noticed there is no exception happens when dividing by 0:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;int i=0;&lt;/P&gt;&lt;P&gt;&amp;nbsp; i=1/i&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The result of above code is i=0x7fffffff, and no exception.&lt;/P&gt;&lt;P&gt;From assemble code, compiler uses divw for the division. divw does not update overflow flow.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If I expect to have exception for dividing by 0, what should I configure to enable this exception? or what kind of compiling option should be used to guarantee this exception?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Aug 2011 01:15:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/floating-point-in-mamba/m-p/162256#M862</guid>
      <dc:creator>sadou</dc:creator>
      <dc:date>2011-08-26T01:15:05Z</dc:date>
    </item>
    <item>
      <title>Re: floating point in mamba</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/floating-point-in-mamba/m-p/162257#M863</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Power architecture has never had a divide-by-zero exception. If you want one then the compiler has to generate code to check the divisor before performing the division. Possibly with "twequi".&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; If I expect to have exception for dividing by 0, what should I configure to&lt;/P&gt;&lt;P&gt;&amp;gt; enable this exception?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;If the CPU has floating point hardware, then there's an enable for a floating point divide-by-zero exception, but you're wanting the integer one to trap.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;gt; or what kind of compiling option should be used to guarantee this exception?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Depends on the compiler. Read all the documentaiton on it, or ask in a forum specific to that compiler.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Of course you should have asked Google, which for "ppc divide zero trap gcc" finds:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://fixunix.com/embedded/341544-divide-zero-does-not-crash.html" rel="nofollow noopener noreferrer noopener noreferrer" target="_blank"&gt;http://fixunix.com/embedded/341544-divide-zero-does-not-crash.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;PRE&gt;The behavior of integer division by 0 is undefined per the C Languagestandard and, hence, implementation-dependent. On x86, division by 0produces a hardware exception. On x86 linux, this exception is presentedto the program as a signal. However, a conforming implementation maychoose to do anything else that is convenient: nothing (leave quotientunmodified), produce random value for the quotient, kill the process.

---

Yes, that's a property of the PowerPC archictecture. AFAIK the theory
 of the hardware designers was that the compiler should produce code
 equivalent to:

 q=n/d;
 if (d == 0)
 raise(SIGFPE);

 The idea is that the check would be performed during the latency of
 the division, so it would usually not cost extra time. So one could
 make the hardware simpler by not putting in the check there. I may be
 confusing PowerPC with another RISC architecture (most likely MIPS)
 wrt this aspect, though.&lt;/PRE&gt;&lt;P&gt;If you want to have divide-by-zeros trap in conforming C code, then you have to add tests on the divisor, or call a function to perform all divides and have it check, or use C++ and overload the "/" operator.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Oct 2020 09:08:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/floating-point-in-mamba/m-p/162257#M863</guid>
      <dc:creator>TomE</dc:creator>
      <dc:date>2020-10-29T09:08:04Z</dc:date>
    </item>
  </channel>
</rss>