<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP Products中的主题 LPC1763 UART DMA Issue</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/LPC1763-UART-DMA-Issue/m-p/1009419#M8518</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LPC1763. Already verified the UART operation on my product. Now needs to use DMA for UART, especially UART0. Based on the&amp;nbsp;example code provided by NXP, upated my source code. While I transmit data through UART0 by using DMA, I am not getting the expected data at the receive side of the other device. I am only receiving the value 0xFF. My message packet contains 0xFF as a first byte, maybe I am receiving only one byte data in the other side. Verified the transfer size set in the register, everything looks fine. Also to mention I am getting DMA interrupt for every Tx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 24 Mar 2020 13:48:03 GMT</pubDate>
    <dc:creator>balakrishnan_ch</dc:creator>
    <dc:date>2020-03-24T13:48:03Z</dc:date>
    <item>
      <title>LPC1763 UART DMA Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LPC1763-UART-DMA-Issue/m-p/1009419#M8518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using LPC1763. Already verified the UART operation on my product. Now needs to use DMA for UART, especially UART0. Based on the&amp;nbsp;example code provided by NXP, upated my source code. While I transmit data through UART0 by using DMA, I am not getting the expected data at the receive side of the other device. I am only receiving the value 0xFF. My message packet contains 0xFF as a first byte, maybe I am receiving only one byte data in the other side. Verified the transfer size set in the register, everything looks fine. Also to mention I am getting DMA interrupt for every Tx.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2020 13:48:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LPC1763-UART-DMA-Issue/m-p/1009419#M8518</guid>
      <dc:creator>balakrishnan_ch</dc:creator>
      <dc:date>2020-03-24T13:48:03Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1763 UART DMA Issue</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/LPC1763-UART-DMA-Issue/m-p/1009420#M8519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Balakrishnan,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you transmit a character repeatedly for example 'A' via DMA mode, then use a scope or logic analyzer to test the TX pin of uart, you can confirm if the DMA transmitted character correctly.&lt;/P&gt;&lt;P&gt;You can post the code so that we can have a review.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Mar 2020 07:22:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/LPC1763-UART-DMA-Issue/m-p/1009420#M8519</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-03-25T07:22:38Z</dc:date>
    </item>
  </channel>
</rss>