<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Getting necessary files for setting up environment for PWM (Pulse Width Modulation) using MPC5567 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161044#M831</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey there!&lt;/P&gt;&lt;P&gt;Im just about to learn how to control a motor with the MPC5567 and now Im gonna obtain the files I need to do my compilations. Problem is, I cant find the listed files in the following pwm readme file that tells me to download them from the freescale homepage. Here is the readme ==&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;This is release 2.0 of the PWM API and example files.&lt;BR /&gt;The user should refer to Application Note AN2849 "Using the Pulse Width&lt;BR /&gt;Modulation (PWM) eTPU Function" which is available from Freescale.&lt;BR /&gt;&lt;BR /&gt;This is a first release of the API without exmaple programs.&lt;BR /&gt;_____________________________________________________________________________&lt;BR /&gt;&lt;BR /&gt;Files included in this package:&lt;BR /&gt;===============================&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ic\readme.txt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev: see below&amp;nbsp; - This file.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;FONT color="#ff0000"&gt;I have these three files but not the rest.&lt;/FONT&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ic\etpu_ic.c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev : 2.0 - The C code file for the PWM API.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ic\etpu_ic.h&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev : 2.0 - The header file for the PWM API.&lt;BR /&gt;&lt;BR /&gt;The following files are needed in order to compile and use the example code:&lt;BR /&gt;_____________________________________________________________________________&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2863SW "Using eTPU standard function set 1"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; etpu_set1\etpu_set1.h&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Image of eTPU set1 function code.&lt;BR /&gt;_____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2864SW "General C Functions for the eTPU."&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; utils\etpu_util.c&amp;nbsp;&amp;nbsp; - C code file for utility functions.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; utils\etpu_util.h&amp;nbsp;&amp;nbsp; - header file for utility functions.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; utils\etpu_struc.h&amp;nbsp; - Register and bit field definitions for the eTPU.&lt;BR /&gt;_____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2855SW "Using GPIO on MPC5500"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\fs_gpio.c - MPC5500 GPIO low level driver C code file.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\fs_gpio.h - MPC5500 GPIO low level driver header file.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\crt0.s&amp;nbsp;&amp;nbsp;&amp;nbsp; - Start-up file&lt;BR /&gt;_____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2856SW "Using the MPC5554 header file"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\mpc5554.h&amp;nbsp; - Register and bit field definitions for MPC5554.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\typedefs.h - Defines all for data types.&lt;BR /&gt;____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;All of the above files are available from the &lt;STRONG&gt;Freescale website.&lt;/STRONG&gt;&lt;BR /&gt;_____________________________________________________________________________&lt;BR /&gt;&lt;/EM&gt;&lt;BR /&gt;How can i get these files?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//Emanuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 11 Mar 2009 19:35:27 GMT</pubDate>
    <dc:creator>Manix</dc:creator>
    <dc:date>2009-03-11T19:35:27Z</dc:date>
    <item>
      <title>Getting necessary files for setting up environment for PWM (Pulse Width Modulation) using MPC5567</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161044#M831</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey there!&lt;/P&gt;&lt;P&gt;Im just about to learn how to control a motor with the MPC5567 and now Im gonna obtain the files I need to do my compilations. Problem is, I cant find the listed files in the following pwm readme file that tells me to download them from the freescale homepage. Here is the readme ==&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;EM&gt;This is release 2.0 of the PWM API and example files.&lt;BR /&gt;The user should refer to Application Note AN2849 "Using the Pulse Width&lt;BR /&gt;Modulation (PWM) eTPU Function" which is available from Freescale.&lt;BR /&gt;&lt;BR /&gt;This is a first release of the API without exmaple programs.&lt;BR /&gt;_____________________________________________________________________________&lt;BR /&gt;&lt;BR /&gt;Files included in this package:&lt;BR /&gt;===============================&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ic\readme.txt&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev: see below&amp;nbsp; - This file.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;FONT color="#ff0000"&gt;I have these three files but not the rest.&lt;/FONT&gt;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ic\etpu_ic.c&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev : 2.0 - The C code file for the PWM API.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; ic\etpu_ic.h&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Rev : 2.0 - The header file for the PWM API.&lt;BR /&gt;&lt;BR /&gt;The following files are needed in order to compile and use the example code:&lt;BR /&gt;_____________________________________________________________________________&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2863SW "Using eTPU standard function set 1"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; etpu_set1\etpu_set1.h&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; - Image of eTPU set1 function code.&lt;BR /&gt;_____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2864SW "General C Functions for the eTPU."&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; utils\etpu_util.c&amp;nbsp;&amp;nbsp; - C code file for utility functions.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; utils\etpu_util.h&amp;nbsp;&amp;nbsp; - header file for utility functions.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; utils\etpu_struc.h&amp;nbsp; - Register and bit field definitions for the eTPU.&lt;BR /&gt;_____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2855SW "Using GPIO on MPC5500"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\fs_gpio.c - MPC5500 GPIO low level driver C code file.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\fs_gpio.h - MPC5500 GPIO low level driver header file.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\crt0.s&amp;nbsp;&amp;nbsp;&amp;nbsp; - Start-up file&lt;BR /&gt;_____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;&amp;nbsp; From AN2856SW "Using the MPC5554 header file"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\mpc5554.h&amp;nbsp; - Register and bit field definitions for MPC5554.&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; mpc5500\typedefs.h - Defines all for data types.&lt;BR /&gt;____________________________________________________________________________&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;All of the above files are available from the &lt;STRONG&gt;Freescale website.&lt;/STRONG&gt;&lt;BR /&gt;_____________________________________________________________________________&lt;BR /&gt;&lt;/EM&gt;&lt;BR /&gt;How can i get these files?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//Emanuel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2009 19:35:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161044#M831</guid>
      <dc:creator>Manix</dc:creator>
      <dc:date>2009-03-11T19:35:27Z</dc:date>
    </item>
    <item>
      <title>Re: Getting necessary files for setting up environment for PWM (Pulse Width Modulation) using MPC556</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161045#M832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hey Manix,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can use the page at this link:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/etpu/" target="test_blank"&gt;http://www.freescale.com/webapp/etpu/&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;It will package all the software you need for your application into one.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Specific links for your requests bellow:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=AN2864SW_UTILS&amp;amp;appType=license&amp;amp;location=null&amp;amp;fpsp=1" rel="nofollow" target="_blank"&gt;AN2864SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=AN2855SW&amp;amp;appType=license&amp;amp;location=null&amp;amp;fsrch=1%20" rel="nofollow" target="_blank"&gt;AN2855SW&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MPC5554&amp;amp;nodeId=0162468rH3bTdG06C10325&amp;amp;fpsp=1&amp;amp;tab=Design_Tools_Tab#" rel="nofollow" target="_blank"&gt;Header Files for the MPC5567&lt;/A&gt; - There was never an applications note for these.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Dayve&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2009 23:06:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161045#M832</guid>
      <dc:creator>dayve</dc:creator>
      <dc:date>2009-03-11T23:06:19Z</dc:date>
    </item>
    <item>
      <title>Re: Getting necessary files for setting up environment for PWM (Pulse Width Modulation)using MPC5567</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161046#M833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Okay! Thanks.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;So, if Im gonna use an AC three-phase motor with the MPC5567, Im I then supposed to get the &lt;SPAN&gt;&lt;SPAN&gt;PWMMAC&lt;/SPAN&gt; AND &lt;SPAN&gt;PWMF&lt;/SPAN&gt; from the &lt;A href="http://www.freescale.com/webapp/etpu/" target="test_blank"&gt;http://www.freescale.com/webapp/etpu/&lt;/A&gt; page? Thus, not the one just called PWM?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;//Manix&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2009 02:36:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Getting-necessary-files-for-setting-up-environment-for-PWM-Pulse/m-p/161046#M833</guid>
      <dc:creator>Manix</dc:creator>
      <dc:date>2009-03-19T02:36:04Z</dc:date>
    </item>
  </channel>
</rss>