<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: PCF2127 RTC RAM does not store data in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974149#M8110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomáš,&lt;/P&gt;&lt;P&gt;thank you for your reply and sorry for the delay.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;So far I had&amp;nbsp;six devices in my hands, two were bought&amp;nbsp;some months ago for prototypes and four belong to a new batch of 16. The 16 devices are soldered, but so far I have commissioned only 4 of them. All are from Digikey, so I do not expect them to be counterfeit. I observed the behavior only on one device.&lt;/LI&gt;&lt;LI&gt;The two from the first batch work, two from the new batch were sent to a customer without testing of this feature (An automatic test only checks whether the RTC communicates and if the time runs and is retained. An automatic check of the RAM was not implemented) one is faulty (that was found out after delivering the first two) and one which I tested after discovering the problem works as expected.&lt;BR /&gt;That leaves 12 more to be tested, not counting the two already delivered which would inevitably return later...&lt;/LI&gt;&lt;LI&gt;Image of the faulty device is attached. The PCBs got a layer of protective varnish, which makes the markings a little harder to read. And it gathered some dust during testing.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87428iF98AFC71E9B306C9/image-size/large?v=v2&amp;amp;px=999" title="Image.jpg" alt="Image.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Aug 2019 13:22:36 GMT</pubDate>
    <dc:creator>quex</dc:creator>
    <dc:date>2019-08-15T13:22:36Z</dc:date>
    <item>
      <title>PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974147#M8108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a problem with one PCF2127 RTC IC.&lt;/P&gt;&lt;P&gt;The clock works, I can set and read the time via I2C.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other feature I'm using is the backed-up RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But when I write the registers and read them back, I get only zeros.&lt;/P&gt;&lt;P&gt;The PCF2127 responds, but the values are zero.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It looks like this:&lt;/P&gt;&lt;P&gt;Writing 5 bytes starting at address 0:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86637i91BBA10BBEF21CF4/image-size/large?v=v2&amp;amp;px=999" title="03_Write5Bytes_Addr0.png" alt="03_Write5Bytes_Addr0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Reading the 5 bytes back:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86683iB92CD8E0755CECE1/image-size/large?v=v2&amp;amp;px=999" title="04_Read5Bytes_Addr0.png" alt="04_Read5Bytes_Addr0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On another unit (the same device type, identical MCU application) it behaves correctly:&lt;/P&gt;&lt;P&gt;Writing 5 bytes starting at address 0:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86721i62D65AA255868807/image-size/large?v=v2&amp;amp;px=999" title="07_Write5Bytes_Addr0_OK.png" alt="07_Write5Bytes_Addr0_OK.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Reading the 5 bytes back:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86644i8F2EB399A65C7072/image-size/large?v=v2&amp;amp;px=999" title="08_Read5Bytes_Addr0_OK.png" alt="08_Read5Bytes_Addr0_OK.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also tried writing 5 bytes @ address 64, but with the same result.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The schematics of the circuit:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86684i647D0867FFDE9800/image-size/large?v=v2&amp;amp;px=999" title="Schematics.png" alt="Schematics.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;It seems to me that the PCF2127 is defective.&lt;/P&gt;&lt;P&gt;Is there any procedure that could be used to test/identify the problem or restore the correct function?&lt;/P&gt;&lt;P&gt;Has this behavior been observed before?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Aug 2019 15:31:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974147#M8108</guid>
      <dc:creator>quex</dc:creator>
      <dc:date>2019-08-09T15:31:29Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974148#M8109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It sounds like a quality issue. I do have a few questions to let us start:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How many parts have you tested so far and on how many of them have you observed this behavior?&lt;/P&gt;&lt;P&gt;2. Are all tested parts from the same batch?&lt;/P&gt;&lt;P&gt;3. What is the complete marking found on the top side of tested parts?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 07:55:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974148#M8109</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-08-12T07:55:40Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974149#M8110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tomáš,&lt;/P&gt;&lt;P&gt;thank you for your reply and sorry for the delay.&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;So far I had&amp;nbsp;six devices in my hands, two were bought&amp;nbsp;some months ago for prototypes and four belong to a new batch of 16. The 16 devices are soldered, but so far I have commissioned only 4 of them. All are from Digikey, so I do not expect them to be counterfeit. I observed the behavior only on one device.&lt;/LI&gt;&lt;LI&gt;The two from the first batch work, two from the new batch were sent to a customer without testing of this feature (An automatic test only checks whether the RTC communicates and if the time runs and is retained. An automatic check of the RAM was not implemented) one is faulty (that was found out after delivering the first two) and one which I tested after discovering the problem works as expected.&lt;BR /&gt;That leaves 12 more to be tested, not counting the two already delivered which would inevitably return later...&lt;/LI&gt;&lt;LI&gt;Image of the faulty device is attached. The PCBs got a layer of protective varnish, which makes the markings a little harder to read. And it gathered some dust during testing.&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/87428iF98AFC71E9B306C9/image-size/large?v=v2&amp;amp;px=999" title="Image.jpg" alt="Image.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Aug 2019 13:22:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974149#M8110</guid>
      <dc:creator>quex</dc:creator>
      <dc:date>2019-08-15T13:22:36Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974150#M8111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Michal,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your answers.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am afraid that&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;it will be necessary to perform a detailed analysis of faulty parts by our quality engineers in their lab.&amp;nbsp;Our standard procedure for this is to submit a CQI (Customer Quality Incident) request through a distributor you bought the parts from (DigiKey).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Best regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Tomas&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 20 Aug 2019 06:51:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974150#M8111</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-08-20T06:51:11Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974151#M8112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Tomas,&lt;/P&gt;&lt;P&gt;please send me information to the procedure of submitting the CQI.&lt;/P&gt;&lt;P&gt;Is NXP involved from the beginning or does the distributor contact NXP?&lt;/P&gt;&lt;P&gt;I will have to have the part de-soldered.&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 29 Sep 2019 12:49:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/974151#M8112</guid>
      <dc:creator>quex</dc:creator>
      <dc:date>2019-09-29T12:49:06Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1153023#M9321</link>
      <description>&lt;P&gt;Did this ever get resolved? I am experiencing the same issue with the exact same chips that we bought around the same time frame. Approximately 35% of our chips the RAM does not work at all, but every other feature works. Same exact boards, circuits, firmware etc...&lt;/P&gt;</description>
      <pubDate>Mon, 14 Sep 2020 18:52:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1153023#M9321</guid>
      <dc:creator>dave_harmonjr</dc:creator>
      <dc:date>2020-09-14T18:52:32Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1229474#M10429</link>
      <description>&lt;DIV class="QmZWSe"&gt;&lt;DIV class="DHcWmd"&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;&lt;DIV class="oSioSc"&gt;&lt;DIV class=""&gt;&lt;DIV class="g9WsWb"&gt;&lt;DIV class="tw-ta-container hide-focus-ring tw-nfl"&gt;&lt;PRE&gt;&lt;SPAN&gt;I have the same question, &lt;BR /&gt;because we have the same problem. &lt;BR /&gt;&lt;BR /&gt;Was there always a workaround, &lt;BR /&gt;or are the ICs defective and have to be replaced?&lt;/SPAN&gt;&lt;/PRE&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Wed, 10 Feb 2021 17:39:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1229474#M10429</guid>
      <dc:creator>BOWUx</dc:creator>
      <dc:date>2021-02-10T17:39:51Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232107#M10464</link>
      <description>&lt;P&gt;We experience something similar, so I'm interested in knowing if you reached a solution or conclusion?&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 14:42:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232107#M10464</guid>
      <dc:creator>tkhansen</dc:creator>
      <dc:date>2021-02-17T14:42:23Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232113#M10465</link>
      <description>&lt;P&gt;In my case I had a bad batch of IC's and simply replacing them with a new batch fixed it.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 14:55:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232113#M10465</guid>
      <dc:creator>dave_harmonjr</dc:creator>
      <dc:date>2021-02-17T14:55:27Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232116#M10466</link>
      <description>&lt;P&gt;Thanks for getting back so quickly. Can you remember the bath codes (week, year etc.)?&lt;/P&gt;&lt;P&gt;In out case these boards where produced last year and we didn't catch anything in production but have received complaints from costumers so it could be we have used components from the same batch.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 15:02:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232116#M10466</guid>
      <dc:creator>tkhansen</dc:creator>
      <dc:date>2021-02-17T15:02:51Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232119#M10467</link>
      <description>&lt;P&gt;This is what is written on one of the faulty IC's.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;"PCF2127T&lt;/P&gt;&lt;P&gt;AFF 173&lt;/P&gt;&lt;P&gt;1&amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp; &amp;nbsp;05&lt;/P&gt;&lt;P&gt;knD19202"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We had probably a 80+% fail rate on all the RTC's we got from this batch.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;After we bought a new batch 100% have worked.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 15:09:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232119#M10467</guid>
      <dc:creator>dave_harmonjr</dc:creator>
      <dc:date>2021-02-17T15:09:05Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232124#M10470</link>
      <description>&lt;P&gt;Thank you very much, I'll reach out to our production to hear if they can give me the batch codes for the failing parts.&lt;/P&gt;</description>
      <pubDate>Wed, 17 Feb 2021 15:15:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1232124#M10470</guid>
      <dc:creator>tkhansen</dc:creator>
      <dc:date>2021-02-17T15:15:43Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1239189#M10527</link>
      <description>&lt;P&gt;Hello, we have 4 faulty tested pieces from 52 ICs from 2 batches,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;which we bought at Farnell over 2 years ago.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;The difference to the problem described here is, that we don't know, when the RAM get into this state (RTC works further very well). &lt;/FONT&gt;&lt;BR /&gt;&lt;FONT color="#0000FF"&gt;And, when we discharge our connected GoldCap capacitor at VBAT (which unfortunately takes about 2 weeks in the closed device) we have full access to the memory again.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#0000FF"&gt;I adjusted the latter on the laboratory bench and unloaded the GoldCap. Then I can write to the RAM again and read back the exact content.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&lt;BR /&gt;We have the following 2 batches:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Batch: 180817000009&lt;/P&gt;&lt;P&gt;48 pieces of PCF2127T&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ACV098.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 19th&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; knD18192&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Batch: 180531000055&lt;/P&gt;&lt;P&gt;4pieces = PCF2127T&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ACT659.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1 59&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; knD18072&lt;BR /&gt;&lt;BR /&gt;Because, the order is more than 2 years old, we have received the answer from Farnell, that NXP will &lt;STRONG&gt;&lt;U&gt;not&lt;/U&gt;&lt;/STRONG&gt; make an CQC failure analysis.&lt;BR /&gt;&lt;BR /&gt;&lt;FONT color="#FF9900"&gt;&lt;STRONG&gt;Was the RAM of the PCF2127 not usable in all of these from the first start of device and permanently?&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF9900"&gt;&lt;STRONG&gt;&amp;nbsp;&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#FF9900"&gt;&lt;STRONG&gt;Does somebody has any idea?&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;Best regards&lt;/P&gt;</description>
      <pubDate>Wed, 03 Mar 2021 08:17:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1239189#M10527</guid>
      <dc:creator>BOWUx</dc:creator>
      <dc:date>2021-03-03T08:17:38Z</dc:date>
    </item>
    <item>
      <title>Re: PCF2127 RTC RAM does not store data</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1298418#M11384</link>
      <description>&lt;P&gt;At the moment i do not have a problem with the Ram, but i have many problems with the acuracy of the frequency.&lt;BR /&gt;The data sheet says +-3 ppm. But our chips of the year 2019 have more than &lt;STRONG&gt;19 ppm&lt;/STRONG&gt;. If i understood our customer, they have several days per year time differences (&lt;STRONG&gt;&amp;gt; 100 ppm&lt;/STRONG&gt;).&lt;BR /&gt;&lt;BR /&gt;The batch code is:&lt;BR /&gt;ACU4771.1 05&lt;BR /&gt;knE18142&lt;/P&gt;</description>
      <pubDate>Fri, 25 Jun 2021 11:13:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/PCF2127-RTC-RAM-does-not-store-data/m-p/1298418#M11384</guid>
      <dc:creator>NXPRalf</dc:creator>
      <dc:date>2021-06-25T11:13:28Z</dc:date>
    </item>
  </channel>
</rss>