<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: USB stack for iMX21? in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159670#M809</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I"m the one who posted the Linux MX21 USB Host Controller Driver mentionned above.&lt;/P&gt;&lt;P&gt;I should point out that is is _only_ the HCD component for _linux_. [Ie it is not a complete USB stack - linux already provides that fortunately, nor is it likely to be easilly portable to another (RT)OS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I expect to post I new version soon which has most of the problems worked out and runs the usbtest suite sucessfully.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've still got one strange problem : when multiple devices are using the bus it sometimes happens that the transfer completes (as witnessed by the completion code in the ETD being != 0xF (not accessed) and generally == 0x00 (Success)). However the ETD is not marked as done (and I don't get an interrupt). The problem never occurs with a single device using the bus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've worked around this in my driver by checking for this condition at each SOF but its not pretty.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know anything about this?&amp;nbsp; (can't find any mention of it in the errata).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Jun 2009 00:04:08 GMT</pubDate>
    <dc:creator>mfuzzey</dc:creator>
    <dc:date>2009-06-02T00:04:08Z</dc:date>
    <item>
      <title>USB stack for iMX21?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159668#M807</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all!&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We are using iMX21 on our custom system, using our in-house developed RTOS. I need to add USB device functionality. Do there exist any USB stacks already ported on iMX21?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;We have one open-source USB stack implementation, but it is not ported to iMX21, and before digging into this, I'd like to know if someone has already done that.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;n.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 08 Mar 2009 05:13:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159668#M807</guid>
      <dc:creator>niksa</dc:creator>
      <dc:date>2009-03-08T05:13:50Z</dc:date>
    </item>
    <item>
      <title>Re: USB stack for iMX21?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159669#M808</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can check this MX21 USB patch posted on ARM linux kernel mailing list: &lt;A href="http://marc.info/?l=linux-arm-kernel&amp;amp;m=123654014123907&amp;amp;w=2" rel="nofollow" target="_blank"&gt;http://marc.info/?l=linux-arm-kernel&amp;amp;m=123654014123907&amp;amp;w=2&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Fabio Estevam&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2009 05:17:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159669#M808</guid>
      <dc:creator>fabio_estevam</dc:creator>
      <dc:date>2009-03-09T05:17:25Z</dc:date>
    </item>
    <item>
      <title>Re: USB stack for iMX21?</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159670#M809</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I"m the one who posted the Linux MX21 USB Host Controller Driver mentionned above.&lt;/P&gt;&lt;P&gt;I should point out that is is _only_ the HCD component for _linux_. [Ie it is not a complete USB stack - linux already provides that fortunately, nor is it likely to be easilly portable to another (RT)OS.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I expect to post I new version soon which has most of the problems worked out and runs the usbtest suite sucessfully.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've still got one strange problem : when multiple devices are using the bus it sometimes happens that the transfer completes (as witnessed by the completion code in the ETD being != 0xF (not accessed) and generally == 0x00 (Success)). However the ETD is not marked as done (and I don't get an interrupt). The problem never occurs with a single device using the bus.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I've worked around this in my driver by checking for this condition at each SOF but its not pretty.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does anyone know anything about this?&amp;nbsp; (can't find any mention of it in the errata).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Martin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jun 2009 00:04:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/USB-stack-for-iMX21/m-p/159670#M809</guid>
      <dc:creator>mfuzzey</dc:creator>
      <dc:date>2009-06-02T00:04:08Z</dc:date>
    </item>
  </channel>
</rss>