<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックProblem reading the SC18IS602B buffer</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/907919#M7419</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the SC18IS602B to bridge from an I2C bus to a SPI component. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have gotten the "WRITE" side of the equation working. The SC18IS602B sends the data to the SPI chip as expected and I can get the SPI to return correct data when reading on the SPI device, all confirmed on the scope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BUT, I can't manage to get anything but a single 0x00 byte from the SC18IS602B buffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On top of that the example in the datasheet, chapter 8, step 8 seems to be wrong, or I am missing something. It indicates 0x50 on the I2C bus after the start bit, which is a write operation. It is then very unclear about the remaining bytes whether those are coming from the microcontroller or is sent by SC18IS602B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also remarkably little information available on the Internet and nxp.com, indicating that the chip isn't that much used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So... anybody got any ideas of what I might be doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FTR, in all this, I have been using "i2cdetect", "i2cget" and "i2cset" Linux commands to interact with the SC18IS602B, and maybe I need to do a write command (which the example seems to suggest, but conflicts with 7.1.4 in datasheet) and scoop up bytes coming back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Datasheet I have been looking at is; &lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf" title="https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help whatsoever is greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Niclas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 10 May 2019 07:09:13 GMT</pubDate>
    <dc:creator>niclas1</dc:creator>
    <dc:date>2019-05-10T07:09:13Z</dc:date>
    <item>
      <title>Problem reading the SC18IS602B buffer</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/907919#M7419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am using the SC18IS602B to bridge from an I2C bus to a SPI component. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have gotten the "WRITE" side of the equation working. The SC18IS602B sends the data to the SPI chip as expected and I can get the SPI to return correct data when reading on the SPI device, all confirmed on the scope.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BUT, I can't manage to get anything but a single 0x00 byte from the SC18IS602B buffer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On top of that the example in the datasheet, chapter 8, step 8 seems to be wrong, or I am missing something. It indicates 0x50 on the I2C bus after the start bit, which is a write operation. It is then very unclear about the remaining bytes whether those are coming from the microcontroller or is sent by SC18IS602B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is also remarkably little information available on the Internet and nxp.com, indicating that the chip isn't that much used.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So... anybody got any ideas of what I might be doing wrong?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;FTR, in all this, I have been using "i2cdetect", "i2cget" and "i2cset" Linux commands to interact with the SC18IS602B, and maybe I need to do a write command (which the example seems to suggest, but conflicts with 7.1.4 in datasheet) and scoop up bytes coming back.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Datasheet I have been looking at is; &lt;A class="link-titled" href="https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf" title="https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf"&gt;https://www.nxp.com/docs/en/data-sheet/SC18IS602B.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help whatsoever is greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Niclas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 May 2019 07:09:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/907919#M7419</guid>
      <dc:creator>niclas1</dc:creator>
      <dc:date>2019-05-10T07:09:13Z</dc:date>
    </item>
    <item>
      <title>Re: Problem reading the SC18IS602B buffer</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/907920#M7420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have managed to figure out what the problem is; The Linux CLI tool (i2cget) seems to be flaky at best. Once I coded up the communications via the Linux low-level APIs, I am getting the expected values back.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 May 2019 01:50:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/907920#M7420</guid>
      <dc:creator>niclas1</dc:creator>
      <dc:date>2019-05-13T01:50:01Z</dc:date>
    </item>
    <item>
      <title>Re: Problem reading the SC18IS602B buffer</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/1164400#M9545</link>
      <description>&lt;P&gt;Hi.&lt;BR /&gt;Can you please share the API you have used to establish communication to read the data from buffer, as we are also facing the same issue.&lt;BR /&gt;&lt;BR /&gt;Thanks in Advance&lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2020 08:57:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Problem-reading-the-SC18IS602B-buffer/m-p/1164400#M9545</guid>
      <dc:creator>ABHIN</dc:creator>
      <dc:date>2020-10-08T08:57:46Z</dc:date>
    </item>
  </channel>
</rss>