<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックMPC8313RDB board Kernel Source</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157429#M732</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Hi&lt;BR /&gt; &lt;BR /&gt; I am trying to compile a USB driver for MPC8313 Reference Design Board.&amp;nbsp; I do not have the source code to compile the drivers on Linux. They say they have to be extracted from an .iso file (which is non existent). Is there a way to develop the driver without using the Kernel source files (some GCC switches for OS Linux &amp;amp; powerpc as target)? Or can somebody help me find/locate Kernel source files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If at all the kernel source is present on the CD then under what filename is this hiding?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel Version: 2.6.20&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;BR /&gt;Ak&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Oct 2007 03:45:06 GMT</pubDate>
    <dc:creator>ak79</dc:creator>
    <dc:date>2007-10-23T03:45:06Z</dc:date>
    <item>
      <title>MPC8313RDB board Kernel Source</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157429#M732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;P&gt;Hi&lt;BR /&gt; &lt;BR /&gt; I am trying to compile a USB driver for MPC8313 Reference Design Board.&amp;nbsp; I do not have the source code to compile the drivers on Linux. They say they have to be extracted from an .iso file (which is non existent). Is there a way to develop the driver without using the Kernel source files (some GCC switches for OS Linux &amp;amp; powerpc as target)? Or can somebody help me find/locate Kernel source files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; If at all the kernel source is present on the CD then under what filename is this hiding?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kernel Version: 2.6.20&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks in advance,&lt;BR /&gt;Ak&lt;/P&gt;&lt;DIV&gt; &lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Oct 2007 03:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157429#M732</guid>
      <dc:creator>ak79</dc:creator>
      <dc:date>2007-10-23T03:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313RDB board Kernel Source</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157430#M733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;&lt;DIV&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;ak79,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The kernel files are in a package file, so you will not find them directly on the CD you get with the board.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;To get to the Kernel source files, you have to do an install of the LTIB environment and then request the kernel files to be extracted and built.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;When it comes to installing the LTIB environment it can be done fromt the CD or by dowloading the latest .iso file from the Freescale site. I would recommend doing the download as you will get the latest source code that way (if you really want to load from the CD, the instructions are just about the same except you need to mount the CD directly with execute privileges and run the install script from it)&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;To find the latest BSP for the MPC8313, if you login to the Freescale site and do a keyword search at the Freescale for MPC8313 and BSP you get a link to it:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;STRONG&gt;&lt;A href="https://www.freescale.com/webapp/Download?colCode=CWF-MPC8313E-RDB&amp;amp;location=null&amp;amp;fsrch=1" target="test_blank"&gt;https://www.freescale.com/webapp/Download?colCode=CWF-MPC8313E-RDB&amp;amp;location=null&amp;amp;fsrch=1&lt;/A&gt;&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Fill out the form and download the file.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Download that file, put it into a working directory, as root mount the .iso file CD image as an executable directory, and then as your normal Linux login, run install (example):&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~$ ls *.iso&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;MPC8313E_RDB_K26_20070831-LTIB.iso&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~$ su&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;Password:&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;raptor:/home/alan# ls -ld cdmount&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;drwxrwxrwx 2 alan alan 4096 2007-05-29 11:51 cdmount&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;raptor:/home/alan# mount -o loop MPC8313E_RDB_K26_20070831-LTIB.iso cdmount&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;raptor:/home/alan# exit&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;exit&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~$&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~$ cdmount/install&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;Once you've done that, you need to change directory to the one you installed it in and run ltib for the first time (example)&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~$ cd ltib-mpc8313erdb-20070824/&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;Assuming that you've gottent the install and initial build completed, you can now ask for the Linux kernel sources to be extracted and built by;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ ./ltib --configure&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;On the first menu that pops up, select the following two options, then exit&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;[*] Configure the kernel&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;[*] Leave the sources after building&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;When the kernel config menu comes up, you can just select exit.&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;The kernel sources will then be extracted and built, if you do this with the current version the main Linux kernel source can be found at:&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~/ltib-mpc8313erdb-20070824$ cd rpm/BUILD/linux-2.6.20/&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20$&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20$ ls&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;arch CREDITS drivers init kernel Makefile net scripts System.map vmlinux.bin.gz&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;block crypto fs ipc lib mm README security usr&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;COPYING Documentation include Kbuild MAINTAINERS Module.symvers REPORTING-BUGS sound vmlinux&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;The usb drivers are under the drivers directory.&lt;/FONT&gt;&lt;/P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;alan@raptor:~/ltib-mpc8313erdb-20070824/rpm/BUILD/linux-2.6.20/drivers/usb$ ls&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;atm class gadget image Kconfig misc net README storage&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT face="Courier New" size="2"&gt;&lt;STRONG&gt;built-in.o core host input Makefile mon otg serial usb-skeleton.c&lt;/STRONG&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;FONT size="2"&gt;&lt;/FONT&gt;&lt;P&gt;&lt;FONT size="2"&gt;Hope this helps :smileyhappy:&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;Best regards,&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;abartky&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Oct 2007 00:31:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157430#M733</guid>
      <dc:creator>abartky</dc:creator>
      <dc:date>2007-10-25T00:31:44Z</dc:date>
    </item>
    <item>
      <title>Re: MPC8313RDB board Kernel Source</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157431#M734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;DIV&gt;&lt;/DIV&gt;Thanks abartky,&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&lt;BR /&gt;&amp;nbsp; &amp;nbsp; &amp;nbsp; The steps mentioned made the process of extracting kernel files easy from the iso package and your instructions were really helpful.&lt;BR /&gt;&lt;BR /&gt;Thanks again,&lt;BR /&gt;Ak&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Nov 2007 03:58:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/MPC8313RDB-board-Kernel-Source/m-p/157431#M734</guid>
      <dc:creator>ak79</dc:creator>
      <dc:date>2007-11-09T03:58:59Z</dc:date>
    </item>
  </channel>
</rss>