<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックChip Configuration missing for imx8</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Chip-Configuration-missing-for-imx8/m-p/895925#M7263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This question is regarding the i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual (rev D.)where it describes the ADC registers (Chapter 16).&lt;/P&gt;&lt;P&gt;ADC Command Low Buffer Register (CMDL1 - CMDL15) registers have a field called ADCH.&lt;/P&gt;&lt;P&gt;The description states that there are 32 A and B channel inputs to the ADC that can be used as the input to the ADC for this command.&lt;/P&gt;&lt;P&gt;It also states:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;NOTE: Not all pairs are intended to be converted as differential channels. For the pin pairings available&lt;BR /&gt;for differential conversions for your device, see the Chip Configuration details.&lt;BR /&gt;NOTE: Some of the input channels are from internal resources such as temperature sensors and&lt;BR /&gt;bandgap voltage sources and may only be connected to individual instances of the ADC module.&lt;BR /&gt;Some of the input channel options in the bitfield-setting descriptions might not be available for&lt;BR /&gt;your device. For the ADC channel assignments for your device, see the Chip Configuration&lt;BR /&gt;details.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The detail in the Pin descriptions says there are potentially six input pins available to the ADC, depending on the pin muxing.&lt;/P&gt;&lt;P&gt;I want to know:&lt;/P&gt;&lt;P&gt;1. How do the six input pins map to the ADCH channels as descroibed for this register.&lt;/P&gt;&lt;P&gt;2. Where is the description of the potential internal inputs for this device (e.g. temp sensors), and how do they map to these inputs?&lt;/P&gt;&lt;P&gt;I am unable to find the "Chip Configuration" the documentation refers to that defines this information.&lt;/P&gt;&lt;P&gt;Thanks for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 15 Apr 2019 08:53:29 GMT</pubDate>
    <dc:creator>glynj</dc:creator>
    <dc:date>2019-04-15T08:53:29Z</dc:date>
    <item>
      <title>Chip Configuration missing for imx8</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Chip-Configuration-missing-for-imx8/m-p/895925#M7263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This question is regarding the i.MX 8DualXPlus/8QuadXPlus Applications Processor Reference Manual (rev D.)where it describes the ADC registers (Chapter 16).&lt;/P&gt;&lt;P&gt;ADC Command Low Buffer Register (CMDL1 - CMDL15) registers have a field called ADCH.&lt;/P&gt;&lt;P&gt;The description states that there are 32 A and B channel inputs to the ADC that can be used as the input to the ADC for this command.&lt;/P&gt;&lt;P&gt;It also states:&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;NOTE: Not all pairs are intended to be converted as differential channels. For the pin pairings available&lt;BR /&gt;for differential conversions for your device, see the Chip Configuration details.&lt;BR /&gt;NOTE: Some of the input channels are from internal resources such as temperature sensors and&lt;BR /&gt;bandgap voltage sources and may only be connected to individual instances of the ADC module.&lt;BR /&gt;Some of the input channel options in the bitfield-setting descriptions might not be available for&lt;BR /&gt;your device. For the ADC channel assignments for your device, see the Chip Configuration&lt;BR /&gt;details.&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;The detail in the Pin descriptions says there are potentially six input pins available to the ADC, depending on the pin muxing.&lt;/P&gt;&lt;P&gt;I want to know:&lt;/P&gt;&lt;P&gt;1. How do the six input pins map to the ADCH channels as descroibed for this register.&lt;/P&gt;&lt;P&gt;2. Where is the description of the potential internal inputs for this device (e.g. temp sensors), and how do they map to these inputs?&lt;/P&gt;&lt;P&gt;I am unable to find the "Chip Configuration" the documentation refers to that defines this information.&lt;/P&gt;&lt;P&gt;Thanks for any help.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 08:53:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Chip-Configuration-missing-for-imx8/m-p/895925#M7263</guid>
      <dc:creator>glynj</dc:creator>
      <dc:date>2019-04-15T08:53:29Z</dc:date>
    </item>
    <item>
      <title>Re: Chip Configuration missing for imx8</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Chip-Configuration-missing-for-imx8/m-p/895926#M7264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jones,&lt;BR /&gt;The i.MX8DX/QX is still on preproduction, so, no additional information could be provided yet. In case of having doubts, please refer with your Sales/FAE.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Just as additional recommendation, you could take a look to the following document, which explains the functionality of the ADC module included on Kinetis microcontrollers, which is a little bit similar to the included on i.MX8X:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/docs/en/supporting-information/Analog-to-digital-Converter-Training.pdf" title="https://www.nxp.com/docs/en/supporting-information/Analog-to-digital-Converter-Training.pdf"&gt;https://www.nxp.com/docs/en/supporting-information/Analog-to-digital-Converter-Training.pdf&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Hope this will be useful for you.&lt;BR /&gt;Best regards!&lt;BR /&gt;/Carlos&lt;BR /&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Apr 2019 21:32:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Chip-Configuration-missing-for-imx8/m-p/895926#M7264</guid>
      <dc:creator>CarlosCasillas</dc:creator>
      <dc:date>2019-04-15T21:32:04Z</dc:date>
    </item>
  </channel>
</rss>