<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Floating Outputs on MC33883 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/Floating-Outputs-on-MC33883/m-p/888052#M7138</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am testing the MC33883 in the typical application (as shown in figure 14) and noticed that when the output of the mosfet (source of high side mosfet/drain of low side mosfet) is not connected to a load the voltage sits at Vboost - 4 and can supply enough current to drive small loads even when the inputs are low.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this within the expected operation of the circuit or can I modify the circuit so that the output is floating when not connected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rhyse&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Feb 2019 20:02:33 GMT</pubDate>
    <dc:creator>rmaryniu</dc:creator>
    <dc:date>2019-02-06T20:02:33Z</dc:date>
    <item>
      <title>Floating Outputs on MC33883</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/Floating-Outputs-on-MC33883/m-p/888052#M7138</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am testing the MC33883 in the typical application (as shown in figure 14) and noticed that when the output of the mosfet (source of high side mosfet/drain of low side mosfet) is not connected to a load the voltage sits at Vboost - 4 and can supply enough current to drive small loads even when the inputs are low.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this within the expected operation of the circuit or can I modify the circuit so that the output is floating when not connected?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Rhyse&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Feb 2019 20:02:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/Floating-Outputs-on-MC33883/m-p/888052#M7138</guid>
      <dc:creator>rmaryniu</dc:creator>
      <dc:date>2019-02-06T20:02:33Z</dc:date>
    </item>
  </channel>
</rss>