<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic TJA1059 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1059/m-p/882060#M7046</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does TJA1059 comply the following standard ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ISO 11898-1:&lt;/STRONG&gt; International standard defining the CAN data link layer including LLC, MAC and PLS sub-layers.&lt;/P&gt;&lt;P&gt;In the datasheet, it specifies that the TJA1059 complies with ISO 11898-2:2016 and SAE J2284-1 to SAE J2284-5, but there is no information regarding ISO 11898 -1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 10 Mar 2019 04:49:20 GMT</pubDate>
    <dc:creator>deepaknath</dc:creator>
    <dc:date>2019-03-10T04:49:20Z</dc:date>
    <item>
      <title>TJA1059</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1059/m-p/882060#M7046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Does TJA1059 comply the following standard ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;ISO 11898-1:&lt;/STRONG&gt; International standard defining the CAN data link layer including LLC, MAC and PLS sub-layers.&lt;/P&gt;&lt;P&gt;In the datasheet, it specifies that the TJA1059 complies with ISO 11898-2:2016 and SAE J2284-1 to SAE J2284-5, but there is no information regarding ISO 11898 -1.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 10 Mar 2019 04:49:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1059/m-p/882060#M7046</guid>
      <dc:creator>deepaknath</dc:creator>
      <dc:date>2019-03-10T04:49:20Z</dc:date>
    </item>
    <item>
      <title>Re: TJA1059</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/TJA1059/m-p/882061#M7047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Srinath,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As already written in your question: “ISO 11898-1: International standard defining the CAN data link layer including LLC, MAC and PLS sub-layers”. ISO11898-1 defines the CAN protocol, which is handled by the CAN controller and is not relevant for the transceiver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Our transceivers need to comply to ISO11898-2, which is the physical layer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Tomas&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;EM style="border: none windowtext 1.0pt; padding: 0in; color: #3d3d3d; font-size: 9.0pt; "&gt;PS:&amp;nbsp;If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.&lt;/EM&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Mar 2019 10:54:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/TJA1059/m-p/882061#M7047</guid>
      <dc:creator>TomasVaverka</dc:creator>
      <dc:date>2019-03-12T10:54:33Z</dc:date>
    </item>
  </channel>
</rss>