<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>Other NXP ProductsのトピックRe: NXQ1TXH5 application</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/NXQ1TXH5-application/m-p/879454#M7015</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hualong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can still implement the wireless charging functions if you don’t use these 2 pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pins 3 and 4 (SDA and SCL) are for the I2C interface as part of the support interface for the NXQ1TXH5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NXQ1TXH5 is an easy to use fully integrated chip that can be completely configured by means of external resistors so in general there is no need for customers to have access to the I2C bus to configure the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check section 2.1.7 Support interface for the application note AN11775 &lt;A href="https://www.nxp.com/docs/en/application-note/AN11775.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11775.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Paulina&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jan 2019 18:43:58 GMT</pubDate>
    <dc:creator>lisettelozano</dc:creator>
    <dc:date>2019-01-18T18:43:58Z</dc:date>
    <item>
      <title>NXQ1TXH5 application</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXQ1TXH5-application/m-p/879453#M7014</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear all.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;When I look at the NXQ1TXH5 data sheet, I don't understand the functions of pins 3 and 4 (SDA and SCL). If I don't use these 2 pins, can I implement the wireless charging function?Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Jan 2019 13:23:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXQ1TXH5-application/m-p/879453#M7014</guid>
      <dc:creator>549290520</dc:creator>
      <dc:date>2019-01-16T13:23:31Z</dc:date>
    </item>
    <item>
      <title>Re: NXQ1TXH5 application</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/NXQ1TXH5-application/m-p/879454#M7015</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Hualong,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you can still implement the wireless charging functions if you don’t use these 2 pins.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The pins 3 and 4 (SDA and SCL) are for the I2C interface as part of the support interface for the NXQ1TXH5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NXQ1TXH5 is an easy to use fully integrated chip that can be completely configured by means of external resistors so in general there is no need for customers to have access to the I2C bus to configure the chip.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can check section 2.1.7 Support interface for the application note AN11775 &lt;A href="https://www.nxp.com/docs/en/application-note/AN11775.pdf"&gt;https://www.nxp.com/docs/en/application-note/AN11775.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt;"&gt;Paulina&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2019 18:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/NXQ1TXH5-application/m-p/879454#M7015</guid>
      <dc:creator>lisettelozano</dc:creator>
      <dc:date>2019-01-18T18:43:58Z</dc:date>
    </item>
  </channel>
</rss>