<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SJA1124 clock input in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878691#M7003</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JuanCar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, it is ok if you use a 8MHz oscillator and the PLL can be adjusted from the registers so that you can generate any desired baudrate.&lt;/P&gt;&lt;P&gt;But it is important that the tolerance of the external clock reference should be within ±0.3%.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Apr 2019 20:28:03 GMT</pubDate>
    <dc:creator>reyes</dc:creator>
    <dc:date>2019-04-04T20:28:03Z</dc:date>
    <item>
      <title>SJA1124 clock input</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878688#M7000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's been a while since I've used this forum (apologies if this post is in the wrong place). I am interested in using an SJA1124 IC. I don't fully understand the "CLK" input. Am I supposed to use an external oscillator or use an mcu clock output?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope someone has already dealt with this&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Apr 2019 20:21:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878688#M7000</guid>
      <dc:creator>Skaptor</dc:creator>
      <dc:date>2019-04-03T20:21:31Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1124 clock input</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878689#M7001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JuanCar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A good quality input clock is necessary for proper PLL performance. It can be either from an external oscillator or from a mcu clock output as long&amp;nbsp; as the frequency of the reference clock on pin CLK is within the specified operating range, fclk(PLL)in. = External reference frequency operating range between 0.4 and 10 MHz.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;To meet LIN master requirements for baud rate deviation, the tolerance of the external clock reference should be within ±0.3%.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jose&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 15:38:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878689#M7001</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-04-04T15:38:57Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1124 clock input</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878690#M7002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jose,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the quick answer. So is it ok if I use an external 8MHz oscillator? Then the PLL can be adjusted from the registers so that I can generated any desired baudrate. is this right?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 16:38:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878690#M7002</guid>
      <dc:creator>Skaptor</dc:creator>
      <dc:date>2019-04-04T16:38:04Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1124 clock input</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878691#M7003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi JuanCar,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Yes, it is ok if you use a 8MHz oscillator and the PLL can be adjusted from the registers so that you can generate any desired baudrate.&lt;/P&gt;&lt;P&gt;But it is important that the tolerance of the external clock reference should be within ±0.3%.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Apr 2019 20:28:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878691#M7003</guid>
      <dc:creator>reyes</dc:creator>
      <dc:date>2019-04-04T20:28:03Z</dc:date>
    </item>
    <item>
      <title>Re: SJA1124 clock input</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878692#M7004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jose,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The boards finally arrived, do you know where I can get some example code? I am having trouble getting the "LIN normal mode" status&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Jun 2019 18:32:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/SJA1124-clock-input/m-p/878692#M7004</guid>
      <dc:creator>Skaptor</dc:creator>
      <dc:date>2019-06-11T18:32:49Z</dc:date>
    </item>
  </channel>
</rss>