<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: imx7 in Other NXP Products</title>
    <link>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870166#M6884</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;changes are performed manually, may be useful to check ddr tool presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331528"&gt;DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 08 Mar 2019 07:24:20 GMT</pubDate>
    <dc:creator>igorpadykov</dc:creator>
    <dc:date>2019-03-08T07:24:20Z</dc:date>
    <item>
      <title>imx7</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870163#M6881</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi there,&lt;/P&gt;&lt;P&gt;I got an imx7ulpevk board. For some reason, the DRAM was changed to a 2Gb LPDDR4. After that, it passes the stress test using the ddr_stress_tester_v3.00 and can run up to 500MHz. However, I didn't find "genuine" document regarding how to build a linux kernel for imx7 that can accommodate the change of the DRAM. When I use the default kernel image download from NXP web site, there is nothing coming out from debug port so I can't not check anything wrong.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please help and thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR,&lt;/P&gt;&lt;P&gt;KY&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 08:35:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870163#M6881</guid>
      <dc:creator>kayiyeh</dc:creator>
      <dc:date>2019-03-06T08:35:06Z</dc:date>
    </item>
    <item>
      <title>Re: imx7</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870164#M6882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;one can look at Porting Guide in &lt;A href="https://www.nxp.com/webapp/Download?colCode=L4.14.78_1.0.0_LINUX_DOCS&amp;amp;appType=license&amp;amp;location=null" target="_blank"&gt;Linux L4.14.78_1.0.0 Documentation&lt;/A&gt;&lt;/P&gt;&lt;P&gt;General steps are to update dcd header (imximage.cfg) with new ddr calibration settings&lt;/P&gt;&lt;P&gt;found from ddr tester&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx7ulp_evk?h=imx_v2018.03_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/board/freescale/mx7ulp_evk?h=imx_v2018.03_4.14.78_1.0.0_ga"&gt;mx7ulp_evk\freescale\board - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Memory size can be adjusted with #define PHYS_SDRAM_SIZE&amp;nbsp;&amp;nbsp; in&lt;/P&gt;&lt;P&gt;uboot/include/configs/mx7ulp_evk.h&amp;nbsp;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx7ulp_evk.h?h=imx_v2018.03_4.14.78_1.0.0_ga" title="https://source.codeaurora.org/external/imx/uboot-imx/tree/include/configs/mx7ulp_evk.h?h=imx_v2018.03_4.14.78_1.0.0_ga"&gt;mx7ulp_evk.h\configs\include - uboot-imx - i.MX U-Boot&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Mar 2019 10:32:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870164#M6882</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-03-06T10:32:21Z</dc:date>
    </item>
    <item>
      <title>Re: imx7</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870165#M6883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;Thank you for your quick response. I tried the suggestion you gave me, and download the u-boot source. However, I don’t know how to change the DCD or the imximage.cfg file. The reason is that all I got from the ddr stress tool is a calibration log, which I attached in this file. I see nothing similar between the file and the imximage.cfg. Could you give me more hint? Do I get the wrong ddr stress tool?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ka-Yi Yeh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 06:07:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870165#M6883</guid>
      <dc:creator>kayiyeh</dc:creator>
      <dc:date>2019-03-08T06:07:19Z</dc:date>
    </item>
    <item>
      <title>Re: imx7</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870166#M6884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ka-Yi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;changes are performed manually, may be useful to check ddr tool presentation&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-331528"&gt;DES-N1936 i.MX 6UltraLite DDR Tools Overview and Hardware Design Considerations&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;BR /&gt;igor&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 07:24:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870166#M6884</guid>
      <dc:creator>igorpadykov</dc:creator>
      <dc:date>2019-03-08T07:24:20Z</dc:date>
    </item>
    <item>
      <title>Re: imx7</title>
      <link>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870167#M6885</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Igor,&lt;/P&gt;&lt;P&gt;Thanks a lot. I will study more. However, I have more questions. You suggest some files need to be changed in the previous mail. Because I found using Yocto project  to build SD card is more straightforward for me, I want to build kernel/uboot from Yocto. But I found there are same file names. I don’t know which one is correct one? For example, under my build directory, there are 107 imximage.cfg files. I can rule out many of them because the directory name suggest they are not relevant, but there are still many files I can’t tell. BTW, I use “fsl-imx-fb” distro because all I need is command line interface.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ka-Yi Yeh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Mar 2019 08:44:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/Other-NXP-Products/imx7/m-p/870167#M6885</guid>
      <dc:creator>kayiyeh</dc:creator>
      <dc:date>2019-03-08T08:44:32Z</dc:date>
    </item>
  </channel>
</rss>